![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|


Go to the source code of this file.
Macros | |
| #define | FSL_ISF_UART1 UART0_IDX |
Functions | |
| void | ISF_UART1_IRQHandler (void) |
Variables | |
| uart_state_t | ISF_UART1_State |
| const uart_user_config_t | ISF_UART1_InitConfig0 |
| UART configuration declaration. More... | |
Definition in file ISF_UART1.h.