![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "MMA955x_2.h"#include "isf_util.h"#include "isf_spi_master_types.h"#include "ChipSelect.h"#include "SensorReset.h"
Go to the source code of this file.
Macros | |
| #define | FSL_SENSOR_SPI_CMD_LENG 0x1 |
Functions | |
| void | mma955xSetSamplingRate (uint32 samplePeriod) |
| isf_status_t | fsl_955x_spi_slave_init (void) |
| isf_status_t | fsl_955x_spi_slave_write_preprocess (void *pCmdOut, uint32 offset, uint32 size, void *pWritebuffer) |
| isf_status_t | fsl_955x_spi_slave_write_postprocess (void *pCmdOut) |
| isf_status_t | fsl_955x_spi_slave_read_preprocess (void *pCmdOut, uint32 offset, uint32 size) |
| isf_status_t | fsl_955x_spi_slave_read_postprocess (void *pCmdOut, void *pDataOut) |
Variables | |
| uint8 | MMA955x_2_ConfigRegisterBuffer [MMA955x_2_CONFIG_REGISTER_SIZE] |
| uint8 | SelectedSampleRate [] = { 0x06, 0x20, 0x0C, 0x01, 0x00 } |
| uint8 | SelectedAFEPriority [] = { 0x01, 0x20, 0x32, 0x01, 0x00 } |
| uint8 | SelectedMBoxPriority [] = { 0x01, 0x20, 0x30, 0x01, 0x00 } |
| const uint8 | SampleRates [] |
| const uint8 | ApplicationPriorities [] |
| const uint8 const | FSRange_2g [] = { 0x06, 0x20, 0x00, 0x01, 0x40 } |
| const uint8 const | FSRange_4g [] = { 0x06, 0x20, 0x00, 0x01, 0x80 } |
| const uint8 const | FSRange_8g [] = { 0x06, 0x20, 0x00, 0x01, 0x00 } |
| const uint8 const | WakeApplication [] = { 0x12, 0x20, 0x06, 0x01, 0x00 } |
| const uint8 const | LegacyMode [] = { 0x18, 0x20, 0x00, 0x01, 0x10 } |
| const uint8 const | NormalMode [] = { 0x18, 0x20, 0x00, 0x01, 0x00 } |
| const uint8 const | SleepApplication [] = { 0x12, 0x20, 0x06, 0x01, 0x01 } |
| const uint8 const | MBoxQRDataXYZ [] = { 0x04, 0x20, 0x2C, 0x0C, 0x06, 0x13, 0x06, 0x12, 0x06, 0x15, 0x06, 0x14, 0x06, 0x17, 0x06, 0x16 } |
| const uint8 const | ReadPedometerData [] = { 0x15, 0x30, 0x00, 0x0C } |
| const uint8 const | ReadPedometerConfiguration [] = { 0x15, 0x10, 0x00, 0x11 } |
| const uint8 const | WritePedometerConfiguration [] = { 0x15, 0x20, 0x00, 0x11 } |
| const mma955x_Command_t const | MMA955x_InitializeSequence [] |
| const mma955x_Command_t const | MMA955x_ConfigureSequence [] |
| const mma955x_Command_t const | MMA955x_StartDataSequence [] |
| const mma955x_Command_t const | MMA955x_StopDataSequence [] |
| const mma955x_Command_t const | MMA955x_ShutdownDataSequence [] |
| const mma955x_Command_t const | MMA955x_ReadConfigurationSequence [] |
| const mma955x_Command_t const | MMA955x_WriteConfigurationSequence [] |
| const mma955x_Command_t const | MMA955x_ReadPeadometerDataSequence [] |
| mma955x_Sensor_Specific_Settings_t | MMA955x_2_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MMA955x_2_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| spi_master_slaveInfo_t | fsl_spi_sensor_type_MMA955x_2 |
| const spi_master_CommSpecificInfo_t | MMA955x_2_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
Definition in file MMA955x_2.c.