![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "I2C1.h"#include <isf_sensor_types.h>#include <isf_fifo.h>#include <isf_pressure_types.h>#include "mpl3115.h"#include "fsl_mpl3115_i2c_1D_press.h"#include "fsl_i2c_master_driver.h"#include "Cpu.h"

Go to the source code of this file.
Macros | |
| #define | MPL3115_1_DATA_TYPE mpl3115_DataBuffer_t |
Variables | |
| mpl3115_Sensor_Specific_Settings_t | MPL3115_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MPL3115_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MPL3115_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
Definition in file MPL3115_1.h.