![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "RLI1.h"#include "isf_util.h"#include "fsl_gpio_driver.h"#include "isf_spi_master_types.h"
Go to the source code of this file.
Macros | |
| #define | RLI1_TASK_NAME "RLI1_task" |
| #define | RLI1_TASK_STACK_SIZE 1280 |
| #define | RLI1_TASK_PRIORITY 12 |
Functions | |
| OSA_TASK_DEFINE (RLI1, RLI1_TASK_STACK_SIZE) | |
| void | rli_app_task (void) |
| void | RLI1_MainTask (os_task_param_t task_init_data) |
| void | RLI1_init (void) |
| isf_status_t | rli_spi_slave_init (void) |
| isf_status_t | rli_spi_slave_write_preprocess (void *pCmdOut, uint32 offset, uint32 size, void *pWritebuffer) |
| isf_status_t | rli_spi_slave_write_postprocess (void *pCmdOut) |
| isf_status_t | rli_spi_slave_read_preprocess (void *pCmdOut, uint32 offset, uint32 size) |
| isf_status_t | rli_spi_slave_read_postprocess (void *pCmdOut, void *pDataOut) |
| spi_master_CommSpecificInfo_t | rli_spi_get_config (uint16 spiAddress) |
Variables | |
| spi_master_slaveInfo_t | rli_spi_sensor_type |
| gpio_output_pin_user_config_t | gpioX_OutConfig0 [] |
| const spi_master_CommSpecificInfo_t | RLI_SPI_DeviceInfo |
Definition in file RLI1.c.