![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Command interpreter source file that implements the legacy mailbox protocol functionality. More...
#include "isf.h"#include "isf_ci.h"#include "isf_ci_protocol.h"#include "task_ci.h"#include "ci_protocol_mbox.h"#include "crc.h"
Go to the source code of this file.
Data Structures | |
| struct | ci_mbox_app_info_t |
Macros | |
| #define | MBOX_APP_DATA "MBOX App" |
Functions | |
| ci_status_t | isf_ci_qr_update (uint8 aAppId, int8 anumBytes, uint8 *apSrc) |
| This API updates the Quick-Read mailboxes. More... | |
| uint32 | isf_ci_app_read (uint8 aAppId, uint32 anumBytes, uint8 *apDst) |
| This API reads data from the host via the mailboxes. More... | |
| uint32 | isf_ci_app_write (uint8 aAppId, uint32 anumBytes, uint8 *apSrc) |
| This API writes data to the host via the mailboxes. More... | |
| void | ci_update_first_data_mb (void) |
| Finds the first mailbox available for data pay load, how many mailboxes are available for data pay load, and updates a bit mask that tracks which of the 32 mailboxes are used for quick read. More... | |
| ci_response_enum | ci_qr_update (uint32 mb_read_bits) |
| Based upon mailbox bit mask, invoke the application's command interpreter callback to to update quick read mailboxes. More... | |
| isf_status_t | ci_mbox_init (uint8 aprotocolID, void *apInitData) |
| ci_response_t | isf_app_callback_mbox (ci_host_cmd_packet_t *apHostPacket, ci_app_resp_packet_t *apAppPacket) |
| Callback function for mailbox application ID, ISF_APP_ID_MBOX. More... | |
| ci_response_t | isf_app_callback_dev_info (ci_host_cmd_packet_t *apHostPacket, ci_app_resp_packet_t *apAppPacket) |
| Callback function for the device info command, ISF_APP_ID_DEV_INFO. More... | |
| isf_status_t | ci_protocol_CB_mbox (uint32 anumBytes, uint8 *apSrc, uint32 *apnumDestBytes, uint8 *apDest) |
Variables | |
| ci_funcp_t | ci_callback [] |
| Command interpreter callbacks. The array index is the application ID. More... | |
Command interpreter source file that implements the legacy mailbox protocol functionality.
Definition in file ci_protocol_mbox.c.
| #define MBOX_APP_DATA "MBOX App" |
Definition at line 27 of file ci_protocol_mbox.c.
| isf_status_t ci_mbox_init | ( | uint8 | aprotocolID, |
| void * | apInitData | ||
| ) |
Definition at line 528 of file ci_protocol_mbox.c.
References _fw_device_info_get(), qr_config_t::appId, qr_config_t::byte_id, ci_callback, CI_PROTOCOL_ID_INDEX, ci_update_first_data_mb(), ci_regs_t::ciCtrlReg, isf_ci_app_write(), ISF_ERR_LIB_INIT, ISF_SUCCESS, MAX_ISF_APPLICATIONS, MAX_NUM_MAILBOXES, ci_regs_t::qr_config, and ci_ctrl_reg_t::reg.

| isf_status_t ci_protocol_CB_mbox | ( | uint32 | anumBytes, |
| uint8 * | apSrc, | ||
| uint32 * | apnumDestBytes, | ||
| uint8 * | apDest | ||
| ) |
Definition at line 795 of file ci_protocol_mbox.c.
References ci_host_cmd_packet_t::appId, ci_host_cmd_packet_t::byte_cnt, ci_app_resp_packet_t::bytes_left, ci_app_resp_packet_t::bytes_xfer, ccitt_crc16_cal(), ci_callback, CI_CMD_DEBUG_LOOPBACK, CI_CMD_LAST, CI_CMD_READ_VERSION, CI_CMD_RESET_APP, CI_CMD_UPDATE_QUICKREAD, CI_CMD_WRITE_CONFIG, CI_CMD_WRITE_SREC_FLASH, CI_ERROR_CB_NOT_REGISTERED, CI_ERROR_COMMAND, CI_ERROR_INVALID_LENGTH, CI_ERROR_NONE, CI_ERROR_PARAM, ci_get_first_mailbox, ci_get_wr_appid, ci_get_wr_cmd, ci_get_wr_cmdId, ci_get_wr_cnt, ci_get_wr_offset, ci_insert_crc, CI_INVALID_COUNT, CI_PROTOCOL_DATA_OFFSET, CI_PROTOCOL_ID_SIZE, CI_RW_NULL, ci_send_packet(), ci_host_cmd_packet_t::cmd, CMD_PACKET_BITS, COCO_BIT_MASK, FIRST_DATA_MAILBOX_NUM, ISF_SUCCESS, MAX_NUM_MAILBOXES, MB_APP_RESP_SIZE, MB_HOST_CMD, MB_HOST_CMD_SIZE, MB_RESP_APP_ID, MB_RESP_BYTES_XFER, MB_RESP_COUNT, MB_RESP_STATUS_CC, MBOX_CRC_BYTE_SIZE, ci_host_cmd_packet_t::offset, and ci_app_resp_packet_t::rw.

| ci_response_enum ci_qr_update | ( | uint32 | mb_read_bits | ) |
Based upon mailbox bit mask, invoke the application's
command interpreter callback to to update quick read mailboxes.
| (in) | mb_read_bits - Bit setting that indicates if a mailbox has been read. The corresponding mailbox quick read configuration is examined and its callback is invoked with command to update quick read registers. Each bit corresponds with each of the 32 mailboxes. |
A bit that is set indicates that the corresponding
mailbox has been read.
Definition at line 436 of file ci_protocol_mbox.c.
References APP_ID_NULL, qr_config_t::appId, ci_host_cmd_packet_t::appId, ci_host_cmd_packet_t::byte_cnt, ci_callback, CI_CMD_UPDATE_QUICKREAD, CI_ERROR_NONE, ci_host_cmd_packet_t::cmd, FIRST_QR_MAILBOX_NUM, ISF_APP_ID_NULL, ci_host_cmd_packet_t::offset, and ci_regs_t::qr_config.
Referenced by isf_app_callback_mbox().

| void ci_update_first_data_mb | ( | void | ) |
Finds the first mailbox available for data pay load, how many
mailboxes are available for data pay load, and updates a bit mask
that tracks which of the 32 mailboxes are used for quick read.
Definition at line 336 of file ci_protocol_mbox.c.
References APP_ID_NULL, qr_config_t::appId, FIRST_DATA_MAILBOX_NUM, FIRST_QR_MAILBOX_NUM, NUM_QR_MAILBOXES, and ci_regs_t::qr_config.
Referenced by ci_mbox_init(), and isf_app_callback_mbox().

| ci_response_t isf_app_callback_dev_info | ( | ci_host_cmd_packet_t * | apHostPacket, |
| ci_app_resp_packet_t * | apAppPacket | ||
| ) |
Callback function for the device info command, ISF_APP_ID_DEV_INFO.
| packet_ptr | - host command packet |
| mb_data_ptr | - pointer to first mailbox address containing data. |
Definition at line 768 of file ci_protocol_mbox.c.
References _fw_device_info_get(), ci_host_cmd_packet_t::appId, ci_app_resp_packet_t::bytes_left, ci_app_resp_packet_t::bytes_xfer, CI_ERROR_NONE, CI_RW_WRITE, isf_ci_app_write(), and ci_app_resp_packet_t::rw.

| ci_response_t isf_app_callback_mbox | ( | ci_host_cmd_packet_t * | apHostPacket, |
| ci_app_resp_packet_t * | apAppPacket | ||
| ) |
Callback function for mailbox application ID, ISF_APP_ID_MBOX.
This function is the mailbox application callback.
| packet_ptr | - host command packet |
| mb_data_ptr | - pointer to first mailbox address containing data. |
Definition at line 620 of file ci_protocol_mbox.c.
References ci_host_cmd_packet_t::appId, ci_host_cmd_packet_t::byte_cnt, ci_app_resp_packet_t::bytes_left, ci_app_resp_packet_t::bytes_xfer, CI_CMD_READ_APP_DATA, CI_CMD_READ_CONFIG, CI_CMD_READ_VERSION, CI_CMD_RESET_APP, CI_CMD_UPDATE_QUICKREAD, CI_CMD_WRITE_CONFIG, CI_ERROR_COMMAND, CI_ERROR_INVALID_LENGTH, CI_ERROR_NONE, CI_INVALID_COUNT, ci_qr_update(), CI_RW_NULL, CI_RW_READ, CI_RW_WRITE, ci_update_first_data_mb(), ci_regs_t::ciCtrlReg, ci_host_cmd_packet_t::cmd, isf_ci_app_read(), isf_ci_app_write(), ci_host_cmd_packet_t::offset, ci_regs_t::qr_config, qr_config_clear, ci_ctrl_reg_t::reg, and ci_app_resp_packet_t::rw.

This API reads data from the host via the mailboxes.
This API function is called by an application that reads data from the host in response to a host command.
| [in] | aAppId | ID of the application reading data from the host. |
| [in] | anumBytes | The number of bytes to read from the mailboxes. The range is 1 to 28. |
| [in] | apDst | Pointer to the destination where the data is to be stored. |
Definition at line 226 of file ci_protocol_mbox.c.
References ISF_SUCCESS.
Referenced by App1_ci_app_callback(), BasicApp1_CI_Callback(), isf_app_callback_mbox(), and rli_ci_app_callback().

This API writes data to the host via the mailboxes.
This API function is called by an application that sends data to the host in response to a host command. Data is sent to the host via the mailboxes.
| [in] | aAppId | ID of application writing data to the host. |
| [in] | anumBytes | The number of bytes to write to the mailboxes. The range is 1 to 28. |
| [in] | apSrc | Pointer to the source of the data to write to the host. |
Definition at line 277 of file ci_protocol_mbox.c.
References ISF_SUCCESS, and MAX_NUM_OUT_BUFFER.
Referenced by App1_ci_app_callback(), BasicApp1_CI_Callback(), ci_mbox_init(), isf_app_callback_dev_info(), isf_app_callback_mbox(), and rli_ci_app_callback().

| ci_status_t isf_ci_qr_update | ( | uint8 | aAppId, |
| int8 | anumBytes, | ||
| uint8 * | apSrc | ||
| ) |
This API updates the Quick-Read mailboxes.
This API function is called by an application to write data to the host via the mailboxes designated as Quick-Read for that application. The host must configure the mailboxes for Quick-Read by configuring the mailbox application. The host reads these Quick-Read mailboxes directly without sending a command to the CI.
| [in] | aAppId | ID of the application writing data to the mailboxes for the host. |
| [in] | anumBytes | The number of bytes to write to the mailboxes. The range is 1 to 28. |
| [in] | apSrc | Pointer to the source of the data to write to the mailboxes designated as Quick-Read for the application specified in appId. |
| ISF_SUCCESS | The Quick-Read update completed successfully. |
| ISF_CI_FAILURE | A timeout error occurred while waiting for the mailboxes to be free for updates. |
Definition at line 100 of file ci_protocol_mbox.c.
References qr_config_t::appId, ci_ctrl_reg_t::Bits, ci_ctrl_reg_t::blockTransferMode, qr_config_t::byte_id, ccitt_crc16_cal(), ci_insert_crc, CI_PROTOCOL_DATA_OFFSET, CI_PROTOCOL_ID_SIZE, CI_RESP_QUICKREAD, ci_send_packet(), CI_STREAMING_MODE, ci_regs_t::ciCtrlReg, FIRST_QR_MAILBOX_NUM, ISF_CI_FAILURE, ISF_SUCCESS, MAX_NUM_MAILBOXES, MB_APP_RESP_SIZE, MB_RESP_INDEX_APP_ID, MB_RESP_INDEX_BYTES_XFER, MB_RESP_INDEX_COUNT, MB_RESP_INDEX_STATUS_CC, MBOX_CRC_BYTE_SIZE, NUM_QR_MAILBOXES, and ci_regs_t::qr_config.
Referenced by App1_ci_app_callback(), and App1_MainTask().