![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|

Files | |
| file | Ac_Fixed_utils.h [code] |
| file | isf.h [code] |
| Main ISF header file. Contains code common to all ISF components. | |
| file | isf_bm.h [code] |
| API definitions, types, and macros for the Intelligent Sensing Framework (ISF) Bus Manager (BM). | |
| file | isf_ci.h [code] |
| API definitions, types, and macros for the Intelligent Sensing Framework (ISF) Command Interpreter (CI). | |
| file | isf_comm.h [code] |
| isf_comm.h defines the common types for the Communications Service Family of the Intelligent Sensing Framework (ISF). | |
| file | isf_devmsg.h [code] |
| isf_devmsg.h defines the API definitions and types for the Intelligent Sensing (ISF) Device Messaging (DM) component. | |
| file | isf_dsa_adapter.h [code] |
| file | isf_dsa_direct.h [code] |
| file | isf_dsa_direct_types.h [code] |
| file | isf_dsa_utils.h [code] |
| file | isf_fifo.h [code] |
| file | isf_init.h [code] |
| The isf_init.h file contains the task initialization attributes required for initialization of the following ISF tasks: . | |
| file | isf_pm.h [code] |
| isf_pm.h describes the API definitions, types, and macros for the Intelligent Sensing Framework (ISF) Power Manager (PM). | |
| file | isf_sensor_configuration.h [code] |
| The isf_sensor_configuration.h contains the enumerated list of Digital Sensor Abstraction (DSA) sensor drivers and the external declarations of the currently supported sensor drivers. | |
| file | isf_sensor_configuration_extern.h [code] |
| The isf_sensor_configuration_extern.h contains external declarations referenced by the Sensor Manager for the Digital Sensor Abstration (DSA) implementation. | |
| file | isf_sensor_types.h [code] |
| The isf_sensor_types.h contains the enumerated list of sensor types used by ISF. | |
| file | isf_sm_api.h [code] |
| The isf_sm_api.h contains the collection of APIs for the Sensor Manager as well as related defines and data structures required. | |
| file | isf_sm_types.h [code] |
| The isf_sm_types.h contains the collection of type definitions used in the Sensor Manager Interface as well as related defines and data structures required. | |
| file | isf_sysconf_comms_extern.h [code] |
| System Communications channel configuration. | |
| file | isf_systick_defs.h [code] |
| Register definitions for accessing the standard ARM SYSTICK-related registers. | |
| file | isf_target.h [code] |
| ISF board support header files. | |
| file | isf_types.h [code] |
| The isf_types.h file contains the ISF data type definitions and some of the globally used macros. | |
| file | isf_user_config.h [code] |
| The isf_user_config.h file contains the user configurable settings to either include or exclude an ISF component. | |
| file | isf_util.h [code] |
| The isf_util.h file contains the utility method declarations and macros. | |
| file | version.h [code] |
| Device and ISF Version information. | |