![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The fsl_fxas21002_i2cspi_3D_gyro.h file contains the definitions and functions supporting the FXAS21002 Sensor Adapter. More...


Go to the source code of this file.
Data Structures | |
| struct | fxas21002_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
| struct | fxas21002_ODR_Table_tag |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation. More... | |
| struct | fxas21000_ODR_Table_tag |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21000 operation. More... | |
| struct | fxas21002_ConfigTable_tag |
| the structure defines the configuration table. More... | |
Macros | |
| #define | FXAS21002_WHO_AM_I_VALUE_PRE_RELEASE 0xD6 |
| Define the WHO_AM_I register values for both possible sensor variations. More... | |
| #define | FXAS21002_WHO_AM_I_VALUE_RELEASE 0xD7 |
| #define | FXAS21000_WHO_AM_I_VALUE 0xD1 |
Typedefs | |
| typedef int32 | fxas21002_Status_t |
| FXAS21002 internal return codes. More... | |
| typedef enum fxas21002_Power_tag | fxas21002_Power_t |
| Enumeration for the FXAS21002 power modes. More... | |
| typedef enum fxas21002_InternalState_tag | fxas21002_InternalState_t |
| Enumeration for the FXAS21002 driver internal states. More... | |
| typedef enum fxas21002_Range_tag | fxas21002_Range_t |
| typedef struct fxas21002_ODR_Table_tag | fxas21002_ODR_Table_t |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation. More... | |
| typedef struct fxas21000_ODR_Table_tag | fxas21000_ODR_Table_t |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21000 operation. More... | |
| typedef struct fxas21002_ConfigTable_tag | fxas21002_ConfigTable_t |
| the structure defines the configuration table. More... | |
Enumerations | |
| enum | fxas21002_Error_tag { FXAS21002_ERROR_WHOAMI = 1, FXAS21002_ERROR_WAITFORACTIVE, FXAS21002_ERROR_BURSTWRITE, FXAS21002_ERROR_CONFIG, FXAS21002_ERROR_SETPOWER, FXAS21002_ERROR_WRITE, FXAS21002_ERROR_READ } |
| Enumeration for the FXAS21002 internal error codes. More... | |
| enum | fxas21002_Power_tag { FXAS21002_POWER_STANDBY = 0, FXAS21002_POWER_ACTIVE = 1 } |
| Enumeration for the FXAS21002 power modes. More... | |
| enum | fxas21002_InternalState_tag { FXAS21002_STATE_UNINTIALIZED, FXAS21002_STATE_INITIALIZED, FXAS21002_STATE_CONFIGURED, FXAS21002_STATE_STARTED } |
| Enumeration for the FXAS21002 driver internal states. More... | |
| enum | fxas21002_Range_tag { FXAS21002_RANGE_2000DPS = 0, FXAS21002_RANGE_1000DPS = 1, FXAS21002_RANGE_500DPS = 2, FXAS21002_RANGE_MAX = FXAS21002_RANGE_2000DPS } |
Functions | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Initialize (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter initialization. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSubSettings) |
| This is the concrete implementation of the FXAS21002 sensor adapter for validating current settings. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXAS21002 sensor adapter for configuration. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_StartData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter for start Data. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_EndData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter for End Data. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| This is the concrete implementation of the FXAS21002 sensor adapter for calibration . More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter for shutdown . More... | |
| void | fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback (void *pSensorHandle) |
| The callback function for the Bus Manager(BM). More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
Variables | |
| isf_SensorTypes_t | fxas21002_SupportedSensorTypes [] |
| Supported sensor and data types for MMA8652. More... | |
| isf_SensorDataTypes_t | fxas21002_SupportedDataTypes [] |
The fsl_fxas21002_i2cspi_3D_gyro.h file contains the definitions and functions supporting the FXAS21002 Sensor Adapter.
Definition in file fsl_fxas21002_i2cspi_3D_gyro.h.