![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <isf.h>#include <isf_types.h>#include <isf_sm_api.h>#include <isf_dsa_adapter.h>#include <isf_bm.h>#include <isf_sensor_types.h>#include <isf_fifo.h>#include <isf_pedometer_types.h>#include <isf_comm.h>#include <isf_util.h>#include <isf_sensors.h>#include "fxlc95000.h"#include "fsl_fxlc95000_i2cspi_pedo.h"#include "Ac_Fixed_utils.h"
Go to the source code of this file.
Macros | |
| #define | CI_READ_WRITE_MAX_LEN 32 |
| #define | CI_READ_WRITE_HDR_LEN 6 |
| #define | CI_READ_WRITE_ADDR_LEN 2 |
Variables | |
| isf_SensorTypes_t | fxlc95000_SupportedSensorTypes [] = { TYPE_ACCELEROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
| Supported sensor and data types. More... | |
| isf_SensorDataTypes_t | fxlc95000_SupportedDataTypes [] = { TYPE_RAW_ACCELERATION_3D, TYPE_NATIVE_SENSOR_DATA_TYPE } |
| #define CI_READ_WRITE_ADDR_LEN 2 |
Referenced by fsl_fxlc95000_Flash().
| #define CI_READ_WRITE_HDR_LEN 6 |
Referenced by fsl_fxlc95000_Flash().
| #define CI_READ_WRITE_MAX_LEN 32 |
Referenced by fsl_fxlc95000_Flash().
| int32 fxlc95000_GetConfig | ( | isf_SensorHandle_t * | pSensorHandle, |
| fxlc95000_appConfigRegister_t * | pConfig | ||
| ) |
Definition at line 760 of file fsl_fxlc95000_i2cspi_pedo.c.
References fxlc95000_Sensor_Specific_Settings_t::configRegisterReadOffset, fxlc95000_Sensor_Specific_Settings_t::configRegisterReadSize, fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_read(), fxlc95000_send(), fxlc95000_CommandList_t::numCommands, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, fxlc95000_Sensor_Specific_Settings_t::readConfigCommands, and SENSOR_ERROR_GETDATA.
Referenced by fsl_fxlc95000_Configure().


| int32 fxlc95000_GetData | ( | int32_t * | status, |
| isf_SensorHandle_t * | pSensorHandle, | ||
| void * | pBuffer | ||
| ) |
This function retrieves the raw data from the MAG3110 sensor.
Definition at line 741 of file fsl_fxlc95000_i2cspi_pedo.c.
References fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_read(), isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, fxlc95000_Sensor_Specific_Settings_t::sampleDataOffset, fxlc95000_Sensor_Specific_Settings_t::sampleDataSize, and SENSOR_ERROR_GETDATA.
Referenced by fsl_fxlc95000_PeriodicCallback().


| int32 fxlc95000_read | ( | dm_DeviceDescriptor_t * | pDeviceHandle, |
| int32 | offset, | ||
| int32 | numBytes, | ||
| uint8 * | pBuffer | ||
| ) |
Definition at line 819 of file fsl_fxlc95000_i2cspi_pedo.c.
References dm_channel_acquire_lock(), dm_channel_release_lock(), dm_device_read(), ISF_SUCCESS, and dm_DeviceDescriptor_struct::pChannelDescriptor.
Referenced by fxlc95000_GetConfig(), and fxlc95000_GetData().


| int32 fxlc95000_send | ( | dm_DeviceDescriptor_t * | pDeviceHandle, |
| const fxlc95000_CommandList_t * | aCommandList | ||
| ) |
Definition at line 833 of file fsl_fxlc95000_i2cspi_pedo.c.
References fxlc95000_CommandList_t::commands, dm_channel_acquire_lock(), dm_channel_release_lock(), dm_device_write(), fxlc95000_waitForCoCo(), ISF_SUCCESS, fxlc95000_Command_t::nByteWrite, fxlc95000_CommandList_t::numCommands, fxlc95000_Command_t::offset, dm_DeviceDescriptor_struct::pChannelDescriptor, and fxlc95000_Command_t::pWriteBuffer.
Referenced by fsl_fxlc95000_Configure(), fsl_fxlc95000_EndData(), fsl_fxlc95000_Flash(), fsl_fxlc95000_Shutdown(), fsl_fxlc95000_StartData(), fxlc95000_GetConfig(), and fxlc95000_ValidateConfig().


| void fxlc95000_ValidateConfig | ( | int32_t * | status, |
| isf_SensorHandle_t * | pSensorHandle, | ||
| isf_dsa_SensorSettings_t * | pSubSettings | ||
| ) |
This function validates the configuration for the MAG3110 sensor.
Definition at line 722 of file fsl_fxlc95000_i2cspi_pedo.c.
References fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_send(), ISF_SUCCESS, fxlc95000_CommandList_t::numCommands, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and fxlc95000_Sensor_Specific_Settings_t::validateSettingsCommands.
Referenced by fsl_fxlc95000_ValidateSettings().


| uint8 fxlc95000_waitForCoCo | ( | dm_DeviceDescriptor_t * | pDeviceHandle | ) |
Definition at line 864 of file fsl_fxlc95000_i2cspi_pedo.c.
References dm_device_read(), and ISF_SUCCESS.
Referenced by fxlc95000_send().


| int32 fxlc95000_WriteConfig | ( | isf_SensorHandle_t * | pSensorHandle, |
| fxlc95000_appConfigRegister_t * | pConfig | ||
| ) |
Definition at line 783 of file fsl_fxlc95000_i2cspi_pedo.c.
References fxlc95000_CommandList_t::commands, fxlc95000_Sensor_Specific_Settings_t::configRegisterReadSize, fxlc95000_DeviceDescriptor_t::deviceHandle, dm_channel_acquire_lock(), dm_channel_release_lock(), dm_device_write(), ISF_SUCCESS, fxlc95000_Command_t::nByteWrite, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, fxlc95000_Command_t::pWriteBuffer, SENSOR_ERROR_GETDATA, and fxlc95000_Sensor_Specific_Settings_t::writeConfigRegisterPreamble.
Referenced by fsl_fxlc95000_Configure().