![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The FXLS8952 Sensor Adapter for the 3-axis consumer accelerometer that supports I2C protocol. More...
#include <isf.h>#include <isf_types.h>#include <isf_sm_api.h>#include <isf_dsa_adapter.h>#include <isf_bm.h>#include <isf_sensor_types.h>#include <isf_fifo.h>#include <isf_accelerometer_types.h>#include <isf_comm.h>#include <isf_util.h>#include <isf_sensors.h>#include "fxls8952.h"#include "fsl_os_abstraction.h"#include "isf_eventhandler.h"#include "fsl_fxls8952_i2c_3D_accel.h"
Go to the source code of this file.
Macros | |
| #define | FXLS8952_ACCEL_FLOAT_CONVERSION_FACTOR (0.1) |
| #define | FXLS8952_ACCEL_FLOAT_CONVERSION_OFFSET (0.0) |
| #define | FXLS8952_ACCEL_FIXED_CONVERSION_FACTOR (1638) |
| #define | FXLS8952_ACCEL_FIXED_CONVERSION_OFFSET (0) |
| #define | MAX_ACCEL_FULL_SCALE_RANGE FXLS8952_RANGE_MAX |
| #define | FXLS8952_SAMPLE_PERIOD_MAX 1280409 |
| #define | FXLS8952_SAMPLE_PERIOD_MIN 312 |
| #define | GET_ODR_CONFIG 0x0 |
| #define | GET_ODR_VALUE 0x01 |
| #define | NUM_STATUS_BYTES 1 |
| #define | NUMBER_OF_AXES_3D 0x3 |
| #define | MAX_NUM_AXES 0x3 |
| #define | MAX_FXLS8952_DM_BYTES 0x30 |
| #define | NUM_INTERNAL_ADDRESS_BYTES 0x1 |
| #define | ASSIGN_REG_BITS_VALUE(addr, val, mask, shift) (addr) = (((addr) & ~ (mask)) | (((val) << shift)& (mask)) ) |
| #define | GET_MODE(mode) ((mode) <= FXLS8952_MODE_HYBRID) ? (mode) : FXLS8952_MODE_HYBRID |
| #define | GET_STRUCT_MEMBER_ADDRESS(p, m) (&(p)->m) |
| #define | GET_MEMBER_SIZE(p, m) sizeof((p)->m) |
Functions | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Initialize (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter initialization. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXLS8952 sensor adapter for validating current settings. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXLS8952 sensor adapter for configuration. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_StartData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for start Data. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_EndData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for End Data. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| This is the concrete implementation of the FXLS8952 sensor adapter for calibration . More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for shutdown . More... | |
| void | fsl_fxls8952_i2c_3D_accel_PeriodicCallback (void *pSensorHandle) |
| The callback function for the Bus Manager(BM). More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
Variables | |
| uint8 | LE_BE_check =0 |
| isf_SensorTypes_t | fxls8952_SupportedSensorTypes [] = { TYPE_ACCELEROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
| Supported sensor and data types for FXLS8952. More... | |
| isf_SensorDataTypes_t | fxls8952_SupportedDataTypes [] = { TYPE_RAW_ACCELERATION_3D , TYPE_NATIVE_SENSOR_DATA_TYPE } |
| const fxls8952_ODR_Table_t | fxls8952_odrTable [] |
| The table that describes the configuration value based on ODR (output data rate). Note: This table is irregular after the 25HZ, so can't use FLOORLOG2 algorithm. More... | |
| struct { | |
| float floatFactor | |
| float floatOffset | |
| int32 fixedFactor | |
| int32 fixedOffset | |
| } | fxls8952AccelConvTable [] |
The FXLS8952 Sensor Adapter for the 3-axis consumer accelerometer that supports I2C protocol.
File: fsl_FXLS8952_i2c_3D_accel.c
Copyright (c) 2015, Freescale Semiconductor, Inc.
Definition in file fsl_fxls8952_i2c_3D_accel.c.