![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The fsl_fxls8952_i2c_3D_accel.h file contains the definitions and functions supporting the FXLS8952 Sensor adapter header file. More...


Go to the source code of this file.
Data Structures | |
| struct | fxls8952_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
| struct | fxls8952_ODR_Table_tag |
| the structure defines the ODR table between Hybrid and normal mode of device operation. More... | |
| struct | fxls8952_ConfigTable_tag |
| the structure defines the configuration table. More... | |
Macros | |
| #define | FXLS8952_WHO_AM_I_VALUE 0x18 |
Typedefs | |
| typedef int32 | fxls8952_Status_t |
| fxls8952 internal return codes. More... | |
| typedef enum fxls8952_Power_tag | fxls8952_Power_t |
| Enumeration for the fxls8952 power modes. More... | |
| typedef enum fxls8952_InternalState_tag | fxls8952_InternalState_t |
| Enumeration for the fxls8952 driver internal states. More... | |
| typedef enum fxls8952_Range_tag | fxls8952_Range_t |
| typedef struct fxls8952_ODR_Table_tag | fxls8952_ODR_Table_t |
| the structure defines the ODR table between Hybrid and normal mode of device operation. More... | |
| typedef struct fxls8952_ConfigTable_tag | fxls8952_ConfigTable_t |
| the structure defines the configuration table. More... | |
Enumerations | |
| enum | fxls8952_Error_tag { FXLS8952_ERROR_WHOAMI = 1, FXLS8952_ERROR_WAITFORACTIVE, FXLS8952_ERROR_BURSTWRITE, FXLS8952_ERROR_CONFIG, FXLS8952_ERROR_SETPOWER, FXLS8952_ERRO_WRITE, FXLS8952_ERRO_READ } |
| Enumeration for the fxls8952 internal error codes. More... | |
| enum | fxls8952_Power_tag { FXLS8952_POWER_STANDBY = 0, FXLS8952_POWER_ACTIVE = 1 } |
| Enumeration for the fxls8952 power modes. More... | |
| enum | fxls8952_InternalState_tag { FXLS8952_STATE_UNINTIALIZED, FXLS8952_STATE_INITIALIZED, FXLS8952_STATE_CONFIGURED, FXLS8952_STATE_STARTED } |
| Enumeration for the fxls8952 driver internal states. More... | |
| enum | fxls8952_Range_tag { FXLS8952_RANGE_2G = 0, FXLS8952_RANGE_4G = 1, FXLS8952_RANGE_8G = 2, FXLS8952_RANGE_16G = 3, FXLS8952_RANGE_MAX = FXLS8952_RANGE_16G } |
Functions | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Initialize (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter initialization. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXLS8952 sensor adapter for validating current settings. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXLS8952 sensor adapter for configuration. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_StartData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for start Data. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_EndData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for End Data. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| This is the concrete implementation of the FXLS8952 sensor adapter for calibration . More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for shutdown . More... | |
| void | fsl_fxls8952_i2c_3D_accel_PeriodicCallback (void *pSensorHandle) |
| The callback function for the Bus Manager(BM). More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
Variables | |
| isf_SensorTypes_t | fxls8952_SupportedSensorTypes [] |
| Supported sensor and data types for MMA8652. More... | |
| isf_SensorDataTypes_t | fxls8952_SupportedDataTypes [] |
The fsl_fxls8952_i2c_3D_accel.h file contains the definitions and functions supporting the FXLS8952 Sensor adapter header file.
Definition in file fsl_fxls8952_i2c_3D_accel.h.