![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The fxas21002.h file contains the FXAS21002 Magnetometer register definitions, access macros, and device access functions. More...
#include "isf.h"#include <isf_types.h>#include <isf_devmsg.h>#include <isf_bm.h>#include <isf_sm_api.h>#include <isf_dsa_adapter.h>

Go to the source code of this file.
Data Structures | |
| struct | gyro_config_t |
| The structure defines the FXAS21002 configuration. More... | |
| struct | fxas21002_Sensor_Specific_Reg_t |
| struct | fxas21002_Sensor_Specific_Settings_t |
Typedefs | |
| typedef int32 | fxas21002_status_t |
Enumerations | |
| enum | { FXAS21002_STATUS = 0x00, FXAS21002_OUT_X_MSB = 0x01, FXAS21002_OUT_X_LSB = 0x02, FXAS21002_OUT_Y_MSB = 0x03, FXAS21002_OUT_Y_LSB = 0x04, FXAS21002_OUT_Z_MSB = 0x05, FXAS21002_OUT_Z_LSB = 0x06, FXAS21002_DR_STATUS = 0x07, FXAS21002_F_STATUS = 0x08, FXAS21002_F_SETUP = 0x09, FXAS21002_F_EVENT = 0x0A, FXAS21002_INT_SRC_FLAG = 0x0B, FXAS21002_WHO_AM_I = 0x0C, FXAS21002_CTRL_REG0 = 0x0D, FXAS21002_RT_CFG = 0x0E, FXAS21002_RT_SRC = 0x0F, FXAS21002_RT_THS = 0x10, FXAS21002_RT_COUNT = 0x11, FXAS21002_TEMP = 0x12, FXAS21002_CTRL_REG1 = 0x13, FXAS21002_CTRL_REG2 = 0x14, FXAS21002_CTRL_REG3 = 0x15, FXAS21002_RESERVED = 0x16 } |
| The FXAS21002 Sensor Internal Register Map. More... | |
The fxas21002.h file contains the FXAS21002 Magnetometer register definitions, access macros, and device access functions.
Definition in file fxas21002.h.
| #define FXAS21000_WHOAMI_VALUE (0xD1) |
Definition at line 188 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure(), and fsl_fxas21002_i2cspi_3D_gyro_Initialize().
| #define FXAS21002_ACTIVE_MASK (0x02) |
Definition at line 150 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure().
| #define FXAS21002_ACTIVE_SHIFT 1 |
Definition at line 151 of file fxas21002.h.
| #define FXAS21002_BOOTEND_MASK (0x08) |
Definition at line 116 of file fxas21002.h.
| #define FXAS21002_BOOTEND_SHIFT 3 |
Definition at line 117 of file fxas21002.h.
| #define FXAS21002_BW_MASK (0xC0) |
Definition at line 130 of file fxas21002.h.
| #define FXAS21002_BW_SHIFT 6 |
Definition at line 131 of file fxas21002.h.
| #define FXAS21002_DR_MASK (0x1C) |
Definition at line 148 of file fxas21002.h.
| #define FXAS21002_DR_SHIFT 2 |
Definition at line 149 of file fxas21002.h.
| #define FXAS21002_EXTCTRLEN_MASK (0x04) |
Definition at line 180 of file fxas21002.h.
| #define FXAS21002_EXTCTRLEN_SHIFT 2 |
Definition at line 181 of file fxas21002.h.
| #define FXAS21002_F_EVENT_MASK (0x20) |
Definition at line 108 of file fxas21002.h.
| #define FXAS21002_F_EVENT_SHIFT 5 |
Definition at line 109 of file fxas21002.h.
| #define FXAS21002_F_MODE_MASK (0xC0) |
Definition at line 100 of file fxas21002.h.
| #define FXAS21002_F_MODE_SHIFT 6 |
Definition at line 101 of file fxas21002.h.
| #define FXAS21002_F_OVF_MASK (0x80) |
Definition at line 92 of file fxas21002.h.
| #define FXAS21002_F_OVF_SHIFT 7 |
Definition at line 93 of file fxas21002.h.
| #define FXAS21002_F_WMKF_MASK (0x40) |
Definition at line 94 of file fxas21002.h.
| #define FXAS21002_F_WMKF_SHIFT 6 |
Definition at line 95 of file fxas21002.h.
| #define FXAS21002_F_WMRK_MASK (0x3F) |
Definition at line 102 of file fxas21002.h.
| #define FXAS21002_F_WMRK_SHIFT 0 |
Definition at line 103 of file fxas21002.h.
| #define FXAS21002_FE_TIME_MASK (0x1F) |
Definition at line 110 of file fxas21002.h.
| #define FXAS21002_FE_TIME_SHIFT 0 |
Definition at line 111 of file fxas21002.h.
| #define FXAS21002_FS_MASK (0x02) |
Definition at line 138 of file fxas21002.h.
| #define FXAS21002_FS_SHIFT 0 |
Definition at line 139 of file fxas21002.h.
| #define FXAS21002_FSDOUBLE_MASK (0x01) |
Definition at line 182 of file fxas21002.h.
| #define FXAS21002_FSDOUBLE_SHIFT 0 |
Definition at line 183 of file fxas21002.h.
| #define FXAS21002_GET_FIELD | ( | name, | |
| val | |||
| ) | ((val&FXAS21002_##name##_MASK)>>FXAS21002_##name##_SHIFT) |
Definition at line 67 of file fxas21002.h.
| #define FXAS21002_HPF_EN_MASK (0x04) |
Definition at line 136 of file fxas21002.h.
| #define FXAS21002_HPF_EN_SHIFT 2 |
Definition at line 137 of file fxas21002.h.
| #define FXAS21002_IIC_ADDRESS 0x20 |
Definition at line 22 of file fxas21002.h.
| #define FXAS21002_INT_CFG_DRDY_MASK (0x08) |
Definition at line 166 of file fxas21002.h.
| #define FXAS21002_INT_CFG_DRDY_SHIFT 3 |
Definition at line 167 of file fxas21002.h.
| #define FXAS21002_INT_CFG_FIFO_MASK (0x80) |
Definition at line 158 of file fxas21002.h.
| #define FXAS21002_INT_CFG_FIFO_SHIFT 7 |
Definition at line 159 of file fxas21002.h.
| #define FXAS21002_INT_CFG_RT_MASK (0x20) |
Definition at line 162 of file fxas21002.h.
| #define FXAS21002_INT_CFG_RT_SHIFT 5 |
Definition at line 163 of file fxas21002.h.
| #define FXAS21002_INT_EN_DRDY_MASK (0x04) |
Definition at line 168 of file fxas21002.h.
| #define FXAS21002_INT_EN_DRDY_SHIFT 2 |
Definition at line 169 of file fxas21002.h.
| #define FXAS21002_INT_EN_FIFO_MASK (0x40) |
Definition at line 160 of file fxas21002.h.
| #define FXAS21002_INT_EN_FIFO_SHIFT 6 |
Definition at line 161 of file fxas21002.h.
| #define FXAS21002_INT_EN_RT_MASK (0x10) |
Definition at line 164 of file fxas21002.h.
| #define FXAS21002_INT_EN_RT_SHIFT 4 |
Definition at line 165 of file fxas21002.h.
| #define FXAS21002_IPOL_MASK (0x02) |
Definition at line 170 of file fxas21002.h.
| #define FXAS21002_IPOL_SHIFT 1 |
Definition at line 171 of file fxas21002.h.
| #define FXAS21002_NUMBER_AXIS 3 |
The FXAS21002 registers, masks, and constants.
Definition at line 27 of file fxas21002.h.
| #define FXAS21002_NUMBER_BYTES_AXIS 2 |
Definition at line 28 of file fxas21002.h.
| #define FXAS21002_PP_OD_MASK (0x01) |
Definition at line 172 of file fxas21002.h.
| #define FXAS21002_PP_OD_SHIFT 0 |
Definition at line 173 of file fxas21002.h.
| #define FXAS21002_READY_MASK (0x01) |
Definition at line 152 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure().
| #define FXAS21002_READY_SHIFT 0 |
Definition at line 153 of file fxas21002.h.
| #define FXAS21002_RST_MASK (0x40) |
Definition at line 144 of file fxas21002.h.
| #define FXAS21002_RST_SHIFT 7 |
Definition at line 145 of file fxas21002.h.
| #define FXAS21002_SEL_MASK (0x18) |
Definition at line 134 of file fxas21002.h.
| #define FXAS21002_SEL_SHIFT 3 |
Definition at line 135 of file fxas21002.h.
| #define FXAS21002_SET_FIELD | ( | name, | |
| val | |||
| ) | (((val)<<FXAS21002_##name##_SHIFT)&(FXAS21002_##name##_MASK)) |
Definition at line 66 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure().
| #define FXAS21002_SPIW_MASK (0x20) |
Definition at line 132 of file fxas21002.h.
| #define FXAS21002_SPIW_SHIFT 5 |
Definition at line 133 of file fxas21002.h.
| #define FXAS21002_SRC_DRDY_MASK (0x01) |
Definition at line 122 of file fxas21002.h.
| #define FXAS21002_SRC_DRDY_SHIFT 0 |
Definition at line 123 of file fxas21002.h.
| #define FXAS21002_SRC_FIFO_MASK (0x04) |
Definition at line 118 of file fxas21002.h.
| #define FXAS21002_SRC_FIFO_SHIFT 2 |
Definition at line 119 of file fxas21002.h.
| #define FXAS21002_SRC_RT_MASK (0x02) |
Definition at line 120 of file fxas21002.h.
| #define FXAS21002_SRC_RT_SHIFT 1 |
Definition at line 121 of file fxas21002.h.
| #define FXAS21002_ST_MASK (0x20) |
Definition at line 146 of file fxas21002.h.
| #define FXAS21002_ST_SHIFT 5 |
Definition at line 147 of file fxas21002.h.
| #define FXAS21002_STANDBY_TO_ACTIVE_SAMPLE_WAIT (49) |
Definition at line 194 of file fxas21002.h.
| #define FXAS21002_WHOAMI_VALUE_PRE_RELEASE (0xD6) |
Definition at line 189 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Initialize().
| #define FXAS21002_WHOAMI_VALUE_RELEASE (0xD7) |
Definition at line 190 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Initialize().
| #define FXAS21002_WRAPTOONE_MASK (0x08) |
Definition at line 178 of file fxas21002.h.
| #define FXAS21002_WRAPTOONE_SHIFT 3 |
Definition at line 179 of file fxas21002.h.
| #define FXAS21002_XDR_MASK (0x01) |
Definition at line 86 of file fxas21002.h.
| #define FXAS21002_XDR_SHIFT 0 |
Definition at line 87 of file fxas21002.h.
| #define FXAS21002_XOW_MASK (0x10) |
Definition at line 78 of file fxas21002.h.
| #define FXAS21002_XOW_SHIFT 4 |
Definition at line 79 of file fxas21002.h.
| #define FXAS21002_YDR_MASK (0x02) |
Definition at line 84 of file fxas21002.h.
| #define FXAS21002_YDR_SHIFT 1 |
Definition at line 85 of file fxas21002.h.
| #define FXAS21002_YOW_MASK (0x20) |
Definition at line 76 of file fxas21002.h.
| #define FXAS21002_YOW_SHIFT 5 |
Definition at line 77 of file fxas21002.h.
| #define FXAS21002_ZDR_MASK (0x04) |
Definition at line 82 of file fxas21002.h.
| #define FXAS21002_ZDR_SHIFT 2 |
Definition at line 83 of file fxas21002.h.
| #define FXAS21002_ZOW_MASK (0x40) |
Definition at line 74 of file fxas21002.h.
| #define FXAS21002_ZOW_SHIFT 6 |
Definition at line 75 of file fxas21002.h.
| #define FXAS21002_ZYXDR_MASK (0x08) |
Definition at line 80 of file fxas21002.h.
| #define FXAS21002_ZYXDR_SHIFT 3 |
Definition at line 81 of file fxas21002.h.
| #define FXAS21002_ZYXOW_MASK (0x80) |
Definition at line 72 of file fxas21002.h.
| #define FXAS21002_ZYXOW_SHIFT 7 |
Definition at line 73 of file fxas21002.h.
| #define MAG3100_READ_BUF_SIZE (6) |
Definition at line 186 of file fxas21002.h.
Referenced by mag3110_GetData().
| #define NUMBER_OF_BYTES_TIMESTAMP (4) |
Definition at line 187 of file fxas21002.h.
| typedef int32 fxas21002_status_t |
Definition at line 196 of file fxas21002.h.
| anonymous enum |
The FXAS21002 Sensor Internal Register Map.
Definition at line 34 of file fxas21002.h.