![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The fxls8471.h contains the FXLS8471 Accelerometer register definitions, access macros, and device access functions. More...

Go to the source code of this file.
Data Structures | |
| struct | fxls8471_Sensor_Specific_Reg_t |
| struct | fxls8471_Sensor_Specific_Settings_t |
The fxls8471.h contains the FXLS8471 Accelerometer register definitions, access macros, and device access functions.
Definition in file fxls8471.h.
| #define FXLS8471_A_FFMT_DBCNTM_MASK 0x80 |
Definition at line 276 of file fxls8471.h.
| #define FXLS8471_A_FFMT_DBCNTM_SHIFT 7 |
Definition at line 277 of file fxls8471.h.
| #define FXLS8471_A_FFMT_EA_MASK 0x80 |
Definition at line 258 of file fxls8471.h.
| #define FXLS8471_A_FFMT_EA_SHIFT 7 |
Definition at line 259 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ELE_MASK 0x80 |
Definition at line 245 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ELE_SHIFT 7 |
Definition at line 246 of file fxls8471.h.
| #define FXLS8471_A_FFMT_OAE_MASK 0x40 |
Definition at line 247 of file fxls8471.h.
| #define FXLS8471_A_FFMT_OAE_SHIFT 6 |
Definition at line 248 of file fxls8471.h.
| #define FXLS8471_A_FFMT_THS_MASK 0x7F |
Definition at line 278 of file fxls8471.h.
| #define FXLS8471_A_FFMT_THS_SHIFT 0 |
Definition at line 279 of file fxls8471.h.
| #define FXLS8471_A_FFMT_THS_XYZ_EN_MASK 0x80 |
Definition at line 284 of file fxls8471.h.
| #define FXLS8471_A_FFMT_THS_XYZ_EN_SHIFT 7 |
Definition at line 285 of file fxls8471.h.
| #define FXLS8471_A_FFMT_XEFE_MASK 0x08 |
Definition at line 253 of file fxls8471.h.
| #define FXLS8471_A_FFMT_XEFE_SHIFT 3 |
Definition at line 254 of file fxls8471.h.
| #define FXLS8471_A_FFMT_XHE_MASK 0x02 |
Definition at line 268 of file fxls8471.h.
| #define FXLS8471_A_FFMT_XHE_SHIFT 1 |
Definition at line 269 of file fxls8471.h.
| #define FXLS8471_A_FFMT_XHP_MASK 0x01 |
Definition at line 270 of file fxls8471.h.
| #define FXLS8471_A_FFMT_XHP_SHIFT 0 |
Definition at line 271 of file fxls8471.h.
| #define FXLS8471_A_FFMT_YEFE_MASK 0x10 |
Definition at line 251 of file fxls8471.h.
| #define FXLS8471_A_FFMT_YEFE_SHIFT 4 |
Definition at line 252 of file fxls8471.h.
| #define FXLS8471_A_FFMT_YHE_MASK 0x08 |
Definition at line 264 of file fxls8471.h.
| #define FXLS8471_A_FFMT_YHE_SHIFT 3 |
Definition at line 265 of file fxls8471.h.
| #define FXLS8471_A_FFMT_YHP_MASK 0x04 |
Definition at line 266 of file fxls8471.h.
| #define FXLS8471_A_FFMT_YHP_SHIFT 2 |
Definition at line 267 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ZEFE_MASK 0x20 |
Definition at line 249 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ZEFE_SHIFT 5 |
Definition at line 250 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ZHE_MASK 0x20 |
Definition at line 260 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ZHE_SHIFT 5 |
Definition at line 261 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ZHP_MASK 0x10 |
Definition at line 262 of file fxls8471.h.
| #define FXLS8471_A_FFMT_ZHP_SHIFT 4 |
Definition at line 263 of file fxls8471.h.
| #define FXLS8471_A_VECM_DBCNTM_MASK 0x80 |
Definition at line 452 of file fxls8471.h.
| #define FXLS8471_A_VECM_DBCNTM_SHIFT 7 |
Definition at line 453 of file fxls8471.h.
| #define FXLS8471_A_VECM_ELE_MASK 0x40 |
Definition at line 440 of file fxls8471.h.
| #define FXLS8471_A_VECM_ELE_SHIFT 6 |
Definition at line 441 of file fxls8471.h.
| #define FXLS8471_A_VECM_EN_MASK 0x08 |
Definition at line 446 of file fxls8471.h.
| #define FXLS8471_A_VECM_EN_SHIFT 3 |
Definition at line 447 of file fxls8471.h.
| #define FXLS8471_A_VECM_INITM_MASK 0x20 |
Definition at line 442 of file fxls8471.h.
| #define FXLS8471_A_VECM_INITM_SHIFT 5 |
Definition at line 443 of file fxls8471.h.
| #define FXLS8471_A_VECM_THS_MSB_MASK 0x18 |
Definition at line 454 of file fxls8471.h.
| #define FXLS8471_A_VECM_THS_MSB_SHIFT 0 |
Definition at line 455 of file fxls8471.h.
| #define FXLS8471_A_VECM_UPDM_MASK 0x10 |
Definition at line 444 of file fxls8471.h.
| #define FXLS8471_A_VECM_UPDM_SHIFT 4 |
Definition at line 445 of file fxls8471.h.
| #define FXLS8471_ACTIVE (FXLS8471_ACTIVE_MASK) |
Definition at line 361 of file fxls8471.h.
| #define FXLS8471_ACTIVE_MASK 0x01 |
Definition at line 358 of file fxls8471.h.
| #define FXLS8471_ACTIVE_SHIFT 0 |
Definition at line 359 of file fxls8471.h.
| #define FXLS8471_ASLP_RATE_MASK 0xC0 |
Definition at line 350 of file fxls8471.h.
| #define FXLS8471_ASLP_RATE_SHIFT 6 |
Definition at line 351 of file fxls8471.h.
| #define FXLS8471_AXX_MASK 0x10 |
Definition at line 336 of file fxls8471.h.
| #define FXLS8471_AXY_MASK 0x20 |
Definition at line 335 of file fxls8471.h.
| #define FXLS8471_AXZ_MASK 0x40 |
Definition at line 334 of file fxls8471.h.
| #define FXLS8471_BAFRO_MASK 0x01 |
Definition at line 215 of file fxls8471.h.
| #define FXLS8471_BAFRO_SHIFT 0 |
Definition at line 216 of file fxls8471.h.
| #define FXLS8471_BKFR_MASK 0xC0 |
Definition at line 229 of file fxls8471.h.
| #define FXLS8471_BKFR_SHIFT 6 |
Definition at line 230 of file fxls8471.h.
| #define FXLS8471_DBCNTM_MASK 0x80 |
Definition at line 221 of file fxls8471.h.
| #define FXLS8471_DBCNTM_SHIFT 7 |
Definition at line 222 of file fxls8471.h.
| #define FXLS8471_DPA_MASK 0x80 |
Definition at line 314 of file fxls8471.h.
| #define FXLS8471_DPA_SHIFT 7 |
Definition at line 315 of file fxls8471.h.
| #define FXLS8471_DPE_MASK 0x08 |
Definition at line 337 of file fxls8471.h.
| #define FXLS8471_DR_MASK 0x38 |
Definition at line 352 of file fxls8471.h.
| #define FXLS8471_DR_SHIFT 3 |
Definition at line 353 of file fxls8471.h.
| #define FXLS8471_F_CNT_MASK 0x3F |
Definition at line 124 of file fxls8471.h.
| #define FXLS8471_F_CNT_SHIFT 0 |
Definition at line 125 of file fxls8471.h.
| #define FXLS8471_F_MODE_CIRCULAR 0x01 |
Definition at line 136 of file fxls8471.h.
| #define FXLS8471_F_MODE_DISABLED 0x00 |
Definition at line 135 of file fxls8471.h.
| #define FXLS8471_F_MODE_FILL 0x02 |
Definition at line 137 of file fxls8471.h.
| #define FXLS8471_F_MODE_MASK 0xC0 |
Definition at line 130 of file fxls8471.h.
| #define FXLS8471_F_MODE_SHIFT 6 |
Definition at line 131 of file fxls8471.h.
| #define FXLS8471_F_MODE_TRIGGER 0x03 |
Definition at line 138 of file fxls8471.h.
| #define FXLS8471_F_OVF_MASK 0x80 |
Definition at line 120 of file fxls8471.h.
| #define FXLS8471_F_OVF_SHIFT 7 |
Definition at line 121 of file fxls8471.h.
| #define FXLS8471_F_WMRK_FLAG_MASK 0x40 |
Definition at line 122 of file fxls8471.h.
| #define FXLS8471_F_WMRK_FLAG_SHIFT 6 |
Definition at line 123 of file fxls8471.h.
| #define FXLS8471_F_WMRK_MASK 0x3F |
Definition at line 132 of file fxls8471.h.
| #define FXLS8471_F_WMRK_SHIFT 0 |
Definition at line 133 of file fxls8471.h.
| #define FXLS8471_FGERR_MASK 0x80 |
Definition at line 157 of file fxls8471.h.
| #define FXLS8471_FGERR_SHIFT 7 |
Definition at line 158 of file fxls8471.h.
| #define FXLS8471_FGT_MASK 0x7C |
Definition at line 159 of file fxls8471.h.
| #define FXLS8471_FGT_SHIFT 2 |
Definition at line 160 of file fxls8471.h.
| #define FXLS8471_FIFO_GATE_MASK 0x80 |
Definition at line 381 of file fxls8471.h.
| #define FXLS8471_FIFO_GATE_SHIFT 7 |
Definition at line 382 of file fxls8471.h.
| #define FXLS8471_FREAD_MASK 0x02 |
Definition at line 356 of file fxls8471.h.
| #define FXLS8471_FREAD_SHIFT 1 |
Definition at line 357 of file fxls8471.h.
| #define FXLS8471_FS_MASK 0x03 |
Definition at line 193 of file fxls8471.h.
| #define FXLS8471_FS_SHIFT 0 |
Definition at line 194 of file fxls8471.h.
| #define FXLS8471_GET_FIELD | ( | name, | |
| val | |||
| ) | ((val&FXLS8471_##name##_MASK)>>FXLS8471_##name##_SHIFT) |
Definition at line 97 of file fxls8471.h.
Referenced by fxls8471_GetData().
| #define FXLS8471_HPF_BYP_MASK 0x01 |
Definition at line 297 of file fxls8471.h.
| #define FXLS8471_HPF_BYP_SHIFT 0 |
Definition at line 298 of file fxls8471.h.
| #define FXLS8471_HPF_OUT_MASK 0x10 |
Definition at line 191 of file fxls8471.h.
| #define FXLS8471_HPF_OUT_SHIFT 4 |
Definition at line 192 of file fxls8471.h.
| #define FXLS8471_HYS_MASK 0x07 |
Definition at line 239 of file fxls8471.h.
| #define FXLS8471_HYS_SHIFT 0 |
Definition at line 240 of file fxls8471.h.
| #define FXLS8471_INT_CFG_A_VECM_MASK 0x02 |
Definition at line 432 of file fxls8471.h.
| #define FXLS8471_INT_CFG_A_VECM_SHIFT 1 |
Definition at line 433 of file fxls8471.h.
| #define FXLS8471_INT_CFG_ASLP_MASK 0x80 |
Definition at line 420 of file fxls8471.h.
| #define FXLS8471_INT_CFG_ASLP_SHIFT 7 |
Definition at line 421 of file fxls8471.h.
| #define FXLS8471_INT_CFG_DRDY_MASK 0x01 |
Definition at line 434 of file fxls8471.h.
| #define FXLS8471_INT_CFG_DRDY_SHIFT 0 |
Definition at line 435 of file fxls8471.h.
| #define FXLS8471_INT_CFG_FFMT_MASK 0x04 |
Definition at line 430 of file fxls8471.h.
| #define FXLS8471_INT_CFG_FFMT_SHIFT 2 |
Definition at line 431 of file fxls8471.h.
| #define FXLS8471_INT_CFG_FIFO_MASK 0x40 |
Definition at line 422 of file fxls8471.h.
| #define FXLS8471_INT_CFG_FIFO_SHIFT 6 |
Definition at line 423 of file fxls8471.h.
| #define FXLS8471_INT_CFG_LNDPRT_MASK 0x10 |
Definition at line 426 of file fxls8471.h.
| #define FXLS8471_INT_CFG_LNDPRT_SHIFT 4 |
Definition at line 427 of file fxls8471.h.
| #define FXLS8471_INT_CFG_PULSE_MASK 0x08 |
Definition at line 428 of file fxls8471.h.
| #define FXLS8471_INT_CFG_PULSE_SHIFT 3 |
Definition at line 429 of file fxls8471.h.
| #define FXLS8471_INT_CFG_TRANS_MASK 0x20 |
Definition at line 424 of file fxls8471.h.
| #define FXLS8471_INT_CFG_TRANS_SHIFT 5 |
Definition at line 425 of file fxls8471.h.
| #define FXLS8471_INT_EN_A_VECM_MASK 0x02 |
Definition at line 412 of file fxls8471.h.
| #define FXLS8471_INT_EN_A_VECM_SHIFT 1 |
Definition at line 413 of file fxls8471.h.
| #define FXLS8471_INT_EN_ASLP_MASK 0x80 |
Definition at line 400 of file fxls8471.h.
| #define FXLS8471_INT_EN_ASLP_SHIFT 7 |
Definition at line 401 of file fxls8471.h.
| #define FXLS8471_INT_EN_DRDY_MASK 0x01 |
Definition at line 414 of file fxls8471.h.
| #define FXLS8471_INT_EN_DRDY_SHIFT 0 |
Definition at line 415 of file fxls8471.h.
| #define FXLS8471_INT_EN_FFMT_MASK 0x04 |
Definition at line 410 of file fxls8471.h.
| #define FXLS8471_INT_EN_FFMT_SHIFT 2 |
Definition at line 411 of file fxls8471.h.
| #define FXLS8471_INT_EN_FIFO_MASK 0x40 |
Definition at line 402 of file fxls8471.h.
| #define FXLS8471_INT_EN_FIFO_SHIFT 6 |
Definition at line 403 of file fxls8471.h.
| #define FXLS8471_INT_EN_LNDPRT_MASK 0x10 |
Definition at line 406 of file fxls8471.h.
| #define FXLS8471_INT_EN_LNDPRT_SHIFT 4 |
Definition at line 407 of file fxls8471.h.
| #define FXLS8471_INT_EN_PULSE_MASK 0x08 |
Definition at line 408 of file fxls8471.h.
| #define FXLS8471_INT_EN_PULSE_SHIFT 3 |
Definition at line 409 of file fxls8471.h.
| #define FXLS8471_INT_EN_TRANS_MASK 0x20 |
Definition at line 404 of file fxls8471.h.
| #define FXLS8471_INT_EN_TRANS_SHIFT 5 |
Definition at line 405 of file fxls8471.h.
| #define FXLS8471_IPOL_MASK 0x02 |
Definition at line 393 of file fxls8471.h.
| #define FXLS8471_IPOL_SHIFT 1 |
Definition at line 394 of file fxls8471.h.
| #define FXLS8471_LAPO_MASK 0x06 |
Definition at line 213 of file fxls8471.h.
| #define FXLS8471_LAPO_SHIFT 1 |
Definition at line 214 of file fxls8471.h.
| #define FXLS8471_LNOISE_MASK 0x04 |
Definition at line 354 of file fxls8471.h.
| #define FXLS8471_LNOISE_SHIFT 2 |
Definition at line 355 of file fxls8471.h.
| #define FXLS8471_LO_MASK 0x40 |
Definition at line 211 of file fxls8471.h.
| #define FXLS8471_LO_SHIFT 6 |
Definition at line 212 of file fxls8471.h.
| #define FXLS8471_MODS_MASK 0x03 |
Definition at line 375 of file fxls8471.h.
| #define FXLS8471_MODS_SHIFT 0 |
Definition at line 376 of file fxls8471.h.
| #define FXLS8471_NEWLP_MASK 0x80 |
Definition at line 209 of file fxls8471.h.
| #define FXLS8471_NEWLP_SHIFT 7 |
Definition at line 210 of file fxls8471.h.
| #define FXLS8471_PEA_MASK 0x80 |
Definition at line 333 of file fxls8471.h.
| #define FXLS8471_PELE_MASK 0x40 |
Definition at line 316 of file fxls8471.h.
| #define FXLS8471_PELE_SHIFT 6 |
Definition at line 317 of file fxls8471.h.
| #define FXLS8471_PL_EN_MASK 0x40 |
Definition at line 223 of file fxls8471.h.
| #define FXLS8471_PL_EN_SHIFT 6 |
Definition at line 224 of file fxls8471.h.
| #define FXLS8471_PL_THS_MASK 0xF8 |
Definition at line 237 of file fxls8471.h.
| #define FXLS8471_PL_THS_SHIFT 3 |
Definition at line 238 of file fxls8471.h.
| #define FXLS8471_POLX_MASK 0x01 |
Definition at line 340 of file fxls8471.h.
| #define FXLS8471_POLY_MASK 0x02 |
Definition at line 339 of file fxls8471.h.
| #define FXLS8471_POLZ_MASK 0x04 |
Definition at line 338 of file fxls8471.h.
| #define FXLS8471_PP_OD_MASK 0x01 |
Definition at line 395 of file fxls8471.h.
| #define FXLS8471_PP_OD_SHIFT 0 |
Definition at line 396 of file fxls8471.h.
| #define FXLS8471_PTHS_MASK 0x7F |
Definition at line 344 of file fxls8471.h.
| #define FXLS8471_PTHS_SHIFT 0 |
Definition at line 345 of file fxls8471.h.
| #define FXLS8471_PULSE_HPF_BYP_MASK 0x20 |
Definition at line 199 of file fxls8471.h.
| #define FXLS8471_PULSE_HPF_BYP_SHIFT 5 |
Definition at line 200 of file fxls8471.h.
| #define FXLS8471_PULSE_LPF_EN_MASK 0x10 |
Definition at line 201 of file fxls8471.h.
| #define FXLS8471_PULSE_LPF_EN_SHIFT 4 |
Definition at line 202 of file fxls8471.h.
| #define FXLS8471_RST_MASK 0x40 |
Definition at line 369 of file fxls8471.h.
Referenced by fxls8471_Reset().
| #define FXLS8471_RST_SHIFT 6 |
Definition at line 370 of file fxls8471.h.
| #define FXLS8471_SEL_MASK 0x03 |
Definition at line 203 of file fxls8471.h.
| #define FXLS8471_SEL_SHIFT 0 |
Definition at line 204 of file fxls8471.h.
| #define FXLS8471_SET_FIELD | ( | name, | |
| val | |||
| ) | (((val)<<FXLS8471_##name##_SHIFT)&(FXLS8471_##name##_MASK)) |
Definition at line 96 of file fxls8471.h.
Referenced by fxls8471_SetConfig().
| #define FXLS8471_SLPE_MASK 0x04 |
Definition at line 373 of file fxls8471.h.
| #define FXLS8471_SLPE_SHIFT 2 |
Definition at line 374 of file fxls8471.h.
| #define FXLS8471_SMODS_MASK 0x18 |
Definition at line 371 of file fxls8471.h.
| #define FXLS8471_SMODS_SHIFT 3 |
Definition at line 372 of file fxls8471.h.
| #define FXLS8471_SRC_A_VECM_MASK 0x02 |
Definition at line 183 of file fxls8471.h.
| #define FXLS8471_SRC_A_VECM_SHIFT 1 |
Definition at line 184 of file fxls8471.h.
| #define FXLS8471_SRC_ASLP_MASK 0x80 |
Definition at line 171 of file fxls8471.h.
| #define FXLS8471_SRC_ASLP_SHIFT 7 |
Definition at line 172 of file fxls8471.h.
| #define FXLS8471_SRC_DRDY_MASK 0x01 |
Definition at line 185 of file fxls8471.h.
| #define FXLS8471_SRC_DRDY_SHIFT 0 |
Definition at line 186 of file fxls8471.h.
| #define FXLS8471_SRC_FFMT_MASK 0x04 |
Definition at line 181 of file fxls8471.h.
| #define FXLS8471_SRC_FFMT_SHIFT 2 |
Definition at line 182 of file fxls8471.h.
| #define FXLS8471_SRC_FIFO_MASK 0x40 |
Definition at line 173 of file fxls8471.h.
| #define FXLS8471_SRC_FIFO_SHIFT 6 |
Definition at line 174 of file fxls8471.h.
| #define FXLS8471_SRC_LNDPRT_MASK 0x10 |
Definition at line 177 of file fxls8471.h.
| #define FXLS8471_SRC_LNDPRT_SHIFT 4 |
Definition at line 178 of file fxls8471.h.
| #define FXLS8471_SRC_PULSE_MASK 0x08 |
Definition at line 179 of file fxls8471.h.
| #define FXLS8471_SRC_PULSE_SHIFT 3 |
Definition at line 180 of file fxls8471.h.
| #define FXLS8471_SRC_TRANS_MASK 0x20 |
Definition at line 175 of file fxls8471.h.
| #define FXLS8471_SRC_TRANS_SHIFT 5 |
Definition at line 176 of file fxls8471.h.
| #define FXLS8471_ST_MASK 0x80 |
Definition at line 367 of file fxls8471.h.
| #define FXLS8471_ST_SHIFT 7 |
Definition at line 368 of file fxls8471.h.
| #define FXLS8471_STANDBY 0x00 |
Definition at line 362 of file fxls8471.h.
| #define FXLS8471_SYSMOD_MASK 0x03 |
Definition at line 161 of file fxls8471.h.
| #define FXLS8471_SYSMOD_SHIFT 0 |
Definition at line 162 of file fxls8471.h.
| #define FXLS8471_SYSMOD_SLEEP 0x02 |
Definition at line 166 of file fxls8471.h.
| #define FXLS8471_SYSMOD_STANDBY 0x00 |
Definition at line 164 of file fxls8471.h.
| #define FXLS8471_SYSMOD_WAKE 0x01 |
Definition at line 165 of file fxls8471.h.
| #define FXLS8471_TEA_MASK 0x40 |
Definition at line 303 of file fxls8471.h.
| #define FXLS8471_TELE_MASK 0x10 |
Definition at line 289 of file fxls8471.h.
| #define FXLS8471_TELE_SHIFT 4 |
Definition at line 290 of file fxls8471.h.
| #define FXLS8471_TRIG_A_VECM_MASK 0x02 |
Definition at line 151 of file fxls8471.h.
| #define FXLS8471_TRIG_A_VECM_SHIFT 1 |
Definition at line 152 of file fxls8471.h.
| #define FXLS8471_TRIG_FFMT_MASK 0x04 |
Definition at line 149 of file fxls8471.h.
| #define FXLS8471_TRIG_FFMT_SHIFT 2 |
Definition at line 150 of file fxls8471.h.
| #define FXLS8471_TRIG_LNDPRT_MASK 0x10 |
Definition at line 145 of file fxls8471.h.
| #define FXLS8471_TRIG_LNDPRT_SHIFT 4 |
Definition at line 146 of file fxls8471.h.
| #define FXLS8471_TRIG_PULSE_MASK 0x08 |
Definition at line 147 of file fxls8471.h.
| #define FXLs8471_TRIG_PULSE_SHIFT 3 |
Definition at line 148 of file fxls8471.h.
| #define FXLS8471_TRIG_TRANS_MASK 0x20 |
Definition at line 143 of file fxls8471.h.
| #define FXLS8471_TRIG_TRANS_SHIFT 5 |
Definition at line 144 of file fxls8471.h.
| #define FXLS8471_WAKE_A_VECM_MASK 0x04 |
Definition at line 391 of file fxls8471.h.
| #define FXLS8471_WAKE_A_VECM_SHIFT 2 |
Definition at line 392 of file fxls8471.h.
| #define FXLS8471_WAKE_FFMT_MASK 0x08 |
Definition at line 389 of file fxls8471.h.
| #define FXLS8471_WAKE_FFMT_SHIFT 3 |
Definition at line 390 of file fxls8471.h.
| #define FXLS8471_WAKE_LNDPRT_MASK 0x20 |
Definition at line 385 of file fxls8471.h.
| #define FXLS8471_WAKE_LNDPRT_SHIFT 5 |
Definition at line 386 of file fxls8471.h.
| #define FXLS8471_WAKE_PULSE_MASK 0x10 |
Definition at line 387 of file fxls8471.h.
| #define FXLS8471_WAKE_PULSE_SHIFT 4 |
Definition at line 388 of file fxls8471.h.
| #define FXLS8471_WAKE_TRANS_MASK 0x40 |
Definition at line 383 of file fxls8471.h.
| #define FXLS8471_WAKE_TRANS_SHIFT 6 |
Definition at line 384 of file fxls8471.h.
| #define FXLS8471_WHOAMI_VALUE (0x6A) |
Definition at line 88 of file fxls8471.h.
Referenced by fxls8471_CheckId().
| #define FXLS8471_X_TRANS_POL_MASK 0x01 |
Definition at line 309 of file fxls8471.h.
| #define FXLS8471_XDPEFE_MASK 0x02 |
Definition at line 326 of file fxls8471.h.
| #define FXLS8471_XDPEFE_SHIFT 1 |
Definition at line 327 of file fxls8471.h.
| #define FXLS8471_XDR_MASK 0x01 |
Definition at line 111 of file fxls8471.h.
| #define FXLS8471_XOW_MASK 0x10 |
Definition at line 106 of file fxls8471.h.
| #define FXLS8471_XSPEFE_MASK 0x01 |
Definition at line 328 of file fxls8471.h.
| #define FXLS8471_XSPEFE_SHIFT 0 |
Definition at line 329 of file fxls8471.h.
| #define FXLS8471_XTEFE_MASK 0x02 |
Definition at line 295 of file fxls8471.h.
| #define FXLS8471_XTEFE_SHIFT 1 |
Definition at line 296 of file fxls8471.h.
| #define FXLS8471_XTRANSE_MASK 0x02 |
Definition at line 308 of file fxls8471.h.
| #define FXLS8471_Y_TRANS_POL_MASK 0x04 |
Definition at line 307 of file fxls8471.h.
| #define FXLS8471_YDPEFE_MASK 0x08 |
Definition at line 322 of file fxls8471.h.
| #define FXLS8471_YDPEFE_SHIFT 3 |
Definition at line 323 of file fxls8471.h.
| #define FXLS8471_YDR_MASK 0x02 |
Definition at line 110 of file fxls8471.h.
| #define FXLS8471_YOW_MASK 0x20 |
Definition at line 105 of file fxls8471.h.
| #define FXLS8471_YSPEFE_MASK 0x04 |
Definition at line 324 of file fxls8471.h.
| #define FXLS8471_YSPEFE_SHIFT 2 |
Definition at line 325 of file fxls8471.h.
| #define FXLS8471_YTEFE_MASK 0x04 |
Definition at line 293 of file fxls8471.h.
| #define FXLS8471_YTEFE_SHIFT 2 |
Definition at line 294 of file fxls8471.h.
| #define FXLS8471_YTRANSE_MASK 0x08 |
Definition at line 306 of file fxls8471.h.
| #define FXLS8471_Z_TRANS_POL_MASK 0x10 |
Definition at line 305 of file fxls8471.h.
| #define FXLS8471_ZDPEFE_MASK 0x20 |
Definition at line 318 of file fxls8471.h.
| #define FXLS8471_ZDPEFE_SHIFT 5 |
Definition at line 319 of file fxls8471.h.
| #define FXLS8471_ZDR_MASK 0x04 |
Definition at line 109 of file fxls8471.h.
| #define FXLS8471_ZLOCK_MASK 0x07 |
Definition at line 231 of file fxls8471.h.
| #define FXLS8471_ZLOCK_SHIFT 0 |
Definition at line 232 of file fxls8471.h.
| #define FXLS8471_ZOW_MASK 0x40 |
Definition at line 104 of file fxls8471.h.
| #define FXLS8471_ZSPEFE_MASK 0x10 |
Definition at line 320 of file fxls8471.h.
| #define FXLS8471_ZSPEFE_SHIFT 4 |
Definition at line 321 of file fxls8471.h.
| #define FXLS8471_ZTEFE_MASK 0x08 |
Definition at line 291 of file fxls8471.h.
| #define FXLS8471_ZTEFE_SHIFT 3 |
Definition at line 292 of file fxls8471.h.
| #define FXLS8471_ZTRANSE_MASK 0x20 |
Definition at line 304 of file fxls8471.h.
| #define FXLS8471_ZYXDR_MASK 0x08 |
Definition at line 107 of file fxls8471.h.
| #define FXLS8471_ZYXDR_SHIFT 3 |
Definition at line 108 of file fxls8471.h.
| #define FXLS8471_ZYXOW_MASK 0x80 |
Definition at line 102 of file fxls8471.h.
| #define FXLS8471_ZYXOW_SHIFT 7 |
Definition at line 103 of file fxls8471.h.
| anonymous enum |
The FXLS8471 types.
The FXLS8471 Sensor Internal Register Map.
Definition at line 20 of file fxls8471.h.
| anonymous enum |
| Enumerator | |
|---|---|
| FXLS8471_SUCCESS | |
| FXLS8471_DATA_OVERWRITE | |
| FXLS8471_ERROR | |
Definition at line 464 of file fxls8471.h.