![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | subscriptionConfig_t |
| This structure holds the sensor subscriptions configuration info. More... | |
| struct | pseudoSettings_t |
| struct | appSubscriptionResponse_t |
| This structure holds the ISF application subscriptions information in the "GET_APP_SUBSCRIPTION" CI command response buffer. More... | |
Macros | |
| #define | App1_TASK_NAME "App1_task" |
| #define | App1_TASK_STACK_SIZE 1200 |
| #define | App1_TASK_PRIORITY 11 |
| #define | startof(type, member) ((int32)&((type *)0)->member) |
| #define | NUM_SENSORS (sizeof(App1AppInstance.info)/sizeof(SensorInfo_t)) |
| Macro thats holds number of active sensors. More... | |
| #define | SET_FIELD(name, val) (((val)<<name##_SHIFT)&(name##_MASK)) |
| Macro that extracts one of the fields below. More... | |
| #define | GET_FIELD(name, val) ((val&name##_MASK)>>name##_SHIFT) |
| #define | CTRL_STATE_MASK 0x0F |
| Control register mask/shift definitions for the application. More... | |
| #define | CTRL_STATE_SHIFT 0 |
| #define | CTRL_QREN_MASK 0x10 |
| #define | CTRL_QREN_SHIFT 4 |
| #define | CTRL_RESET_MASK 0x20 |
| #define | CTRL_RESET_SHIFT 5 |
| #define | CTRL_POWER_MASK 0xC0 |
| #define | CTRL_POWER_SHIFT 6 |
Functions | |
| OSA_TASK_DEFINE (App1, App1_TASK_STACK_SIZE) | |
| int32 | App1_GotoState (uint8 desiredState) |
| void | App1_task (os_task_param_t task_init_data) |
| void | App1_init (void) |
| void | App1_MainTask (void) |
| ci_response_t | App1_ci_app_callback (ci_host_cmd_packet_t *pHostPacket, ci_app_resp_packet_t *pAppPacket) |
| void | App1_ReturnSensorsToInit () |
Variables | |
| App1AppInstance_t | App1AppInstance |
| #define App1_TASK_NAME "App1_task" |
Definition at line 236 of file App1.c.
Referenced by App1_init().
| #define App1_TASK_PRIORITY 11 |
Definition at line 240 of file App1.c.
Referenced by App1_init().
| #define App1_TASK_STACK_SIZE 1200 |
Definition at line 238 of file App1.c.
Referenced by App1_init().
| #define CTRL_POWER_MASK 0xC0 |
Definition at line 290 of file App1.c.
Referenced by App1_ci_app_callback().
| #define CTRL_STATE_MASK 0x0F |
Control register mask/shift definitions for the application.
Definition at line 284 of file App1.c.
Referenced by App1_ci_app_callback(), and App1_GotoState().
| #define GET_FIELD | ( | name, | |
| val | |||
| ) | ((val&name##_MASK)>>name##_SHIFT) |
Definition at line 281 of file App1.c.
Referenced by App1_ci_app_callback(), App1_GotoState(), and App1_MainTask().
| #define NUM_SENSORS (sizeof(App1AppInstance.info)/sizeof(SensorInfo_t)) |
| #define SET_FIELD | ( | name, | |
| val | |||
| ) | (((val)<<name##_SHIFT)&(name##_MASK)) |
Macro that extracts one of the fields below.
Definition at line 280 of file App1.c.
Referenced by App1_ci_app_callback(), and App1_GotoState().
| #define startof | ( | type, | |
| member | |||
| ) | ((int32)&((type *)0)->member) |
Definition at line 274 of file App1.c.
Referenced by App1_ci_app_callback().
| ci_response_t App1_ci_app_callback | ( | ci_host_cmd_packet_t * | pHostPacket, |
| ci_app_resp_packet_t * | pAppPacket | ||
| ) |
Definition at line 1067 of file App1.c.
References App1AppSettings_t::AccelerometerSettings_Sub0, App1AppSettings_t::AccelerometerSettings_Sub1, App1AppSettings_t::AccelerometerSettings_Sub2, App1AppSettings_t::AccelerometerSettings_Sub3, App1AppSettings_t::AccelerometerSettings_Sub4, App1AppSettings_t::AccelerometerSettings_Sub5, App1AppSettings_t::AccelerometerSettings_Sub6, App1AppSettings_t::AccelerometerSettings_Sub7, App1AppSettings_t::AltitudeSettings_Sub15, App1AppSettings_t::AnalogSettings_Sub19, App1_GotoState(), App1_STATE_STOPPED_UNSUBSCRIBED, ci_host_cmd_packet_t::appId, App1AppInstance_t::appId, ci_host_cmd_packet_t::byte_cnt, ci_app_resp_packet_t::bytes_xfer, CI_CMD_GET_APP_SUBSCRIPTION, CI_CMD_READ_APP_DATA, CI_CMD_READ_CONFIG, CI_CMD_READ_VERSION, CI_CMD_RESET_APP, CI_CMD_UPDATE_QUICKREAD, CI_CMD_WRITE_CONFIG, CI_CMD_WRITE_SREC_FLASH, CI_ERROR_COMMAND, CI_ERROR_NONE, CI_INVALID_COUNT, CI_MAX_FLASH_BYTES, ci_host_cmd_packet_t::cmd, App1AppSettings_t::control, CTRL_POWER_MASK, CTRL_STATE_MASK, App1AppSettings_t::CustomSettings_Sub18, App1AppInstance_t::data, GET_FIELD, App1AppSettings_t::GyrometerSettings_Sub10, App1AppSettings_t::GyrometerSettings_Sub11, App1AppInstance_t::info, App1AppInstance_t::instance, isf_ci_app_read(), isf_ci_app_write(), isf_ci_qr_update(), isf_swap4byte(), App1AppSettings_t::MagnetometerSettings_Sub8, App1AppSettings_t::MagnetometerSettings_Sub9, isf_SubscriptionSettings_t::nSamplePeriod, ci_host_cmd_packet_t::offset, App1AppSettings_t::OrientationSettings_Sub14, App1AppInstance_t::outputBufferLock, App1AppSettings_t::PedometerSettings_Sub16, App1AppSettings_t::PedometerSettings_Sub17, App1AppSettings_t::PressureSettings_Sub12, SensorInfo_t::sensorId, SET_FIELD, App1AppInstance_t::settings, startof, and App1AppSettings_t::TemperatureSettings_Sub13.

Definition at line 1612 of file App1.c.
References App1AppInstance_t::AccelerometerDataFifo_Sub0, App1AppInstance_t::AccelerometerDataFifo_Sub1, App1AppInstance_t::AccelerometerDataFifo_Sub2, App1AppInstance_t::AccelerometerDataFifo_Sub3, App1AppInstance_t::AccelerometerDataFifo_Sub4, App1AppInstance_t::AccelerometerDataFifo_Sub5, App1AppInstance_t::AccelerometerDataFifo_Sub6, App1AppInstance_t::AccelerometerDataFifo_Sub7, App1AppInstance_t::AccelerometerInfo_Sub0, App1AppInstance_t::AccelerometerInfo_Sub1, App1AppInstance_t::AccelerometerInfo_Sub2, App1AppInstance_t::AccelerometerInfo_Sub3, App1AppInstance_t::AccelerometerInfo_Sub4, App1AppInstance_t::AccelerometerInfo_Sub5, App1AppInstance_t::AccelerometerInfo_Sub6, App1AppInstance_t::AccelerometerInfo_Sub7, App1AppSettings_t::AccelerometerSettings_Sub0, App1AppSettings_t::AccelerometerSettings_Sub1, App1AppSettings_t::AccelerometerSettings_Sub2, App1AppSettings_t::AccelerometerSettings_Sub3, App1AppSettings_t::AccelerometerSettings_Sub4, App1AppSettings_t::AccelerometerSettings_Sub5, App1AppSettings_t::AccelerometerSettings_Sub6, App1AppSettings_t::AccelerometerSettings_Sub7, App1AppInstance_t::AltitudeDataFifo_Sub15, App1AppInstance_t::AltitudeInfo_Sub15, App1AppSettings_t::AltitudeSettings_Sub15, App1AppInstance_t::AnalogDataFifo_Sub19, App1AppInstance_t::AnalogInfo_Sub19, App1AppSettings_t::AnalogSettings_Sub19, App1_ReturnSensorsToInit(), App1_STATE_STARTED_SUBSCRIBED, App1_STATE_STOPPED_SUBSCRIBED, App1_STATE_STOPPED_UNSUBSCRIBED, configure_sensor(), App1AppSettings_t::control, CTRL_STATE_MASK, App1AppInstance_t::CustomDataFifo_Sub18, App1AppInstance_t::CustomInfo_Sub18, App1AppSettings_t::CustomSettings_Sub18, App1AppInstance_t::fifos, GET_FIELD, App1AppInstance_t::GyrometerDataFifo_Sub10, App1AppInstance_t::GyrometerDataFifo_Sub11, App1AppInstance_t::GyrometerInfo_Sub10, App1AppInstance_t::GyrometerInfo_Sub11, App1AppSettings_t::GyrometerSettings_Sub10, App1AppSettings_t::GyrometerSettings_Sub11, App1AppInstance_t::info, ISF_SUCCESS, App1AppInstance_t::MagnetometerDataFifo_Sub8, App1AppInstance_t::MagnetometerDataFifo_Sub9, App1AppInstance_t::MagnetometerInfo_Sub8, App1AppInstance_t::MagnetometerInfo_Sub9, App1AppSettings_t::MagnetometerSettings_Sub8, App1AppSettings_t::MagnetometerSettings_Sub9, App1AppInstance_t::OrientationDataFifo_Sub14, App1AppInstance_t::OrientationInfo_Sub14, App1AppSettings_t::OrientationSettings_Sub14, App1AppInstance_t::PedometerDataFifo_Sub16, App1AppInstance_t::PedometerDataFifo_Sub17, App1AppInstance_t::PedometerInfo_Sub16, App1AppInstance_t::PedometerInfo_Sub17, App1AppSettings_t::PedometerSettings_Sub16, App1AppSettings_t::PedometerSettings_Sub17, App1AppInstance_t::PressureDataFifo_Sub12, App1AppInstance_t::PressureInfo_Sub12, App1AppSettings_t::PressureSettings_Sub12, SET_FIELD, App1AppInstance_t::settings, shutdown_sensor(), SensorInfo_t::smAdapterHandle, start_sensor(), stop_sensor(), App1AppInstance_t::TemperatureDataFifo_Sub13, App1AppInstance_t::TemperatureInfo_Sub13, and App1AppSettings_t::TemperatureSettings_Sub13.
Referenced by App1_ci_app_callback(), and App1_MainTask().


| void App1_init | ( | void | ) |
Definition at line 397 of file App1.c.
References App1_task(), App1_TASK_NAME, App1_TASK_PRIORITY, and App1_TASK_STACK_SIZE.
Referenced by Components_Init().


| void App1_MainTask | ( | void | ) |
Definition at line 426 of file App1.c.
References App1AppInstance_t::AccelerometerDataFifo_Sub0, App1AppInstance_t::AccelerometerDataFifo_Sub1, App1AppInstance_t::AccelerometerDataFifo_Sub2, App1AppInstance_t::AccelerometerDataFifo_Sub3, App1AppInstance_t::AccelerometerDataFifo_Sub4, App1AppInstance_t::AccelerometerDataFifo_Sub5, App1AppInstance_t::AccelerometerDataFifo_Sub6, App1AppInstance_t::AccelerometerDataFifo_Sub7, App1AppInstance_t::AccelerometerInfo_Sub0, App1AppInstance_t::AccelerometerInfo_Sub1, App1AppInstance_t::AccelerometerInfo_Sub2, App1AppInstance_t::AccelerometerInfo_Sub3, App1AppInstance_t::AccelerometerInfo_Sub4, App1AppInstance_t::AccelerometerInfo_Sub5, App1AppInstance_t::AccelerometerInfo_Sub6, App1AppInstance_t::AccelerometerInfo_Sub7, App1AppSettings_t::AccelerometerSettings_Sub0, App1AppSettings_t::AccelerometerSettings_Sub1, App1AppSettings_t::AccelerometerSettings_Sub2, App1AppSettings_t::AccelerometerSettings_Sub3, App1AppSettings_t::AccelerometerSettings_Sub4, App1AppSettings_t::AccelerometerSettings_Sub5, App1AppSettings_t::AccelerometerSettings_Sub6, App1AppSettings_t::AccelerometerSettings_Sub7, App1AppInstance_t::AltitudeDataFifo_Sub15, App1AppInstance_t::AltitudeInfo_Sub15, App1AppSettings_t::AltitudeSettings_Sub15, App1AppInstance_t::AnalogDataFifo_Sub19, App1AppInstance_t::AnalogInfo_Sub19, App1AppSettings_t::AnalogSettings_Sub19, App1_Accelerometer0_DATA_READY_EVENT, App1_Accelerometer1_DATA_READY_EVENT, App1_Accelerometer2_DATA_READY_EVENT, App1_Accelerometer3_DATA_READY_EVENT, App1_Accelerometer4_DATA_READY_EVENT, App1_Accelerometer5_DATA_READY_EVENT, App1_Accelerometer6_DATA_READY_EVENT, App1_Accelerometer7_DATA_READY_EVENT, App1_ALL_SENSOR_DATA_READY, App1_Altitude15_DATA_READY_EVENT, App1_Analog19_DATA_READY_EVENT, App1_Custom18_DATA_READY_EVENT, App1_Exit(), App1_GotoState(), App1_Gyrometer10_DATA_READY_EVENT, App1_Gyrometer11_DATA_READY_EVENT, App1_Initialization(), App1_Magnetometer8_DATA_READY_EVENT, App1_Magnetometer9_DATA_READY_EVENT, App1_Orientation14_DATA_READY_EVENT, App1_Pedometer16_DATA_READY_EVENT, App1_Pedometer17_DATA_READY_EVENT, App1_Pressure12_DATA_READY_EVENT, App1_ProcessData(), App1_Temperature13_DATA_READY_EVENT, App1AppInstance_t::appId, App1AppSettings_t::control, App1AppInstance_t::CustomDataFifo_Sub18, App1AppInstance_t::CustomInfo_Sub18, App1AppSettings_t::CustomSettings_Sub18, App1AppInstance_t::data, DATA_FIFO_LEN_SUB0, DATA_FIFO_LEN_SUB1, DATA_FIFO_LEN_SUB10, DATA_FIFO_LEN_SUB11, DATA_FIFO_LEN_SUB12, DATA_FIFO_LEN_SUB13, DATA_FIFO_LEN_SUB14, DATA_FIFO_LEN_SUB15, DATA_FIFO_LEN_SUB16, DATA_FIFO_LEN_SUB17, DATA_FIFO_LEN_SUB18, DATA_FIFO_LEN_SUB19, DATA_FIFO_LEN_SUB2, DATA_FIFO_LEN_SUB3, DATA_FIFO_LEN_SUB4, DATA_FIFO_LEN_SUB5, DATA_FIFO_LEN_SUB6, DATA_FIFO_LEN_SUB7, DATA_FIFO_LEN_SUB8, DATA_FIFO_LEN_SUB9, DATA_TYPE_SUB0, DATA_TYPE_SUB1, DATA_TYPE_SUB10, DATA_TYPE_SUB11, DATA_TYPE_SUB12, DATA_TYPE_SUB13, DATA_TYPE_SUB14, DATA_TYPE_SUB15, DATA_TYPE_SUB16, DATA_TYPE_SUB17, DATA_TYPE_SUB18, DATA_TYPE_SUB19, DATA_TYPE_SUB2, DATA_TYPE_SUB3, DATA_TYPE_SUB4, DATA_TYPE_SUB5, DATA_TYPE_SUB6, DATA_TYPE_SUB7, DATA_TYPE_SUB8, DATA_TYPE_SUB9, DSA_Analog_1, DSA_Custom_1, DSA_FXAS21002_1, DSA_FXAS21002_2, DSA_FXLC95000_1, DSA_FXLC95000_2, DSA_FXLS8471_1, DSA_FXLS8471_2, DSA_FXLS8952_1, DSA_FXOS8700_1, DSA_FXOS8700_2, DSA_MAG3110_1, DSA_MMA8491Q_1, DSA_MMA865x_1, DSA_MMA955x_1, DSA_MMA955x_2, DSA_MPL3115_1, DSA_ORIENT_1, App1AppInstance_t::fifos, GET_FIELD, gSensorHandleList, App1AppInstance_t::GyrometerDataFifo_Sub10, App1AppInstance_t::GyrometerDataFifo_Sub11, App1AppInstance_t::GyrometerInfo_Sub10, App1AppInstance_t::GyrometerInfo_Sub11, App1AppSettings_t::GyrometerSettings_Sub10, App1AppSettings_t::GyrometerSettings_Sub11, App1AppInstance_t::info, init_sensor(), App1AppInstance_t::instance, isf_ci_qr_update(), isf_ci_stream_update_data(), isf_fifo_el_clear(), isf_fifo_el_traverse(), isf_fifo_init(), isf_fifo_lock(), isf_fifo_unlock(), ISF_SUCCESS, App1AppInstance_t::MagnetometerDataFifo_Sub8, App1AppInstance_t::MagnetometerDataFifo_Sub9, App1AppInstance_t::MagnetometerInfo_Sub8, App1AppInstance_t::MagnetometerInfo_Sub9, App1AppSettings_t::MagnetometerSettings_Sub8, App1AppSettings_t::MagnetometerSettings_Sub9, isf_SubscriptionSettings_t::nFifoDepth, isf_SubscriptionSettings_t::nSamplePeriod, isf_SubscriptionSettings_t::nSettingsToUse, App1AppInstance_t::OrientationDataFifo_Sub14, App1AppInstance_t::OrientationInfo_Sub14, App1AppSettings_t::OrientationSettings_Sub14, App1AppInstance_t::outputBufferLock, App1AppInstance_t::PedometerDataFifo_Sub16, App1AppInstance_t::PedometerDataFifo_Sub17, App1AppInstance_t::PedometerInfo_Sub16, App1AppInstance_t::PedometerInfo_Sub17, App1AppSettings_t::PedometerSettings_Sub16, App1AppSettings_t::PedometerSettings_Sub17, App1AppInstance_t::PressureDataFifo_Sub12, App1AppInstance_t::PressureInfo_Sub12, App1AppSettings_t::PressureSettings_Sub12, App1SensorData_t::rawAccelerometerData_Sub0, App1SensorData_t::rawAccelerometerData_Sub1, App1SensorData_t::rawAccelerometerData_Sub2, App1SensorData_t::rawAccelerometerData_Sub3, App1SensorData_t::rawAccelerometerData_Sub4, App1SensorData_t::rawAccelerometerData_Sub5, App1SensorData_t::rawAccelerometerData_Sub6, App1SensorData_t::rawAccelerometerData_Sub7, App1SensorData_t::rawAltitudeData_Sub15, App1SensorData_t::rawAnalogData_Sub19, App1SensorData_t::rawCustomData_Sub18, App1SensorData_t::rawGyrometerData_Sub10, App1SensorData_t::rawGyrometerData_Sub11, App1SensorData_t::rawMagnetometerData_Sub8, App1SensorData_t::rawMagnetometerData_Sub9, App1SensorData_t::rawOrientationData_Sub14, App1SensorData_t::rawPedometerData_Sub16, App1SensorData_t::rawPedometerData_Sub17, App1SensorData_t::rawPressureData_Sub12, App1SensorData_t::rawTemperatureData_Sub13, isf_SubscriptionSettings_t::resultFormat, isf_SubscriptionSettings_t::resultType, SensorInfo_t::sensorId, App1AppInstance_t::settings, SensorInfo_t::smAdapterHandle, App1AppInstance_t::smLWEvent, App1AppInstance_t::TemperatureDataFifo_Sub13, App1AppInstance_t::TemperatureInfo_Sub13, and App1AppSettings_t::TemperatureSettings_Sub13.
Referenced by App1_task().


| void App1_ReturnSensorsToInit | ( | ) |
Definition at line 1375 of file App1.c.
References App1AppInstance_t::AccelerometerInfo_Sub0, App1AppInstance_t::AccelerometerInfo_Sub1, App1AppInstance_t::AccelerometerInfo_Sub2, App1AppInstance_t::AccelerometerInfo_Sub3, App1AppInstance_t::AccelerometerInfo_Sub4, App1AppInstance_t::AccelerometerInfo_Sub5, App1AppInstance_t::AccelerometerInfo_Sub6, App1AppInstance_t::AccelerometerInfo_Sub7, isf_SensorHandle_st::adapterStatus, App1AppInstance_t::AltitudeInfo_Sub15, App1AppInstance_t::AnalogInfo_Sub19, App1AppInstance_t::CustomInfo_Sub18, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, App1AppInstance_t::GyrometerInfo_Sub10, App1AppInstance_t::GyrometerInfo_Sub11, App1AppInstance_t::info, App1AppInstance_t::MagnetometerInfo_Sub8, App1AppInstance_t::MagnetometerInfo_Sub9, App1AppInstance_t::OrientationInfo_Sub14, App1AppInstance_t::PedometerInfo_Sub16, App1AppInstance_t::PedometerInfo_Sub17, App1AppInstance_t::PressureInfo_Sub12, shutdown_sensor(), SensorInfo_t::smAdapterHandle, stop_sensor(), and App1AppInstance_t::TemperatureInfo_Sub13.
Referenced by App1_GotoState().


| void App1_task | ( | os_task_param_t | task_init_data | ) |
Definition at line 378 of file App1.c.
References App1_MainTask(), isf_lib_init(), and isf_system_sync().
Referenced by App1_init().


| OSA_TASK_DEFINE | ( | App1 | , |
| App1_TASK_STACK_SIZE | |||
| ) |
| App1AppInstance_t App1AppInstance |