![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | FXLS8471_2_DATA_TYPE fxls8471_DataBuffer_t |
Variables | |
| fxls8471_Sensor_Specific_Settings_t | FXLS8471_2_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXLS8471_2_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXLS8471_2_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| fxls8471_Sensor_Specific_Settings_t | FXLS8471_2_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXLS8471_2_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXLS8471_2_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define FXLS8471_2_DATA_TYPE fxls8471_DataBuffer_t |
Definition at line 114 of file FXLS8471_2.h.
| const isf_dsa_Adapter_t FXLS8471_2_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 169 of file FXLS8471_2.c.
| const isf_dsa_Adapter_t FXLS8471_2_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 169 of file FXLS8471_2.c.
| const i2c_device_t FXLS8471_2_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 184 of file FXLS8471_2.c.
| const i2c_device_t FXLS8471_2_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 184 of file FXLS8471_2.c.
| fxls8471_Sensor_Specific_Settings_t FXLS8471_2_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 106 of file FXLS8471_2.c.
| fxls8471_Sensor_Specific_Settings_t FXLS8471_2_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 106 of file FXLS8471_2.c.