![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | FXLS8952_1_DATA_TYPE fxls8952_DataBuffer_t |
Variables | |
| fxls8952_Sensor_Specific_Settings_t | FXLS8952_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXLS8952_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXLS8952_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| fxls8952_Sensor_Specific_Settings_t | FXLS8952_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXLS8952_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXLS8952_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define FXLS8952_1_DATA_TYPE fxls8952_DataBuffer_t |
Definition at line 145 of file FXLS8952_1.h.
| const isf_dsa_Adapter_t FXLS8952_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 179 of file FXLS8952_1.c.
| const isf_dsa_Adapter_t FXLS8952_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 179 of file FXLS8952_1.c.
| const i2c_device_t FXLS8952_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 194 of file FXLS8952_1.c.
| const i2c_device_t FXLS8952_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 194 of file FXLS8952_1.c.
| fxls8952_Sensor_Specific_Settings_t FXLS8952_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 133 of file FXLS8952_1.c.
| fxls8952_Sensor_Specific_Settings_t FXLS8952_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 133 of file FXLS8952_1.c.