![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | FXOS8700_1_DATA_TYPE fxos8700_DataBuffer_t |
Variables | |
| fxos8700_Sensor_Specific_Settings_t | FXOS8700_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXOS8700_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXOS8700_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| fxos8700_Sensor_Specific_Settings_t | FXOS8700_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXOS8700_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXOS8700_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define FXOS8700_1_DATA_TYPE fxos8700_DataBuffer_t |
Definition at line 102 of file FXOS8700_1.h.
| const isf_dsa_Adapter_t FXOS8700_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 142 of file FXOS8700_1.c.
| const isf_dsa_Adapter_t FXOS8700_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 142 of file FXOS8700_1.c.
| const i2c_device_t FXOS8700_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
This allows access to the sensor communications specific configuration.
Definition at line 157 of file FXOS8700_1.c.
| const i2c_device_t FXOS8700_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
This allows access to the sensor communications specific configuration.
Definition at line 157 of file FXOS8700_1.c.
| fxos8700_Sensor_Specific_Settings_t FXOS8700_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 90 of file FXOS8700_1.c.
| fxos8700_Sensor_Specific_Settings_t FXOS8700_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 90 of file FXOS8700_1.c.