![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Functions | |
| void | Timer_IRQHandler (void) |
| void | isr_bm_callback_tmr (void *dummy) |
| void | bm_timer_init (void) |
Variables | |
| uint32 | bmPITInstance = ISF_BM_PIT_INSTANCE |
| uint32 | bmRolloverPeriod = BM_ROLLOVER_PERIOD |
| void bm_timer_init | ( | void | ) |
Definition at line 49 of file ISFBusManager1.c.
References Timer_IRQHandler().
Referenced by bm_init().


| void isr_bm_callback_tmr | ( | void * | dummy | ) |
Definition at line 570 of file bus_management.c.
References BM_PIPELINE_STAGES, bm_update_cb_list(), bm_t::cb_events, bm_cb_config_t::Cur_period, event_bm_callback, gBm_cb_occurred, gpBm_cb_list, ISF_BM_PIT_CHANNEL_NO, ISF_BM_PIT_INSTANCE, isf_time_util_get_usec(), bm_t::pipeline_index, swdelay(), bm_t::time_keeper_usec, and TRUE.
Referenced by Timer_IRQHandler().


| void Timer_IRQHandler | ( | void | ) |
Definition at line 57 of file ISFBusManager1.c.
References ISF_BM_PIT_CHANNEL_NO, ISF_BM_PIT_INSTANCE, and isr_bm_callback_tmr().
Referenced by bm_timer_init().


| uint32 bmPITInstance = ISF_BM_PIT_INSTANCE |
Definition at line 43 of file ISFBusManager1.c.
| uint32 bmRolloverPeriod = BM_ROLLOVER_PERIOD |
Definition at line 44 of file ISFBusManager1.c.
Referenced by bm_find_smallest_active_period().