![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | MMA8491Q_1_DATA_TYPE mma8491q_DataBuffer_t |
Variables | |
| mma8491q_Sensor_Specific_Settings_t | MMA8491Q_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MMA8491Q_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MMA8491Q_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| mma8491q_Sensor_Specific_Settings_t | MMA8491Q_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MMA8491Q_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MMA8491Q_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define MMA8491Q_1_DATA_TYPE mma8491q_DataBuffer_t |
Definition at line 63 of file MMA8491Q_1.h.
| const isf_dsa_Adapter_t MMA8491Q_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 56 of file MMA8491Q_1.c.
| const isf_dsa_Adapter_t MMA8491Q_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 56 of file MMA8491Q_1.c.
| const i2c_device_t MMA8491Q_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 71 of file MMA8491Q_1.c.
| const i2c_device_t MMA8491Q_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 71 of file MMA8491Q_1.c.
| mma8491q_Sensor_Specific_Settings_t MMA8491Q_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 47 of file MMA8491Q_1.c.
| mma8491q_Sensor_Specific_Settings_t MMA8491Q_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 47 of file MMA8491Q_1.c.