![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | Custom_1_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
| struct | Custom_1_SensorData_EngFixed_t |
| struct | Custom_1_SensorData_Float_t |
| Standard fixed type for three axis accelerometers. More... | |
| struct | Custom_1_Sensor_Specific_Reg_t |
| struct | Custom_1_Sensor_Specific_Settings_t |
| struct | Custom_1_Rate_Specific_Settings_t |
| This structure defines important settings. More... | |
Typedefs | |
| typedef int32 | Custom_1_Status_t |
| SENSOR internal return codes. More... | |
| typedef uint32_t | isf_Custom_1_fixed_data_t |
| typedef float | isf_Custom_1_float_data_t |
Enumerations | |
| enum | { Custom_1_STATUS_00 = 0x00, Custom_1_WHO_AM_I = 0x0D, Custom_1_CTRL_REG1 = 0x2A, Custom_1_CTRL_REG2 = 0x2B } |
| enum | { Custom_1_SUCCESS, Custom_1_DATA_OVERWRITE, Custom_1_ERROR } |
Variables | |
| const uint8_t | Custom_1_Who_Am_I_Values [] = {0x4A, 0x5A} |
| Define the WHO_AM_I register values for both possible sensor variations. More... | |
| Custom_1_Sensor_Specific_Settings_t | Custom_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const i2c_device_t | Custom_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| isf_SensorTypes_t | Custom_1_SupportedSensorTypes [] |
| Supported sensor and data types for the Sensor. More... | |
| isf_SensorDataTypes_t | Custom_1_SupportedDataTypes [] |
| const uint8_t | Custom_1_Who_Am_I_Values [] |
| Define the WHO_AM_I register values for both possible sensor variations. More... | |
| #define __fsl_Sensor_Custom_1_Functions_H_ |
Definition at line 109 of file fsl_Sensor_Custom_1_Functions.h.
| #define __fsl_Sensor_Custom_1_Functions_H__ |
Definition at line 142 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_ACTIVE_MASK 0x01 |
Definition at line 211 of file fsl_Sensor_Custom_1_Functions.h.
Referenced by Custom_1_fsl_Sensor_Custom_Configure(), Custom_1_fsl_Sensor_Custom_EndData(), and Custom_1_fsl_Sensor_Custom_StartData().
| #define Custom_1_ASLP_RATE_MASK 0xC0 |
Definition at line 195 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_ASLP_RATE_SHIFT 6 |
Definition at line 196 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_CONVERT_FIXED_FACTOR 4 |
Definition at line 77 of file fsl_Sensor_Custom_1_Functions.c.
Referenced by Custom_1_fixed_Custom_converter().
| #define Custom_1_CONVERT_FLOAT_FACTOR 0.000061 |
Definition at line 76 of file fsl_Sensor_Custom_1_Functions.c.
Referenced by Custom_1_float_Custom_converter().
| #define Custom_1_DATA_TYPE Custom_1_DataBuffer_t |
Definition at line 137 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_DR_MASK 0x38 |
Definition at line 197 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_DR_SHIFT 3 |
Definition at line 198 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_FREAD_MASK 0x02 |
Definition at line 193 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_FREAD_SHIFT 1 |
Definition at line 194 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_GET_FIELD | ( | name, | |
| val | |||
| ) | ((val&Custom_1_##name##_MASK)>>Custom_1_##name##_SHIFT) |
Definition at line 191 of file fsl_Sensor_Custom_1_Functions.h.
Referenced by Custom_1_fsl_Sensor_Custom_PeriodicCallback(), and Custom_1_fsl_Sensor_Custom_StartData().
| #define Custom_1_MODS_MASK 0x03 |
Definition at line 207 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_MODS_SHIFT 0 |
Definition at line 208 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_RST_MASK 0x40 |
Definition at line 201 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_RST_SHIFT 6 |
Definition at line 202 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_SET_FIELD | ( | name, | |
| val | |||
| ) | (((val)<<Custom_1_##name##_SHIFT)&(Custom_1_##name##_MASK)) |
Definition at line 190 of file fsl_Sensor_Custom_1_Functions.h.
Referenced by Custom_1_fsl_Sensor_Custom_Configure().
| #define Custom_1_SLPE_MASK 0x04 |
Definition at line 203 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_SLPE_SHIFT 2 |
Definition at line 204 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_SMODS_MASK 0x18 |
Definition at line 205 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_SMODS_SHIFT 3 |
Definition at line 206 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_ST_MASK 0x80 |
Definition at line 199 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_ST_SHIFT 7 |
Definition at line 200 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_ZYXDR_MASK 0x08 |
Definition at line 209 of file fsl_Sensor_Custom_1_Functions.h.
| #define Custom_1_ZYXDR_SHIFT 3 |
Definition at line 210 of file fsl_Sensor_Custom_1_Functions.h.
| typedef int32 Custom_1_Status_t |
SENSOR internal return codes.
Definition at line 114 of file fsl_Sensor_Custom_1_Functions.h.
| typedef uint32_t isf_Custom_1_fixed_data_t |
Definition at line 115 of file fsl_Sensor_Custom_1_Functions.h.
| typedef float isf_Custom_1_float_data_t |
Definition at line 116 of file fsl_Sensor_Custom_1_Functions.h.
| anonymous enum |
| Enumerator | |
|---|---|
| Custom_1_STATUS_00 | |
| Custom_1_WHO_AM_I | |
| Custom_1_CTRL_REG1 | |
| Custom_1_CTRL_REG2 | |
Definition at line 167 of file fsl_Sensor_Custom_1_Functions.h.
| anonymous enum |
| Enumerator | |
|---|---|
| Custom_1_SUCCESS | |
| Custom_1_DATA_OVERWRITE | |
| Custom_1_ERROR | |
Definition at line 175 of file fsl_Sensor_Custom_1_Functions.h.
| void Custom_1__Void_ | ( | ) |
Definition at line 55 of file fsl_Sensor_Custom_1_Functions.c.
| isf_dsa_status_t Custom_1_fixed_Custom_converter | ( | Custom_1_Sensor_Specific_Settings_t * | pSensorSpecificConfig, |
| Custom_1_DataBuffer_t * | nativeSample, | ||
| void * | vpConvertedSample | ||
| ) |
Definition at line 109 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_CONVERT_FIXED_FACTOR, Custom_1_DataBuffer_t::data, ISF_SUCCESS, Custom_1_SensorData_EngFixed_t::sensorData, Custom_1_DataBuffer_t::timeStamp, and Custom_1_SensorData_EngFixed_t::timestamp.
Referenced by Custom_1_fsl_Sensor_Custom_Convert().

| isf_dsa_status_t Custom_1_float_Custom_converter | ( | Custom_1_Sensor_Specific_Settings_t * | pSensorSpecificConfig, |
| Custom_1_DataBuffer_t * | nativeSample, | ||
| void * | vpConvertedSample | ||
| ) |
Definition at line 97 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_CONVERT_FLOAT_FACTOR, Custom_1_DataBuffer_t::data, ISF_SUCCESS, Custom_1_SensorData_Float_t::sensorData, Custom_1_DataBuffer_t::timeStamp, and Custom_1_SensorData_Float_t::timestamp.
Referenced by Custom_1_fsl_Sensor_Custom_Convert().

| void Custom_1_fsl_Sensor_Custom_Configure | ( | void * | pSensorHandle, |
| void * | pSensorSettings, | ||
| uint8_t * | retVal | ||
| ) |
Definition at line 541 of file fsl_Sensor_Custom_1_Functions.c.
References BM_ERROR, bm_register_periodic_callback(), DeviceDescriptor_struct::cDescriptor, Custom_1_ACTIVE_MASK, Custom_1_CTRL_REG1, Custom_1_CTRL_REG2, Custom_1_ERROR, Custom_1_fsl_Sensor_Custom_PeriodicCallback(), Custom_1_SET_FIELD, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_acquire_lock(), dm_channel_release_lock(), dm_device_read(), dm_device_write(), DSA_ERR_CONFIGURE, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STOPPED, DSA_STATE_INITIALIZED, ISF_SUCCESS, SENSOR_ERROR_SETMODE, and DeviceDescriptor_struct::token.
Referenced by fsl_Sensor_Custom_1_Configure().


| void Custom_1_fsl_Sensor_Custom_Convert | ( | volatile void * | pSensorHandle, |
| uint32_t | convertToType, | ||
| uint8_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32_t * | numBytes, | ||
| uint8_t * | retVal | ||
| ) |
Definition at line 185 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fixed_Custom_converter(), Custom_1_float_Custom_converter(), DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_RESULT_TYPE_ENG_FIXED, DSA_RESULT_TYPE_ENG_FLOAT, and TYPE_RAW_ACCELERATION_3D.
Referenced by fsl_Sensor_Custom_1_Convert().


| void Custom_1_fsl_Sensor_Custom_EndData | ( | void * | pSensorHandle, |
| uint8_t * | retVal | ||
| ) |
Definition at line 372 of file fsl_Sensor_Custom_1_Functions.c.
References BM_ERROR, bm_stop(), Custom_1_ACTIVE_MASK, Custom_1_CTRL_REG1, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_device_read(), dm_device_write(), DSA_ERR_END_DATA, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, ISF_SUCCESS, SENSOR_ERROR_SETMODE, and DeviceDescriptor_struct::token.
Referenced by fsl_Sensor_Custom_1_EndData().


| void Custom_1_fsl_Sensor_Custom_Initialize | ( | void * | pSensorHandle, |
| uint8_t * | retVal | ||
| ) |
Definition at line 685 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_DataBuffer_t::addr, DeviceDescriptor_struct::cDescriptor, COMM_STATE_OK, Custom_1_WHO_AM_I, Custom_1_DataBuffer_t::data, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_get_state(), dm_channel_init(), dm_channel_start(), dm_device_open(), dm_device_read(), DSA_ERR_INITIALIZE, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, DSA_STATE_NOT_INITIALIZED, ISF_SUCCESS, DeviceDescriptor_struct::pCurrentSample, SENSOR_ERROR_CHECKID, DeviceDescriptor_struct::skipFramecnt, and Custom_1_DataBuffer_t::timeStamp.
Referenced by fsl_Sensor_Custom_1_Initialize().


| void Custom_1_fsl_Sensor_Custom_PeriodicCallback | ( | void * | pSensorHandle | ) |
Definition at line 232 of file fsl_Sensor_Custom_1_Functions.c.
References isf_SensorHandle_st::adapterStatus, BYTES_FOR_FULL_READ, isf_SensorHandle_st::controlData, Custom_1_GET_FIELD, Custom_1_STATUS_00, Custom_1_DataBuffer_t::data, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_device_read(), DSA_STATE_CONFIGURED_STARTED, fsl_Sensor_Custom_1_Convert(), isf_fifo_el_get_insert_pointer(), isf_fifo_el_increment(), ISF_FIFO_FULL, isf_fifo_lock(), isf_fifo_unlock(), ISF_SUCCESS, isf_time_util_get_usec(), isf_dsa_ControlData_st::nEventFieldIndex, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_dsa_ControlData_st::pEventGroup, isf_dsa_SensorSettings_st::pSampleBufferInfo, pSensorData, isf_dsa_SensorSettings_st::resultFormat, isf_dsa_SensorSettings_st::resultType, isf_dsa_ControlData_st::sensorSettings, DeviceDescriptor_struct::skipFramecnt, Custom_1_DataBuffer_t::timeStamp, and TYPE_NATIVE_SENSOR_DATA_TYPE.
Referenced by Custom_1_fsl_Sensor_Custom_Configure().


| void Custom_1_fsl_Sensor_Custom_Shutdown | ( | void * | pSensorHandle, |
| uint8_t * | retVal | ||
| ) |
Definition at line 341 of file fsl_Sensor_Custom_1_Functions.c.
References bm_unregister_callback(), DSA_ERR_PARAM, DSA_STATE_INITIALIZED, ISF_SUCCESS, and DeviceDescriptor_struct::token.
Referenced by fsl_Sensor_Custom_1_Shutdown().


| void Custom_1_fsl_Sensor_Custom_StartData | ( | void * | pSensorHandle, |
| uint8_t * | retVal | ||
| ) |
Definition at line 452 of file fsl_Sensor_Custom_1_Functions.c.
References BM_ERROR, bm_start(), Custom_1_ACTIVE_MASK, Custom_1_CTRL_REG1, Custom_1_GET_FIELD, Custom_1_STATUS_00, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_device_read(), dm_device_write(), DSA_ERR_PARAM, DSA_ERR_START_DATA, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FALSE, ISF_SUCCESS, SENSOR_ERROR_SETMODE, and DeviceDescriptor_struct::token.
Referenced by fsl_Sensor_Custom_1_StartData().


| void Custom_1_fsl_Sensor_Custom_ValidateSettings | ( | void * | pSensorHandle, |
| void * | pSensorSettings, | ||
| uint8_t * | retVal | ||
| ) |
Definition at line 659 of file fsl_Sensor_Custom_1_Functions.c.
References DSA_ERR_PARAM, and ISF_SUCCESS.
Referenced by fsl_Sensor_Custom_1_ValidateSettings().

| isf_dsa_status_t fsl_Sensor_Custom_1_Configure | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 128 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_Configure().

| isf_dsa_status_t fsl_Sensor_Custom_1_Convert | ( | volatile isf_SensorHandle_t * | pSensorHandle, |
| isf_SensorDataTypes_t | convertToType, | ||
| isf_dsa_result_types_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32_t * | numBytes | ||
| ) |
Definition at line 122 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_Convert().
Referenced by Custom_1_fsl_Sensor_Custom_PeriodicCallback().


| isf_dsa_status_t fsl_Sensor_Custom_1_EndData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 152 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_EndData().

| isf_dsa_status_t fsl_Sensor_Custom_1_Initialize | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 140 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_Initialize().

| isf_dsa_status_t fsl_Sensor_Custom_1_Shutdown | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 158 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_Shutdown().

| isf_dsa_status_t fsl_Sensor_Custom_1_StartData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 146 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_StartData().

| isf_dsa_status_t fsl_Sensor_Custom_1_ValidateSettings | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 134 of file fsl_Sensor_Custom_1_Functions.c.
References Custom_1_fsl_Sensor_Custom_ValidateSettings().

| const i2c_device_t Custom_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Updated as per MMA865x device settings.
Definition at line 80 of file fsl_Sensor_Custom_1_Functions.c.
| Custom_1_Sensor_Specific_Settings_t Custom_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 62 of file fsl_Sensor_Custom_1_Functions.c.
| isf_SensorDataTypes_t Custom_1_SupportedDataTypes[] |
Definition at line 92 of file fsl_Sensor_Custom_1_Functions.c.
| isf_SensorTypes_t Custom_1_SupportedSensorTypes[] |
Supported sensor and data types for the Sensor.
Supported sensor and data types.
Definition at line 87 of file fsl_Sensor_Custom_1_Functions.c.
| const uint8_t Custom_1_Who_Am_I_Values[] = {0x4A, 0x5A} |
Define the WHO_AM_I register values for both possible sensor variations.
Definition at line 59 of file fsl_Sensor_Custom_1_Functions.c.
| const uint8_t Custom_1_Who_Am_I_Values[] |
Define the WHO_AM_I register values for both possible sensor variations.
Definition at line 59 of file fsl_Sensor_Custom_1_Functions.c.