![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | fxas21002_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
| struct | fxas21002_ODR_Table_tag |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation. More... | |
| struct | fxas21000_ODR_Table_tag |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21000 operation. More... | |
| struct | fxas21002_ConfigTable_tag |
| the structure defines the configuration table. More... | |
Macros | |
| #define | FXAS21002_WHO_AM_I_VALUE_PRE_RELEASE 0xD6 |
| Define the WHO_AM_I register values for both possible sensor variations. More... | |
| #define | FXAS21002_WHO_AM_I_VALUE_RELEASE 0xD7 |
| #define | FXAS21000_WHO_AM_I_VALUE 0xD1 |
Typedefs | |
| typedef int32 | fxas21002_Status_t |
| FXAS21002 internal return codes. More... | |
| typedef enum fxas21002_Power_tag | fxas21002_Power_t |
| Enumeration for the FXAS21002 power modes. More... | |
| typedef enum fxas21002_InternalState_tag | fxas21002_InternalState_t |
| Enumeration for the FXAS21002 driver internal states. More... | |
| typedef enum fxas21002_Range_tag | fxas21002_Range_t |
| typedef struct fxas21002_ODR_Table_tag | fxas21002_ODR_Table_t |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation. More... | |
| typedef struct fxas21000_ODR_Table_tag | fxas21000_ODR_Table_t |
| the structure defines the ODR table between Hybrid and normal mode of FXAS21000 operation. More... | |
| typedef struct fxas21002_ConfigTable_tag | fxas21002_ConfigTable_t |
| the structure defines the configuration table. More... | |
Enumerations | |
| enum | fxas21002_Error_tag { FXAS21002_ERROR_WHOAMI = 1, FXAS21002_ERROR_WAITFORACTIVE, FXAS21002_ERROR_BURSTWRITE, FXAS21002_ERROR_CONFIG, FXAS21002_ERROR_SETPOWER, FXAS21002_ERROR_WRITE, FXAS21002_ERROR_READ } |
| Enumeration for the FXAS21002 internal error codes. More... | |
| enum | fxas21002_Power_tag { FXAS21002_POWER_STANDBY = 0, FXAS21002_POWER_ACTIVE = 1 } |
| Enumeration for the FXAS21002 power modes. More... | |
| enum | fxas21002_InternalState_tag { FXAS21002_STATE_UNINTIALIZED, FXAS21002_STATE_INITIALIZED, FXAS21002_STATE_CONFIGURED, FXAS21002_STATE_STARTED } |
| Enumeration for the FXAS21002 driver internal states. More... | |
| enum | fxas21002_Range_tag { FXAS21002_RANGE_2000DPS = 0, FXAS21002_RANGE_1000DPS = 1, FXAS21002_RANGE_500DPS = 2, FXAS21002_RANGE_MAX = FXAS21002_RANGE_2000DPS } |
Functions | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Initialize (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter initialization. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSubSettings) |
| This is the concrete implementation of the FXAS21002 sensor adapter for validating current settings. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXAS21002 sensor adapter for configuration. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_StartData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter for start Data. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_EndData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter for End Data. More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| This is the concrete implementation of the FXAS21002 sensor adapter for calibration . More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXAS21002 sensor adapter for shutdown . More... | |
| void | fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback (void *pSensorHandle) |
| The callback function for the Bus Manager(BM). More... | |
| isf_dsa_status_t | fsl_fxas21002_i2cspi_3D_gyro_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
Variables | |
| isf_SensorTypes_t | fxas21002_SupportedSensorTypes [] |
| Supported sensor and data types for MMA8652. More... | |
| isf_SensorDataTypes_t | fxas21002_SupportedDataTypes [] |
| isf_SensorTypes_t | fxas21002_SupportedSensorTypes [] = { TYPE_THERMOMETER, TYPE_GYROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
| Supported sensor and data types for FXAS21002. More... | |
| isf_SensorDataTypes_t | fxas21002_SupportedDataTypes [] = { TYPE_TEMPERATURE, TYPE_ROTATIONAL_RATE_3D , TYPE_NATIVE_SENSOR_DATA_TYPE } |
| #define FXAS21000_WHO_AM_I_VALUE 0xD1 |
Definition at line 22 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| #define FXAS21002_WHO_AM_I_VALUE_PRE_RELEASE 0xD6 |
Define the WHO_AM_I register values for both possible sensor variations.
Definition at line 20 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| #define FXAS21002_WHO_AM_I_VALUE_RELEASE 0xD7 |
Definition at line 21 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| typedef struct fxas21000_ODR_Table_tag fxas21000_ODR_Table_t |
the structure defines the ODR table between Hybrid and normal mode of FXAS21000 operation.
| typedef struct fxas21002_ConfigTable_tag fxas21002_ConfigTable_t |
the structure defines the configuration table.
| typedef enum fxas21002_InternalState_tag fxas21002_InternalState_t |
Enumeration for the FXAS21002 driver internal states.
| typedef struct fxas21002_ODR_Table_tag fxas21002_ODR_Table_t |
the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation.
| typedef enum fxas21002_Power_tag fxas21002_Power_t |
Enumeration for the FXAS21002 power modes.
| typedef enum fxas21002_Range_tag fxas21002_Range_t |
| typedef int32 fxas21002_Status_t |
FXAS21002 internal return codes.
Definition at line 35 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| enum fxas21002_Error_tag |
Enumeration for the FXAS21002 internal error codes.
| Enumerator | |
|---|---|
| FXAS21002_ERROR_WHOAMI |
Error occurred while reading FXAS21002_WHO_AM_I or the value was incorrect. |
| FXAS21002_ERROR_WAITFORACTIVE |
Error occurred while attempting to put device into active mode. |
| FXAS21002_ERROR_BURSTWRITE |
Error occurred while attempting to write a block of memory to the device. |
| FXAS21002_ERROR_CONFIG |
Error occurred while attempting to configure the device. |
| FXAS21002_ERROR_SETPOWER |
Error occurred while attempting to set the power mode of the device. |
| FXAS21002_ERROR_WRITE |
Error occurred while attempting to write the registers directly. |
| FXAS21002_ERROR_READ |
Error occurred while attempting to read the registers directly. |
Definition at line 40 of file fsl_fxas21002_i2cspi_3D_gyro.h.
Enumeration for the FXAS21002 driver internal states.
Definition at line 59 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| enum fxas21002_Power_tag |
Enumeration for the FXAS21002 power modes.
| Enumerator | |
|---|---|
| FXAS21002_POWER_STANDBY |
Device in Standby mode. Less power consumption during the mode. |
| FXAS21002_POWER_ACTIVE |
Device in active mode. |
Definition at line 52 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| enum fxas21002_Range_tag |
| Enumerator | |
|---|---|
| FXAS21002_RANGE_2000DPS | |
| FXAS21002_RANGE_1000DPS | |
| FXAS21002_RANGE_500DPS | |
| FXAS21002_RANGE_MAX | |
Definition at line 66 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_Calibrate | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pCalData | ||
| ) |
This is the concrete implementation of the FXAS21002 sensor adapter for calibration .
The FXAS21000 does not provide the capability to be dynamically calibrated. Therefore, this function simply returns success.
| [in] | pSensorHandle | This is a pointer to the instance of the FXAS21002 sensor adapter. |
| [in] | pCalData | This is a void pointer to the calibration data. |
| ISF_SUCCESS | is returned when the device is calibrated properly. Note: Currently, there is no return error type defined for this API. |
Definition at line 564 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References ISF_SUCCESS.
| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_Configure | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
This is the concrete implementation of the FXAS21002 sensor adapter for configuration.
This function resets the sensor, applies the settings, and registers a callback with the Bus Manager(BM) timer. It does not yet start the timer, as this is done by fsl_fxas21002_i2cspi_3D_gyro_StartData().
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21000 sensor adapter. |
| [in] | pSensorSettings | The reference to the sensor configuration settings. |
| ISF_SUCCESS | is returned when the device is configured successfully. |
| DSA_ERR_CONFIGURE | is returned when the provided configuration settings could not be applied. |
Definition at line 306 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_register_periodic_callback(), DeviceDescriptor_struct::cDescriptor, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_acquire_lock(), dm_channel_release_lock(), dm_device_read(), dm_device_write(), DSA_ERR_CONFIGURE, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STOPPED, DSA_STATE_INITIALIZED, fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), FXAS21000_WHOAMI_VALUE, FXAS21002_ACTIVE_MASK, FXAS21002_CTRL_REG1, FXAS21002_READY_MASK, FXAS21002_SET_FIELD, ISF_SUCCESS, isf_dsa_SensorSettings_st::nSamplePeriod, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, fxas21002_Sensor_Specific_Reg_t::regAddr, fxas21002_Sensor_Specific_Settings_t::regCount, fxas21002_Sensor_Specific_Settings_t::regPairs, fxas21002_Sensor_Specific_Reg_t::regValue, DeviceDescriptor_struct::token, and whoami_read_val.

| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_Convert | ( | volatile isf_SensorHandle_t * | pSensorHandle, |
| isf_SensorDataTypes_t | convertToType, | ||
| isf_dsa_result_types_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32 * | numBytes | ||
| ) |
This function coverts the raw sample data to the desired output type.
Definition at line 727 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_RESULT_TYPE_ENG_FIXED, DSA_RESULT_TYPE_ENG_FLOAT, DSA_RESULT_TYPE_RAW_COUNTS, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, TYPE_ROTATIONAL_RATE_3D, and TYPE_TEMPERATURE.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback().

| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_EndData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXAS21002 sensor adapter for End Data.
This function tells the Bus Manager to stop the callbacks and disable data collection.
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21002 sensor adapter. |
| ISF_SUCCESS | is returned when the data collection stopped successfully. |
| DSA_ERR_PARAM | is returned when a wrong parameter is passed into the function such as an invalid or NULL parameter. |
Definition at line 498 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_stop(), DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_END_DATA, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FXAS21002_POWER_STANDBY, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_Initialize | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXAS21002 sensor adapter initialization.
This function allocates memory for the device descriptor.
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21002 sensor adapter. |
| ISF_SUCCESS | is returned when the device is initialized properly. |
| DSA_ERR_PARAM | is returned when a wrong parameter was passed into the function, i.e. an invalid or NULL parameter. |
| DSA_ERR_INITIALIZE | is returned when the driver could not be initialized successfully. |
Definition at line 181 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References isf_SensorHandle_st::adapterStatus, DeviceDescriptor_struct::cDescriptor, SensorConfig_st::channelId, COMM_STATE_OK, SensorConfig_st::commInfo, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_get_state(), dm_channel_init(), dm_channel_start(), dm_device_open(), DSA_ERR_INITIALIZE, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, DSA_STATE_NOT_INITIALIZED, FXAS21000_WHOAMI_VALUE, FXAS21002_WHOAMI_VALUE_PRE_RELEASE, FXAS21002_WHOAMI_VALUE_RELEASE, fxas21002_DataBuffer_t::gyro, ISF_SUCCESS, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_SensorHandle_st::pSensorStaticConfig, DeviceDescriptor_struct::skipFramecnt, and fxas21002_DataBuffer_t::timeStamp.

| void fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback | ( | void * | pSensorHandle | ) |
The callback function for the Bus Manager(BM).
The Bus Manager calls this function periodically based on the period configured for the FXAS21002.
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21002 sensor adapter. |
Definition at line 611 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References isf_SensorHandle_st::adapterStatus, isf_SensorHandle_st::controlData, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_device_read(), DSA_STATE_CONFIGURED_STARTED, fsl_fxas21002_i2cspi_3D_gyro_Convert(), FXAS21002_OUT_X_MSB, FXAS21002_TEMP, fxas21002_DataBuffer_t::gyro, isf_fifo_el_get_insert_pointer(), isf_fifo_el_increment(), ISF_FIFO_FULL, isf_fifo_lock(), isf_fifo_unlock(), isf_swap2byte(), isf_time_util_get_usec(), MAX_BUF_SIZE, MAX_DATA_READ_SIZE, isf_dsa_ControlData_st::nEventFieldIndex, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_dsa_ControlData_st::pEventGroup, isf_dsa_SensorSettings_st::pSampleBufferInfo, isf_dsa_SensorSettings_st::resultFormat, isf_dsa_SensorSettings_st::resultType, isf_dsa_ControlData_st::sensorSettings, DeviceDescriptor_struct::skipFramecnt, fxas21002_DataBuffer_t::temperature, TEMPERATURE_BUF_SIZE, TEMPERATURE_DATA_READ_SIZE, fxas21002_DataBuffer_t::timeStamp, and TYPE_NATIVE_SENSOR_DATA_TYPE.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure().


| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_Shutdown | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXAS21002 sensor adapter for shutdown .
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21002 sensor adapter. |
| ISF_SUCCESS | is returned when the device is calibrated properly. Note: Currently, there is no return error type defined for this API. |
Definition at line 581 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References isf_SensorHandle_st::adapterStatus, bm_unregister_callback(), DSA_ERR_PARAM, DSA_ERR_SHUTDOWN, DSA_STATE_INITIALIZED, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_StartData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXAS21002 sensor adapter for start Data.
This function tells the Bus Manager to start the callbacks periodically as defined in the bus configuration and enable the data collection.
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21002 sensor adapter. |
| ISF_SUCCESS | is returned when the data collection callback triggered successfully. |
| DSA_ERR_PARAM | is returned when a wrong parameter is passed into the function such as an invalid or NULL parameter. |
Definition at line 436 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_start(), DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_PARAM, DSA_ERR_START_DATA, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FALSE, FXAS21002_POWER_ACTIVE, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_fxas21002_i2cspi_3D_gyro_ValidateSettings | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
This is the concrete implementation of the FXAS21002 sensor adapter for validating current settings.
This function is responsible for validating the current settings and if the current settings are not valid settings, it provides the best suitable settings.
| [in] | pSensorHandle | This is a void pointer to the instance of the FXAS21002 sensor adapter. |
| [in] | pSensorSettings | The reference to the sensor settings. |
| ISF_SUCCESS | is returned when the device settings are successfully validated. |
| DSA_RET_SETTINGS_CHANGED | is returned when the current settings have been changed. |
Definition at line 267 of file fsl_fxas21002_i2cspi_3D_gyro.c.
References DSA_ERR_PARAM, DSA_RET_SETTINGS_CHANGED, ISF_SUCCESS, and isf_dsa_SensorSettings_st::nSamplePeriod.
| isf_SensorDataTypes_t fxas21002_SupportedDataTypes = { TYPE_TEMPERATURE, TYPE_ROTATIONAL_RATE_3D , TYPE_NATIVE_SENSOR_DATA_TYPE } |
Definition at line 55 of file fsl_fxas21002_i2cspi_3D_gyro.c.
| isf_SensorDataTypes_t fxas21002_SupportedDataTypes[] |
Definition at line 254 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| isf_SensorTypes_t fxas21002_SupportedSensorTypes = { TYPE_THERMOMETER, TYPE_GYROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
Supported sensor and data types for FXAS21002.
Supported sensor and data types for MMA8652.
Definition at line 54 of file fsl_fxas21002_i2cspi_3D_gyro.c.
| isf_SensorTypes_t fxas21002_SupportedSensorTypes[] |
Supported sensor and data types for MMA8652.
Supported sensor and data types for MMA8652.
Definition at line 253 of file fsl_fxas21002_i2cspi_3D_gyro.h.