![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | fxlc95000_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
| struct | fxlc95000_DeviceDescriptor_t |
Variables | |
| isf_SensorTypes_t | fxlc95000_SupportedSensorTypes [] |
| Supported sensor and data types for FXLC95000. More... | |
| isf_SensorDataTypes_t | fxlc95000_SupportedDataTypes [] |
| isf_dsa_status_t fsl_fxlc95000_Calibrate | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pCalData | ||
| ) |
Definition at line 376 of file fsl_fxlc95000_i2cspi_pedo.c.
References ISF_SUCCESS.
| isf_dsa_status_t fsl_fxlc95000_Configure | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 166 of file fsl_fxlc95000_i2cspi_pedo.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_register_periodic_callback(), bm_unregister_callback(), isf_SensorHandle_st::controlData, fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_DeviceDescriptor_t::deviceSemaphore, DSA_ERR_CONFIGURE, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STOPPED, DSA_STATE_INITIALIZED, fsl_fxlc95000_PeriodicCallback(), fxlc95000_GetConfig(), fxlc95000_send(), fxlc95000_WriteConfig(), ISF_SUCCESS, isf_swap4byte(), fxlc95000_DeviceDescriptor_t::localCfgBuffer, fxlc95000_SensorSetting_t::nCurrentReportRate, fxlc95000_SensorSetting_t::nCurrentResolution, fxlc95000_SensorSetting_t::nMode, fxlc95000_SensorSetting_t::nRange, isf_dsa_SensorSettings_st::nSamplePeriod, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, isf_dsa_ControlData_st::sensorSettings, fxlc95000_appConfigRegister_t::settings, and fxlc95000_DeviceDescriptor_t::token.

| isf_dsa_status_t fsl_fxlc95000_Convert | ( | volatile isf_SensorHandle_t * | pSensorHandle, |
| isf_SensorDataTypes_t | convertToType, | ||
| isf_dsa_result_types_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32 * | numBytes | ||
| ) |
This function converts the raw sample data to the desired output type.
Definition at line 652 of file fsl_fxlc95000_i2cspi_pedo.c.
References DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_RESULT_TYPE_ENG_FIXED, DSA_RESULT_TYPE_ENG_FLOAT, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and TYPE_RAW_ACCELERATION_3D.
Referenced by fsl_fxlc95000_Flash(), and fsl_fxlc95000_PeriodicCallback().

| isf_dsa_status_t fsl_fxlc95000_EndData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 315 of file fsl_fxlc95000_i2cspi_pedo.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_stop(), fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_DeviceDescriptor_t::deviceSemaphore, DSA_ERR_END_DATA, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, fxlc95000_send(), ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and fxlc95000_DeviceDescriptor_t::token.

| isf_dsa_status_t fsl_fxlc95000_Flash | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pFlashData, | ||
| uint8 | numBytes | ||
| ) |
Definition at line 530 of file fsl_fxlc95000_i2cspi_pedo.c.
References CI_READ_WRITE_ADDR_LEN, CI_READ_WRITE_HDR_LEN, CI_READ_WRITE_MAX_LEN, DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_PARAM, FALSE, fxlc95000_Sensor_Specific_Settings_t::flashPostprocessCommands, fxlc95000_Sensor_Specific_Settings_t::flashPreprocessCommands, fsl_fxlc95000_Convert(), fxlc95000_send(), ISF_SUCCESS, fxlc95000_CommandList_t::numCommands, fxlc95000_Command_t::offset, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and TRUE.

| isf_dsa_status_t fsl_fxlc95000_Initialize | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 56 of file fsl_fxlc95000_i2cspi_pedo.c.
References isf_SensorHandle_st::adapterStatus, fxlc95000_DeviceDescriptor_t::cDescriptor, SensorConfig_st::channelId, COMM_STATE_OK, SensorConfig_st::commInfo, fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_DeviceDescriptor_t::deviceSemaphore, dm_channel_get_state(), dm_channel_init(), dm_channel_start(), dm_device_open(), DSA_ERR_INITIALIZE, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, DSA_STATE_NOT_INITIALIZED, ISF_SUCCESS, fxlc95000_DeviceDescriptor_t::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, and isf_SensorHandle_st::pSensorStaticConfig.

| void fsl_fxlc95000_PeriodicCallback | ( | void * | pSensorHandle | ) |
Definition at line 431 of file fsl_fxlc95000_i2cspi_pedo.c.
References isf_SensorHandle_st::adapterStatus, isf_SensorHandle_st::controlData, fxlc95000_DeviceDescriptor_t::deviceSemaphore, DSA_STATE_CONFIGURED_STARTED, fsl_fxlc95000_Convert(), fxlc95000_GetData(), isf_fifo_el_get_insert_pointer(), isf_fifo_el_increment(), ISF_FIFO_FULL, isf_fifo_lock(), isf_fifo_unlock(), isf_dsa_ControlData_st::nEventFieldIndex, fxlc95000_DeviceDescriptor_t::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_dsa_ControlData_st::pEventGroup, isf_dsa_SensorSettings_st::pSampleBufferInfo, isf_dsa_SensorSettings_st::resultFormat, isf_dsa_SensorSettings_st::resultType, isf_dsa_ControlData_st::sensorSettings, fxlc95000_DataBuffer_t::timeStamp, and TYPE_NATIVE_SENSOR_DATA_TYPE.
Referenced by fsl_fxlc95000_Configure().


| isf_dsa_status_t fsl_fxlc95000_Shutdown | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 396 of file fsl_fxlc95000_i2cspi_pedo.c.
References isf_SensorHandle_st::adapterStatus, bm_unregister_callback(), fxlc95000_DeviceDescriptor_t::deviceHandle, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, fxlc95000_send(), ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and fxlc95000_DeviceDescriptor_t::token.

| isf_dsa_status_t fsl_fxlc95000_StartData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 256 of file fsl_fxlc95000_i2cspi_pedo.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_start(), fxlc95000_DeviceDescriptor_t::deviceHandle, fxlc95000_DeviceDescriptor_t::deviceSemaphore, DSA_ERR_PARAM, DSA_ERR_START_DATA, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FALSE, fxlc95000_send(), ISF_SUCCESS, fxlc95000_CommandList_t::numCommands, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, fxlc95000_Sensor_Specific_Settings_t::startDataCommands, and fxlc95000_DeviceDescriptor_t::token.

| isf_dsa_status_t fsl_fxlc95000_ValidateSettings | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSubSettings | ||
| ) |
Definition at line 133 of file fsl_fxlc95000_i2cspi_pedo.c.
References DSA_ERR_PARAM, and fxlc95000_ValidateConfig().

| isf_SensorDataTypes_t fxlc95000_SupportedDataTypes[] |
Definition at line 28 of file fsl_fxlc95000_i2cspi_pedo.c.
| isf_SensorTypes_t fxlc95000_SupportedSensorTypes[] |
Supported sensor and data types for FXLC95000.
Supported sensor and data types for FXLC95000.
Definition at line 27 of file fsl_fxlc95000_i2cspi_pedo.c.