![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | fxls8952_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
| struct | fxls8952_ODR_Table_tag |
| the structure defines the ODR table between Hybrid and normal mode of device operation. More... | |
| struct | fxls8952_ConfigTable_tag |
| the structure defines the configuration table. More... | |
Macros | |
| #define | FXLS8952_ACCEL_FLOAT_CONVERSION_FACTOR (0.1) |
| #define | FXLS8952_ACCEL_FLOAT_CONVERSION_OFFSET (0.0) |
| #define | FXLS8952_ACCEL_FIXED_CONVERSION_FACTOR (1638) |
| #define | FXLS8952_ACCEL_FIXED_CONVERSION_OFFSET (0) |
| #define | MAX_ACCEL_FULL_SCALE_RANGE FXLS8952_RANGE_MAX |
| #define | FXLS8952_SAMPLE_PERIOD_MAX 1280409 |
| #define | FXLS8952_SAMPLE_PERIOD_MIN 312 |
| #define | GET_ODR_CONFIG 0x0 |
| #define | GET_ODR_VALUE 0x01 |
| #define | NUM_STATUS_BYTES 1 |
| #define | NUMBER_OF_AXES_3D 0x3 |
| #define | MAX_NUM_AXES 0x3 |
| #define | MAX_FXLS8952_DM_BYTES 0x30 |
| #define | NUM_INTERNAL_ADDRESS_BYTES 0x1 |
| #define | ASSIGN_REG_BITS_VALUE(addr, val, mask, shift) (addr) = (((addr) & ~ (mask)) | (((val) << shift)& (mask)) ) |
| #define | GET_MODE(mode) ((mode) <= FXLS8952_MODE_HYBRID) ? (mode) : FXLS8952_MODE_HYBRID |
| #define | GET_STRUCT_MEMBER_ADDRESS(p, m) (&(p)->m) |
| #define | GET_MEMBER_SIZE(p, m) sizeof((p)->m) |
| #define | FXLS8952_WHO_AM_I_VALUE 0x18 |
Typedefs | |
| typedef int32 | fxls8952_Status_t |
| fxls8952 internal return codes. More... | |
| typedef enum fxls8952_Power_tag | fxls8952_Power_t |
| Enumeration for the fxls8952 power modes. More... | |
| typedef enum fxls8952_InternalState_tag | fxls8952_InternalState_t |
| Enumeration for the fxls8952 driver internal states. More... | |
| typedef enum fxls8952_Range_tag | fxls8952_Range_t |
| typedef struct fxls8952_ODR_Table_tag | fxls8952_ODR_Table_t |
| the structure defines the ODR table between Hybrid and normal mode of device operation. More... | |
| typedef struct fxls8952_ConfigTable_tag | fxls8952_ConfigTable_t |
| the structure defines the configuration table. More... | |
Enumerations | |
| enum | fxls8952_Error_tag { FXLS8952_ERROR_WHOAMI = 1, FXLS8952_ERROR_WAITFORACTIVE, FXLS8952_ERROR_BURSTWRITE, FXLS8952_ERROR_CONFIG, FXLS8952_ERROR_SETPOWER, FXLS8952_ERRO_WRITE, FXLS8952_ERRO_READ } |
| Enumeration for the fxls8952 internal error codes. More... | |
| enum | fxls8952_Power_tag { FXLS8952_POWER_STANDBY = 0, FXLS8952_POWER_ACTIVE = 1 } |
| Enumeration for the fxls8952 power modes. More... | |
| enum | fxls8952_InternalState_tag { FXLS8952_STATE_UNINTIALIZED, FXLS8952_STATE_INITIALIZED, FXLS8952_STATE_CONFIGURED, FXLS8952_STATE_STARTED } |
| Enumeration for the fxls8952 driver internal states. More... | |
| enum | fxls8952_Range_tag { FXLS8952_RANGE_2G = 0, FXLS8952_RANGE_4G = 1, FXLS8952_RANGE_8G = 2, FXLS8952_RANGE_16G = 3, FXLS8952_RANGE_MAX = FXLS8952_RANGE_16G } |
Functions | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Initialize (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter initialization. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXLS8952 sensor adapter for validating current settings. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| This is the concrete implementation of the FXLS8952 sensor adapter for configuration. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_StartData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for start Data. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_EndData (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for End Data. More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| This is the concrete implementation of the FXLS8952 sensor adapter for calibration . More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| This is the concrete implementation of the FXLS8952 sensor adapter for shutdown . More... | |
| void | fsl_fxls8952_i2c_3D_accel_PeriodicCallback (void *pSensorHandle) |
| The callback function for the Bus Manager(BM). More... | |
| isf_dsa_status_t | fsl_fxls8952_i2c_3D_accel_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
Variables | |
| uint8 | LE_BE_check =0 |
| isf_SensorTypes_t | fxls8952_SupportedSensorTypes [] = { TYPE_ACCELEROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
| Supported sensor and data types for FXLS8952. More... | |
| isf_SensorDataTypes_t | fxls8952_SupportedDataTypes [] = { TYPE_RAW_ACCELERATION_3D , TYPE_NATIVE_SENSOR_DATA_TYPE } |
| const fxls8952_ODR_Table_t | fxls8952_odrTable [] |
| The table that describes the configuration value based on ODR (output data rate). Note: This table is irregular after the 25HZ, so can't use FLOORLOG2 algorithm. More... | |
| float floatFactor | |
| float floatOffset | |
| int32 fixedFactor | |
| int32 fixedOffset | |
| struct { | |
| float floatFactor | |
| float floatOffset | |
| int32 fixedFactor | |
| int32 fixedOffset | |
| } | fxls8952AccelConvTable [] |
| isf_SensorTypes_t | fxls8952_SupportedSensorTypes [] |
| Supported sensor and data types for MMA8652. More... | |
| isf_SensorDataTypes_t | fxls8952_SupportedDataTypes [] |
| #define ASSIGN_REG_BITS_VALUE | ( | addr, | |
| val, | |||
| mask, | |||
| shift | |||
| ) | (addr) = (((addr) & ~ (mask)) | (((val) << shift)& (mask)) ) |
Definition at line 102 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_ACCEL_FIXED_CONVERSION_FACTOR (1638) |
Definition at line 82 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_ACCEL_FIXED_CONVERSION_OFFSET (0) |
Definition at line 83 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_ACCEL_FLOAT_CONVERSION_FACTOR (0.1) |
Definition at line 80 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_ACCEL_FLOAT_CONVERSION_OFFSET (0.0) |
Definition at line 81 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_SAMPLE_PERIOD_MAX 1280409 |
Definition at line 87 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_SAMPLE_PERIOD_MIN 312 |
Definition at line 88 of file fsl_fxls8952_i2c_3D_accel.c.
| #define FXLS8952_WHO_AM_I_VALUE 0x18 |
Definition at line 27 of file fsl_fxls8952_i2c_3D_accel.h.
| #define GET_MEMBER_SIZE | ( | p, | |
| m | |||
| ) | sizeof((p)->m) |
Definition at line 110 of file fsl_fxls8952_i2c_3D_accel.c.
| #define GET_MODE | ( | mode | ) | ((mode) <= FXLS8952_MODE_HYBRID) ? (mode) : FXLS8952_MODE_HYBRID |
Definition at line 105 of file fsl_fxls8952_i2c_3D_accel.c.
| #define GET_ODR_CONFIG 0x0 |
Definition at line 89 of file fsl_fxls8952_i2c_3D_accel.c.
| #define GET_ODR_VALUE 0x01 |
Definition at line 90 of file fsl_fxls8952_i2c_3D_accel.c.
| #define GET_STRUCT_MEMBER_ADDRESS | ( | p, | |
| m | |||
| ) | (&(p)->m) |
Definition at line 108 of file fsl_fxls8952_i2c_3D_accel.c.
| #define MAX_ACCEL_FULL_SCALE_RANGE FXLS8952_RANGE_MAX |
Definition at line 85 of file fsl_fxls8952_i2c_3D_accel.c.
| #define MAX_FXLS8952_DM_BYTES 0x30 |
Definition at line 96 of file fsl_fxls8952_i2c_3D_accel.c.
| #define MAX_NUM_AXES 0x3 |
Definition at line 95 of file fsl_fxls8952_i2c_3D_accel.c.
| #define NUM_INTERNAL_ADDRESS_BYTES 0x1 |
Definition at line 98 of file fsl_fxls8952_i2c_3D_accel.c.
| #define NUM_STATUS_BYTES 1 |
Definition at line 92 of file fsl_fxls8952_i2c_3D_accel.c.
| #define NUMBER_OF_AXES_3D 0x3 |
Definition at line 94 of file fsl_fxls8952_i2c_3D_accel.c.
| typedef struct fxls8952_ConfigTable_tag fxls8952_ConfigTable_t |
the structure defines the configuration table.
| typedef enum fxls8952_InternalState_tag fxls8952_InternalState_t |
Enumeration for the fxls8952 driver internal states.
| typedef struct fxls8952_ODR_Table_tag fxls8952_ODR_Table_t |
the structure defines the ODR table between Hybrid and normal mode of device operation.
| typedef enum fxls8952_Power_tag fxls8952_Power_t |
Enumeration for the fxls8952 power modes.
| typedef enum fxls8952_Range_tag fxls8952_Range_t |
| typedef int32 fxls8952_Status_t |
fxls8952 internal return codes.
Definition at line 39 of file fsl_fxls8952_i2c_3D_accel.h.
| enum fxls8952_Error_tag |
Enumeration for the fxls8952 internal error codes.
| Enumerator | |
|---|---|
| FXLS8952_ERROR_WHOAMI |
Error occurred while reading FXLS8952_WHO_AM_I or the value was incorrect. |
| FXLS8952_ERROR_WAITFORACTIVE |
Error occurred while attempting to put device into active mode. |
| FXLS8952_ERROR_BURSTWRITE |
Error occurred while attempting to write a block of memory to the device. |
| FXLS8952_ERROR_CONFIG |
Error occurred while attempting to configure the device. |
| FXLS8952_ERROR_SETPOWER |
Error occurred while attempting to set the power mode of the device. |
| FXLS8952_ERRO_WRITE |
Error occurred while attempting to write the registers directly. |
| FXLS8952_ERRO_READ |
Error occurred while attempting to read the registers directly. |
Definition at line 44 of file fsl_fxls8952_i2c_3D_accel.h.
Enumeration for the fxls8952 driver internal states.
Definition at line 63 of file fsl_fxls8952_i2c_3D_accel.h.
| enum fxls8952_Power_tag |
Enumeration for the fxls8952 power modes.
| Enumerator | |
|---|---|
| FXLS8952_POWER_STANDBY |
Device in Standby mode. Less power consumption during the mode. |
| FXLS8952_POWER_ACTIVE |
Device in active mode. |
Definition at line 56 of file fsl_fxls8952_i2c_3D_accel.h.
| enum fxls8952_Range_tag |
| Enumerator | |
|---|---|
| FXLS8952_RANGE_2G | |
| FXLS8952_RANGE_4G | |
| FXLS8952_RANGE_8G | |
| FXLS8952_RANGE_16G | |
| FXLS8952_RANGE_MAX | |
Definition at line 70 of file fsl_fxls8952_i2c_3D_accel.h.
| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_Calibrate | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pCalData | ||
| ) |
This is the concrete implementation of the FXLS8952 sensor adapter for calibration .
The FXLS8952 does not provide the capability to be dynamically calibrated. Therefore, this function simply returns success.
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| ISF_SUCCESS | is returned when the device is calibrated properly. Note: Currently, there is no return error type defined for this API. |
Definition at line 578 of file fsl_fxls8952_i2c_3D_accel.c.
References ISF_SUCCESS.
| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_Configure | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
This is the concrete implementation of the FXLS8952 sensor adapter for configuration.
This function resets the sensor, applies the settings, and registers a callback with the Bus Manager(BM) timer. It does not yet start the timer, as this is done by fsl_FXLS8952_i2c_3D_accel_StartData().
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| [in] | pConfig | The reference to the sensor configuration settings. |
| ISF_SUCCESS | is returned when the device is configured successfully. |
| DSA_ERR_CONFIGURE | is returned when the provided configuration settings could not be applied. |
Definition at line 309 of file fsl_fxls8952_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_register_periodic_callback(), DeviceDescriptor_struct::cDescriptor, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_acquire_lock(), dm_channel_release_lock(), dm_device_read(), dm_device_write(), DSA_ERR_CONFIGURE, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STOPPED, DSA_STATE_INITIALIZED, fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), FXLS8952_ACTIVE_MASK, FXLS8952_LE_BE_MASK, FXLS8952_SENS_CONFIG1, FXLS8952_SENS_CONFIG3, FXLS8952_SET_FIELD, isf_EventHandler_GetSignal(), isf_EventHandler_RegisterEvent(), ISF_SUCCESS, LE_BE_check, isf_dsa_SensorSettings_st::nSamplePeriod, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, fxls8952_Sensor_Specific_Reg_t::regAddr, fxls8952_Sensor_Specific_Settings_t::regCount, fxls8952_Sensor_Specific_Settings_t::regPairs, fxls8952_Sensor_Specific_Reg_t::regValue, fxls8952_Sensor_Specific_Settings_t::signal, DeviceDescriptor_struct::token, and fxls8952_Sensor_Specific_Settings_t::usesInterrupts.

| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_Convert | ( | volatile isf_SensorHandle_t * | pSensorHandle, |
| isf_SensorDataTypes_t | convertToType, | ||
| isf_dsa_result_types_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32 * | numBytes | ||
| ) |
This function coverts the raw sample data to the desired output type.
Definition at line 801 of file fsl_fxls8952_i2c_3D_accel.c.
References DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_RESULT_TYPE_ENG_FIXED, DSA_RESULT_TYPE_ENG_FLOAT, DSA_RESULT_TYPE_RAW_COUNTS, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and TYPE_RAW_ACCELERATION_3D.
Referenced by fsl_fxls8952_i2c_3D_accel_PeriodicCallback().

| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_EndData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXLS8952 sensor adapter for End Data.
This function tells the Bus Manager to stop the callbacks and disable data collection.
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| ISF_SUCCESS | is returned when the data collection stopped successfully. |
| DSA_ERR_PARAM | is returned when a wrong parameter is passed into the function such as an invalid or NULL parameter. |
Definition at line 517 of file fsl_fxls8952_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_stop(), DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_END_DATA, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FXLS8952_POWER_STANDBY, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_Initialize | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXLS8952 sensor adapter initialization.
This function allocates memory for the device descriptor.
| [in] | pSensorHandle | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| ISF_SUCCESS | is returned when the device is initialized properly. |
| DSA_ERR_PARAM | is returned when a wrong parameter was passed into the function, i.e. an invalid or NULL parameter. |
| DSA_ERR_INITIALIZE | is returned when the driver could not be initialized successfully. |
Definition at line 179 of file fsl_fxls8952_i2c_3D_accel.c.
References fxls8952_DataBuffer_t::accel, isf_SensorHandle_st::adapterStatus, DeviceDescriptor_struct::cDescriptor, SensorConfig_st::channelId, COMM_STATE_OK, SensorConfig_st::commInfo, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_get_state(), dm_channel_init(), dm_channel_start(), dm_device_open(), DSA_ERR_INITIALIZE, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, DSA_STATE_NOT_INITIALIZED, FXLS8952_WHOAMI_VALUE, ISF_SUCCESS, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_SensorHandle_st::pSensorStaticConfig, DeviceDescriptor_struct::skipFramecnt, and fxls8952_DataBuffer_t::timeStamp.

| void fsl_fxls8952_i2c_3D_accel_PeriodicCallback | ( | void * | pSensorHandle | ) |
The callback function for the Bus Manager(BM).
The Bus Manager calls this function periodically based on the period configured for the FXLS8952.
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
Definition at line 634 of file fsl_fxls8952_i2c_3D_accel.c.
References fxls8952_DataBuffer_t::accel, isf_SensorHandle_st::adapterStatus, isf_SensorHandle_st::controlData, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_device_read(), dm_device_write(), DSA_STATE_CONFIGURED_STARTED, fsl_fxls8952_i2c_3D_accel_Convert(), FXLS8952_BUF_CONFIG2, FXLS8952_BUF_FLUSH_MASK, FXLS8952_BUF_STATUS, FXLS8952_BUF_X_LSB, FXLS8952_GET_FIELD, FXLS8952_INT_STATUS, FXLS8952_OUT_X_LSB, FXLS8952_SYS_MODE, isf_fifo_el_get_insert_pointer(), isf_fifo_el_increment(), ISF_FIFO_FULL, isf_fifo_lock(), isf_fifo_unlock(), isf_swap2byte(), isf_time_util_get_usec(), LE_BE_check, isf_dsa_ControlData_st::nEventFieldIndex, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_dsa_ControlData_st::pEventGroup, isf_dsa_SensorSettings_st::pSampleBufferInfo, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, isf_dsa_SensorSettings_st::resultFormat, isf_dsa_SensorSettings_st::resultType, fxls8952_Sensor_Specific_Settings_t::samplePeriod, isf_dsa_ControlData_st::sensorSettings, DeviceDescriptor_struct::skipFramecnt, fxls8952_DataBuffer_t::timeStamp, TYPE_NATIVE_SENSOR_DATA_TYPE, and fxls8952_Sensor_Specific_Settings_t::usesBuffer.
Referenced by fsl_fxls8952_i2c_3D_accel_Configure().


| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_Shutdown | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXLS8952 sensor adapter for shutdown .
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| ISF_SUCCESS | is returned when the device is calibrated properly. Note: Currently, there is no return error type defined for this API. |
Definition at line 595 of file fsl_fxls8952_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, bm_unregister_callback(), DSA_ERR_PARAM, DSA_STATE_INITIALIZED, isf_EventHandler_UnregisterEvent(), ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, DeviceDescriptor_struct::token, and fxls8952_Sensor_Specific_Settings_t::usesInterrupts.

| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_StartData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
This is the concrete implementation of the FXLS8952 sensor adapter for start Data.
This function tells the Bus Manager to start the callbacks periodically as defined in the bus configuration and enable the data collection.
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| ISF_SUCCESS | is returned when the data collection callback triggered successfully. |
| DSA_ERR_PARAM | is returned when a wrong parameter is passed into the function such as an invalid or NULL parameter. |
Definition at line 450 of file fsl_fxls8952_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_start(), DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_PARAM, DSA_ERR_START_DATA, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FALSE, FXLS8952_POWER_ACTIVE, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, DeviceDescriptor_struct::token, and fxls8952_Sensor_Specific_Settings_t::usesInterrupts.

| isf_dsa_status_t fsl_fxls8952_i2c_3D_accel_ValidateSettings | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
This is the concrete implementation of the FXLS8952 sensor adapter for validating current settings.
This function is responsible for validating the current settings and if the current settings are not valid settings, it provides the best suitable settings.
| [in] | pSensorHdl | This is a void pointer to the instance of the FXLS8952 sensor adapter. |
| [in] | pSettings | The reference to the sensor settings. |
| ISF_SUCCESS | is returned when the device settings are successfully validated. |
| ::SM_DSA_RET_SETTINGS_CHANGED | is returned when the current settings have been changed. |
Definition at line 264 of file fsl_fxls8952_i2c_3D_accel.c.
References DSA_ERR_PARAM, ISF_SUCCESS, isf_dsa_SensorSettings_st::nSamplePeriod, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and fxls8952_Sensor_Specific_Settings_t::samplePeriod.
| int32 fixedFactor |
Definition at line 148 of file fsl_fxls8952_i2c_3D_accel.c.
| int32 fixedFactor |
Definition at line 148 of file fsl_fxls8952_i2c_3D_accel.c.
| int32 fixedOffset |
Definition at line 149 of file fsl_fxls8952_i2c_3D_accel.c.
| int32 fixedOffset |
Definition at line 149 of file fsl_fxls8952_i2c_3D_accel.c.
| float floatFactor |
Definition at line 146 of file fsl_fxls8952_i2c_3D_accel.c.
| float floatFactor |
Definition at line 146 of file fsl_fxls8952_i2c_3D_accel.c.
| float floatOffset |
Definition at line 147 of file fsl_fxls8952_i2c_3D_accel.c.
| float floatOffset |
Definition at line 147 of file fsl_fxls8952_i2c_3D_accel.c.
| const fxls8952_ODR_Table_t fxls8952_odrTable[] |
The table that describes the configuration value based on ODR (output data rate). Note: This table is irregular after the 25HZ, so can't use FLOORLOG2 algorithm.
The table that describes the configuration value based on ODR (output data rate). Note: This table is irregular after the 25HZ, so can't use FLOORLOG2 algorithm.
Definition at line 122 of file fsl_fxls8952_i2c_3D_accel.c.
| isf_SensorDataTypes_t fxls8952_SupportedDataTypes = { TYPE_RAW_ACCELERATION_3D , TYPE_NATIVE_SENSOR_DATA_TYPE } |
Definition at line 72 of file fsl_fxls8952_i2c_3D_accel.c.
| isf_SensorDataTypes_t fxls8952_SupportedDataTypes[] |
Definition at line 248 of file fsl_fxls8952_i2c_3D_accel.h.
| isf_SensorTypes_t fxls8952_SupportedSensorTypes = { TYPE_ACCELEROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
Supported sensor and data types for FXLS8952.
Supported sensor and data types for MMA8652.
Definition at line 71 of file fsl_fxls8952_i2c_3D_accel.c.
| isf_SensorTypes_t fxls8952_SupportedSensorTypes[] |
Supported sensor and data types for MMA8652.
Supported sensor and data types for MMA8652.
Definition at line 247 of file fsl_fxls8952_i2c_3D_accel.h.
| const { ... } fxls8952AccelConvTable[] |
| uint8 LE_BE_check =0 |
Definition at line 68 of file fsl_fxls8952_i2c_3D_accel.c.
Referenced by fsl_fxls8952_i2c_3D_accel_Configure(), and fsl_fxls8952_i2c_3D_accel_PeriodicCallback().