![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | mma865x_Specific_Settings_t |
| This structure defines important settings. More... | |
| struct | mma865x_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
Macros | |
| #define | BYTES_FOR_FULL_READ 7 |
| This function retrieves the raw data from the MMA865x sensor. More... | |
Typedefs | |
| typedef int32 | mma865x_status_t |
Enumerations | |
| enum | { FSL_MMA865x_ACCEL_800HZ = 1250, FSL_MMA865x_ACCEL_400HZ = 2500, FSL_MMA865x_ACCEL_200HZ = 5000, FSL_MMA865x_ACCEL_100HZ = 10000, FSL_MMA865x_ACCEL_50HZ = 20000, FSL_MMA865x_ACCEL_12p5HZ = 80000, FSL_MMA865x_ACCEL_6p25HZ = 160000, FSL_MMA865x_ACCEL_1p56HZ = 640000 } |
| This enumerator describes the available sample rates for the MM865X family of accelerometers. More... | |
| enum | { FSL_MMA865x_ACCEL_DATA_FULL = 0, FSL_MMA865x_ACCEL_DATA_8BIT = 1 } |
| This enumerator describes the available output resolutions for the MM865X family of accelerometers. More... | |
| enum | { FSL_MMA865x_ACCEL_SCALE_2G = 0, FSL_MMA865x_ACCEL_SCALE_4G = 1, FSL_MMA865x_ACCEL_SCALE_8G = 2 } |
| This enumerator describes the available acceleration ranges for the MM865X family of accelerometers. More... | |
Functions | |
| void | mma865x_Reset (int32_t *status, void *pSensorHandle) |
| This function resets the MMA865x sensor resulting in a default configuration for all registers. More... | |
| void | mma865x_CheckId (int32_t *status, void *pSensorHandle) |
| This function validates the MMA865x sensor is connected via the I2C bus. More... | |
| void | mma865x_SetMode (int32_t *status, void *pSensorHandle, int32_t Mode) |
| This function sets the MMA865x part to the requested mode. More... | |
| void | mma865x_ValidateConfig (int32_t *status, void *pSensorHandle, void *pSettings) |
| This function validates the configuration for the MMA865x sensor. More... | |
| isf_dsa_status_t | mma865x_GetConfig (isf_dsa_SensorSettings_t *pRequiredSettings, DeviceDescriptor_t *pDeviceDes) |
| This function obtains the configuration register values for a given user configuration of the MMA865x. If the configuration has changed then it returns true and saves the new configuration. More... | |
| isf_dsa_status_t | mma865x_SetConfig (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pConfigSettings) |
| This function sets the MMA865x sensor configuration. More... | |
| isf_dsa_status_t | mma865x_GetData (isf_SensorHandle_t *pSensorHandle, void *pBuffer) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Initialize (isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_StartData (isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_EndData (isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| void | fsl_mma865x_i2c_3D_accel_PeriodicCallback (void *pSensorHandle) |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
Variables | |
| struct { | |
| float floatFactor | |
| float floatOffset | |
| int32 fixedFactor | |
| int32 fixedOffset | |
| } | mma865xAccelConvTable [] |
| isf_SensorTypes_t | mma865x_SupportedSensorTypes [] = { TYPE_ACCELEROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
| Supported sensor and data types for MMA865x. More... | |
| isf_SensorDataTypes_t | mma865x_SupportedDataTypes [] = { TYPE_RAW_ACCELERATION_3D, TYPE_NATIVE_SENSOR_DATA_TYPE } |
| isf_SensorTypes_t | mma865x_SupportedSensorTypes [] |
| Supported sensor and data types for MMA865x. More... | |
| isf_SensorDataTypes_t | mma865x_SupportedDataTypes [] |
| #define BYTES_FOR_FULL_READ 7 |
This function retrieves the raw data from the MMA865x sensor.
Definition at line 816 of file fsl_mma865x_i2c_3D_accel.c.
Referenced by mma865x_GetData().
| typedef int32 mma865x_status_t |
Definition at line 72 of file fsl_mma865x_i2c_3D_accel.c.
| anonymous enum |
This enumerator describes the available sample rates for the MM865X family of accelerometers.
Definition at line 24 of file fsl_mma865x_i2c_3D_accel.h.
| anonymous enum |
This enumerator describes the available output resolutions for the MM865X family of accelerometers.
| Enumerator | |
|---|---|
| FSL_MMA865x_ACCEL_DATA_FULL |
select full-scale resolution |
| FSL_MMA865x_ACCEL_DATA_8BIT |
select 8-bit resolution |
Definition at line 36 of file fsl_mma865x_i2c_3D_accel.h.
| anonymous enum |
This enumerator describes the available acceleration ranges for the MM865X family of accelerometers.
| Enumerator | |
|---|---|
| FSL_MMA865x_ACCEL_SCALE_2G |
select +/-2G range |
| FSL_MMA865x_ACCEL_SCALE_4G |
select +/-4G range |
| FSL_MMA865x_ACCEL_SCALE_8G |
select +/-8G range |
Definition at line 42 of file fsl_mma865x_i2c_3D_accel.h.
| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_Calibrate | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pCalData | ||
| ) |
Definition at line 445 of file fsl_mma865x_i2c_3D_accel.c.
References ISF_SUCCESS.
| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_Configure | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 225 of file fsl_mma865x_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_register_periodic_callback(), DeviceDescriptor_struct::cDescriptor, isf_SensorHandle_st::controlData, DeviceDescriptor_struct::deviceSemaphore, dm_channel_acquire_lock(), dm_channel_release_lock(), DSA_ERR_CONFIGURE, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STOPPED, DSA_STATE_INITIALIZED, fsl_mma865x_i2c_3D_accel_PeriodicCallback(), ISF_SUCCESS, mma865x_SetConfig(), mma865x_SetMode(), isf_dsa_SensorSettings_st::nSamplePeriod, isf_SensorHandle_st::pDeviceDescriptor, SENSOR_STANDBY, isf_dsa_ControlData_st::sensorSettings, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_Convert | ( | volatile isf_SensorHandle_t * | pSensorHandle, |
| isf_SensorDataTypes_t | convertToType, | ||
| isf_dsa_result_types_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32 * | numBytes | ||
| ) |
This function coverts the raw sample data to the desired output type.
Definition at line 591 of file fsl_mma865x_i2c_3D_accel.c.
References DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_RESULT_TYPE_ENG_FIXED, DSA_RESULT_TYPE_ENG_FLOAT, DSA_RESULT_TYPE_RAW_COUNTS, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and TYPE_RAW_ACCELERATION_3D.
Referenced by fsl_mma865x_i2c_3D_accel_PeriodicCallback().

| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_EndData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 378 of file fsl_mma865x_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_stop(), DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_END_DATA, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, ISF_SUCCESS, mma865x_SetMode(), isf_SensorHandle_st::pDeviceDescriptor, SENSOR_STANDBY, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_Initialize | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 102 of file fsl_mma865x_i2c_3D_accel.c.
References mma865x_DataBuffer_t::accel, isf_SensorHandle_st::adapterStatus, mma865x_DataBuffer_t::addr, DeviceDescriptor_struct::cDescriptor, SensorConfig_st::channelId, COMM_STATE_OK, SensorConfig_st::commInfo, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_get_state(), dm_channel_init(), dm_channel_start(), dm_device_open(), DSA_ERR_INITIALIZE, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, DSA_STATE_NOT_INITIALIZED, ISF_SUCCESS, mma865x_CheckId(), DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_SensorHandle_st::pSensorStaticConfig, DeviceDescriptor_struct::skipFramecnt, and mma865x_DataBuffer_t::timeStamp.

| void fsl_mma865x_i2c_3D_accel_PeriodicCallback | ( | void * | pSensorHandle | ) |
Definition at line 494 of file fsl_mma865x_i2c_3D_accel.c.
References mma865x_DataBuffer_t::accel, isf_SensorHandle_st::adapterStatus, isf_SensorHandle_st::controlData, DeviceDescriptor_struct::deviceSemaphore, DSA_STATE_CONFIGURED_STARTED, fsl_mma865x_i2c_3D_accel_Convert(), isf_fifo_el_get_insert_pointer(), isf_fifo_el_increment(), ISF_FIFO_FULL, isf_fifo_lock(), isf_fifo_unlock(), isf_time_util_get_usec(), mma865x_GetData(), isf_dsa_ControlData_st::nEventFieldIndex, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_dsa_ControlData_st::pEventGroup, isf_dsa_SensorSettings_st::pSampleBufferInfo, isf_dsa_SensorSettings_st::resultFormat, isf_dsa_SensorSettings_st::resultType, isf_dsa_ControlData_st::sensorSettings, DeviceDescriptor_struct::skipFramecnt, mma865x_DataBuffer_t::timeStamp, and TYPE_NATIVE_SENSOR_DATA_TYPE.
Referenced by fsl_mma865x_i2c_3D_accel_Configure().


| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_Shutdown | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 465 of file fsl_mma865x_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, bm_unregister_callback(), DSA_ERR_PARAM, DSA_STATE_INITIALIZED, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_StartData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 316 of file fsl_mma865x_i2c_3D_accel.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_start(), DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_PARAM, DSA_ERR_START_DATA, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FALSE, ISF_SUCCESS, mma865x_SetMode(), isf_SensorHandle_st::pDeviceDescriptor, SENSOR_ACTIVE, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mma865x_i2c_3D_accel_ValidateSettings | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 196 of file fsl_mma865x_i2c_3D_accel.c.
References DSA_ERR_PARAM, and mma865x_ValidateConfig().

| void mma865x_CheckId | ( | int32_t * | status, |
| void * | pSensorHandle | ||
| ) |
This function validates the MMA865x sensor is connected via the I2C bus.
Definition at line 707 of file fsl_mma865x_i2c_3D_accel.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_read(), ISF_SUCCESS, MMA865x_WHO_AM_I, MMA865x_WHOAMI_VALUE_8652, MMA865x_WHOAMI_VALUE_8653, isf_SensorHandle_st::pDeviceDescriptor, and SENSOR_ERROR_CHECKID.
Referenced by fsl_mma865x_i2c_3D_accel_Initialize().


| isf_dsa_status_t mma865x_GetConfig | ( | isf_dsa_SensorSettings_t * | pRequiredSettings, |
| DeviceDescriptor_t * | pDeviceDes | ||
| ) |
This function obtains the configuration register values for a given user configuration of the MMA865x. If the configuration has changed then it returns true and saves the new configuration.
| [out] | pRequiredSettings | update the data period in settings |
| [out] | pDeviceDes | update the data rate in the generic sensor structure for this device |
| 0 | is returned when the configuration is valid. |
| 1 | is returned when the configuration is modified. |
Definition at line 896 of file fsl_mma865x_i2c_3D_accel.c.
References DSA_RET_SETTINGS_CHANGED, FALSE, FSL_MMA865x_ACCEL_800HZ, isf_dsa_SensorSettings_st::nSamplePeriod, mma865x_Specific_Settings_t::sampleRateIndex, and TRUE.
Referenced by mma865x_ValidateConfig().

| isf_dsa_status_t mma865x_GetData | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pBuffer | ||
| ) |
Definition at line 818 of file fsl_mma865x_i2c_3D_accel.c.
References BYTES_FOR_FULL_READ, DeviceDescriptor_struct::deviceHandle, dm_device_read(), ISF_SUCCESS, MMA865x_GET_FIELD, MMA865x_STATUS_00, isf_SensorHandle_st::pDeviceDescriptor, pSensorData, and SENSOR_ERROR_GETDATA.
Referenced by fsl_mma865x_i2c_3D_accel_PeriodicCallback().


| void mma865x_Reset | ( | int32_t * | status, |
| void * | pSensorHandle | ||
| ) |
This function resets the MMA865x sensor resulting in a default configuration for all registers.
Definition at line 677 of file fsl_mma865x_i2c_3D_accel.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_write(), DSA_ERR_INITIALIZE, ISF_SUCCESS, MMA865x_ASLP_COUNT, MMA865x_CTRL_REG2, MMA865x_RST_MASK, and isf_SensorHandle_st::pDeviceDescriptor.

| isf_dsa_status_t mma865x_SetConfig | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pConfigSettings | ||
| ) |
This function sets the MMA865x sensor configuration.
Definition at line 850 of file fsl_mma865x_i2c_3D_accel.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_write(), DSA_ERR_CONFIGURE, ISF_SUCCESS, MMA865x_CTRL_REG1, MMA865x_ERROR, MMA865x_SET_FIELD, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, and mma865x_Specific_Settings_t::sampleRateIndex.
Referenced by fsl_mma865x_i2c_3D_accel_Configure().


| void mma865x_SetMode | ( | int32_t * | status, |
| void * | pSensorHandle, | ||
| int32_t | Mode | ||
| ) |
This function sets the MMA865x part to the requested mode.
Definition at line 752 of file fsl_mma865x_i2c_3D_accel.c.
References DeviceDescriptor_struct::deviceHandle, and isf_SensorHandle_st::pDeviceDescriptor.
Referenced by fsl_mma865x_i2c_3D_accel_Configure(), fsl_mma865x_i2c_3D_accel_EndData(), and fsl_mma865x_i2c_3D_accel_StartData().

| void mma865x_ValidateConfig | ( | int32_t * | status, |
| void * | pSensorHandle, | ||
| void * | pSettings | ||
| ) |
This function validates the configuration for the MMA865x sensor.
Definition at line 730 of file fsl_mma865x_i2c_3D_accel.c.
References DSA_RET_SETTINGS_CHANGED, ISF_SUCCESS, mma865x_GetConfig(), and isf_SensorHandle_st::pDeviceDescriptor.
Referenced by fsl_mma865x_i2c_3D_accel_ValidateSettings().


| int32 fixedFactor |
Definition at line 59 of file fsl_mma865x_i2c_3D_accel.c.
| int32 fixedOffset |
Definition at line 60 of file fsl_mma865x_i2c_3D_accel.c.
| float floatFactor |
Definition at line 57 of file fsl_mma865x_i2c_3D_accel.c.
| float floatOffset |
Definition at line 58 of file fsl_mma865x_i2c_3D_accel.c.
| isf_SensorDataTypes_t mma865x_SupportedDataTypes[] |
Definition at line 69 of file fsl_mma865x_i2c_3D_accel.c.
| isf_SensorDataTypes_t mma865x_SupportedDataTypes[] = { TYPE_RAW_ACCELERATION_3D, TYPE_NATIVE_SENSOR_DATA_TYPE } |
Definition at line 69 of file fsl_mma865x_i2c_3D_accel.c.
| isf_SensorTypes_t mma865x_SupportedSensorTypes[] |
Supported sensor and data types for MMA865x.
Definition at line 68 of file fsl_mma865x_i2c_3D_accel.c.
| isf_SensorTypes_t mma865x_SupportedSensorTypes[] = { TYPE_ACCELEROMETER_3D, TYPE_NATIVE_SENSOR_TYPE } |
Supported sensor and data types for MMA865x.
Definition at line 68 of file fsl_mma865x_i2c_3D_accel.c.
| const { ... } mma865xAccelConvTable[] |