![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | BOARD_DEBUG_UART_INSTANCE UART1_IDX |
| #define | BOARD_DEBUG_UART_BASEADDR UART1_BASE |
| #define | BOARD_DEBUG_UART_BAUD 115200 |
| #define | BOARD_USE_UART |
Functions | |
| void | hardware_init (void) |
| void | init_adc_pins (uint32_t instance) |
| ADC method sets registers according routing settings. Call this method code to route desired pins into: ADC0, ADC1 peripherals. More... | |
| void | deinit_adc_pins (uint32_t instance) |
| ADC method sets registers according routing settings. Call this method code to disable routing of desired pins for: ADC0, ADC1 peripherals. More... | |
| void | init_cmp_pins (uint32_t instance) |
| CMP method sets registers according routing settings. Call this method code to route desired pins into: CMP0, CMP1, CMP2 peripherals. More... | |
| void | deinit_cmp_pins (uint32_t instance) |
| CMP method sets registers according routing settings. Call this method code to disable routing of desired pins for: CMP0, CMP1, CMP2 peripherals. More... | |
| void | init_enet_pins (uint32_t instance) |
| ENET method sets registers according routing settings. Call this method code to route desired pins into ENET periphery. More... | |
| void | deinit_enet_pins (uint32_t instance) |
| ENET method sets registers according routing settings. Call this method code to disable routing of desired pins for ENET periphery. More... | |
| void | init_gpio_pins (uint32_t instance) |
| GPIO method sets registers according routing settings. Call this method code to route desired pins into: PTA, PTB, PTC, PTD, PTE peripherals. More... | |
| void | deinit_gpio_pins (uint32_t instance) |
| GPIO method sets registers according routing settings. Call this method code to disable routing of desired pins for: PTA, PTB, PTC, PTD, PTE peripherals. More... | |
| void | init_i2c_pins (uint32_t instance) |
| I2C method sets registers according routing settings. Call this method code to route desired pins into: I2C0, I2C1, I2C2 peripherals. More... | |
| void | deinit_i2c_pins (uint32_t instance) |
| I2C method sets registers according routing settings. Call this method code to disable routing of desired pins for: I2C0, I2C1, I2C2 peripherals. More... | |
| void | init_jtag_pins (uint32_t instance) |
| JTAG method sets registers according routing settings. Call this method code to route desired pins into JTAG periphery. More... | |
| void | deinit_jtag_pins (uint32_t instance) |
| JTAG method sets registers according routing settings. Call this method code to disable routing of desired pins for JTAG periphery. More... | |
| void | init_llwu_pins (uint32_t instance) |
| LLWU method sets registers according routing settings. Call this method code to route desired pins into LLWU periphery. More... | |
| void | deinit_llwu_pins (uint32_t instance) |
| LLWU method sets registers according routing settings. Call this method code to disable routing of desired pins for LLWU periphery. More... | |
| void | init_osc_pins (uint32_t instance) |
| OSC method sets registers according routing settings. Call this method code to route desired pins into OSC periphery. More... | |
| void | deinit_osc_pins (uint32_t instance) |
| OSC method sets registers according routing settings. Call this method code to disable routing of desired pins for OSC periphery. More... | |
| void | init_spi_pins (uint32_t instance) |
| SPI method sets registers according routing settings. Call this method code to route desired pins into: SPI0, SPI1, SPI2 peripherals. More... | |
| void | deinit_spi_pins (uint32_t instance) |
| SPI method sets registers according routing settings. Call this method code to disable routing of desired pins for: SPI0, SPI1, SPI2 peripherals. More... | |
| void | init_tpiu_pins (uint32_t instance) |
| TPIU method sets registers according routing settings. Call this method code to route desired pins into TPIU periphery. More... | |
| void | deinit_tpiu_pins (uint32_t instance) |
| TPIU method sets registers according routing settings. Call this method code to disable routing of desired pins for TPIU periphery. More... | |
| void | init_uart_pins (uint32_t instance) |
| UART method sets registers according routing settings. Call this method code to route desired pins into: UART0, UART1, UART2, UART3, UART4, UART5 peripherals. More... | |
| void | deinit_uart_pins (uint32_t instance) |
| UART method sets registers according routing settings. Call this method code to disable routing of desired pins for: UART0, UART1, UART2, UART3, UART4, UART5 peripherals. More... | |
| void | init_can_pins (uint32_t instance) |
| CAN method sets registers according routing settings. Call this method code to route desired pins into CAN0 periphery. More... | |
| void | deinit_can_pins (uint32_t instance) |
| CAN method sets registers according routing settings. Call this method code to disable routing of desired pins for CAN0 periphery. More... | |
| void | init_cmt_pins (uint32_t instance) |
| CMT method sets registers according routing settings. Call this method code to route desired pins into CMT periphery. More... | |
| void | deinit_cmt_pins (uint32_t instance) |
| CMT method sets registers according routing settings. Call this method code to disable routing of desired pins for CMT periphery. More... | |
| void | init_dac_pins (uint32_t instance) |
| DAC method sets registers according routing settings. Call this method code to route desired pins into DAC0 periphery. More... | |
| void | deinit_dac_pins (uint32_t instance) |
| DAC method sets registers according routing settings. Call this method code to disable routing of desired pins for DAC0 periphery. More... | |
| void | init_dma_pins (uint32_t instance) |
| DMA method sets registers according routing settings. Call this method code to route desired pins into DMA periphery. More... | |
| void | deinit_dma_pins (uint32_t instance) |
| DMA method sets registers according routing settings. Call this method code to disable routing of desired pins for DMA periphery. More... | |
| void | init_ewm_pins (uint32_t instance) |
| EWM method sets registers according routing settings. Call this method code to route desired pins into EWM periphery. More... | |
| void | deinit_ewm_pins (uint32_t instance) |
| EWM method sets registers according routing settings. Call this method code to disable routing of desired pins for EWM periphery. More... | |
| void | init_fb_pins (uint32_t instance) |
| FB method sets registers according routing settings. Call this method code to route desired pins into FB periphery. More... | |
| void | deinit_fb_pins (uint32_t instance) |
| FB method sets registers according routing settings. Call this method code to disable routing of desired pins for FB periphery. More... | |
| void | init_ftm_pins (uint32_t instance) |
| FTM method sets registers according routing settings. Call this method code to route desired pins into: FTM0, FTM1, FTM2, FTM3 peripherals. More... | |
| void | deinit_ftm_pins (uint32_t instance) |
| FTM method sets registers according routing settings. Call this method code to disable routing of desired pins for: FTM0, FTM1, FTM2, FTM3 peripherals. More... | |
| void | init_i2s_pins (uint32_t instance) |
| I2S method sets registers according routing settings. Call this method code to route desired pins into I2S0 periphery. More... | |
| void | deinit_i2s_pins (uint32_t instance) |
| I2S method sets registers according routing settings. Call this method code to disable routing of desired pins for I2S0 periphery. More... | |
| void | init_lptmr_pins (uint32_t instance) |
| LPTMR method sets registers according routing settings. Call this method code to route desired pins into LPTMR0 periphery. More... | |
| void | deinit_lptmr_pins (uint32_t instance) |
| LPTMR method sets registers according routing settings. Call this method code to disable routing of desired pins for LPTMR0 periphery. More... | |
| void | init_pdb_pins (uint32_t instance) |
| PDB method sets registers according routing settings. Call this method code to route desired pins into PDB0 periphery. More... | |
| void | deinit_pdb_pins (uint32_t instance) |
| PDB method sets registers according routing settings. Call this method code to disable routing of desired pins for PDB0 periphery. More... | |
| void | init_rcm_pins (uint32_t instance) |
| RCM method sets registers according routing settings. Call this method code to route desired pins into RCM periphery. More... | |
| void | deinit_rcm_pins (uint32_t instance) |
| RCM method sets registers according routing settings. Call this method code to disable routing of desired pins for RCM periphery. More... | |
| void | init_rtc_pins (uint32_t instance) |
| RTC method sets registers according routing settings. Call this method code to route desired pins into RTC periphery. More... | |
| void | deinit_rtc_pins (uint32_t instance) |
| RTC method sets registers according routing settings. Call this method code to disable routing of desired pins for RTC periphery. More... | |
| void | init_scb_pins (uint32_t instance) |
| SCB method sets registers according routing settings. Call this method code to route desired pins into SystemControl periphery. More... | |
| void | deinit_scb_pins (uint32_t instance) |
| SCB method sets registers according routing settings. Call this method code to disable routing of desired pins for SystemControl periphery. More... | |
| void | init_sdhc_pins (uint32_t instance) |
| SDHC method sets registers according routing settings. Call this method code to route desired pins into SDHC periphery. More... | |
| void | deinit_sdhc_pins (uint32_t instance) |
| SDHC method sets registers according routing settings. Call this method code to disable routing of desired pins for SDHC periphery. More... | |
| void | init_sim_pins (uint32_t instance) |
| SIM method sets registers according routing settings. Call this method code to route desired pins into SIM periphery. More... | |
| void | deinit_sim_pins (uint32_t instance) |
| SIM method sets registers according routing settings. Call this method code to disable routing of desired pins for SIM periphery. More... | |
| void | init_supply_pins (uint32_t instance) |
| SUPPLY method sets registers according routing settings. Call this method code to route desired pins into SUPPLY periphery. More... | |
| void | deinit_supply_pins (uint32_t instance) |
| SUPPLY method sets registers according routing settings. Call this method code to disable routing of desired pins for SUPPLY periphery. More... | |
| void | init_usb_pins (uint32_t instance) |
| USB method sets registers according routing settings. Call this method code to route desired pins into USB0 periphery. More... | |
| void | deinit_usb_pins (uint32_t instance) |
| USB method sets registers according routing settings. Call this method code to disable routing of desired pins for USB0 periphery. More... | |
| void | init_usbdcd_pins (uint32_t instance) |
| USBDCD method sets registers according routing settings. Call this method code to route desired pins into USBDCD periphery. More... | |
| void | deinit_usbdcd_pins (uint32_t instance) |
| USBDCD method sets registers according routing settings. Call this method code to disable routing of desired pins for USBDCD periphery. More... | |
| void | init_vref_pins (uint32_t instance) |
| VREF method sets registers according routing settings. Call this method code to route desired pins into VREF periphery. More... | |
| void | deinit_vref_pins (uint32_t instance) |
| VREF method sets registers according routing settings. Call this method code to disable routing of desired pins for VREF periphery. More... | |
| void deinit_adc_pins | ( | uint32_t | instance | ) |
ADC method sets registers according routing settings. Call this method code to disable routing of desired pins for: ADC0, ADC1 peripherals.
| instance | - ADC instance number 0..1 |
Definition at line 1423 of file pin_init.c.
| void deinit_can_pins | ( | uint32_t | instance | ) |
CAN method sets registers according routing settings. Call this method code to disable routing of desired pins for CAN0 periphery.
| instance | - CAN instance number (0 is expected) |
| void deinit_cmp_pins | ( | uint32_t | instance | ) |
CMP method sets registers according routing settings. Call this method code to disable routing of desired pins for: CMP0, CMP1, CMP2 peripherals.
| instance | - CMP instance number 0..2 |
Definition at line 1456 of file pin_init.c.
| void deinit_cmt_pins | ( | uint32_t | instance | ) |
CMT method sets registers according routing settings. Call this method code to disable routing of desired pins for CMT periphery.
| instance | - CMT instance number (0 is expected) |
| void deinit_dac_pins | ( | uint32_t | instance | ) |
DAC method sets registers according routing settings. Call this method code to disable routing of desired pins for DAC0 periphery.
| instance | - DAC instance number (0 is expected) |
| void deinit_dma_pins | ( | uint32_t | instance | ) |
DMA method sets registers according routing settings. Call this method code to disable routing of desired pins for DMA periphery.
| instance | - DMA instance number (0 is expected) |
| void deinit_enet_pins | ( | uint32_t | instance | ) |
ENET method sets registers according routing settings. Call this method code to disable routing of desired pins for ENET periphery.
| instance | - ENET instance number (0 is expected) |
Definition at line 1484 of file pin_init.c.
| void deinit_ewm_pins | ( | uint32_t | instance | ) |
EWM method sets registers according routing settings. Call this method code to disable routing of desired pins for EWM periphery.
| instance | - EWM instance number (0 is expected) |
| void deinit_fb_pins | ( | uint32_t | instance | ) |
FB method sets registers according routing settings. Call this method code to disable routing of desired pins for FB periphery.
| instance | - FB instance number (0 is expected) |
| void deinit_ftm_pins | ( | uint32_t | instance | ) |
FTM method sets registers according routing settings. Call this method code to disable routing of desired pins for: FTM0, FTM1, FTM2, FTM3 peripherals.
| instance | - FTM instance number 0..3 |
| void deinit_gpio_pins | ( | uint32_t | instance | ) |
GPIO method sets registers according routing settings. Call this method code to disable routing of desired pins for: PTA, PTB, PTC, PTD, PTE peripherals.
| instance | - GPIO instance number 0..4 |
Definition at line 1548 of file pin_init.c.
| void deinit_i2c_pins | ( | uint32_t | instance | ) |
I2C method sets registers according routing settings. Call this method code to disable routing of desired pins for: I2C0, I2C1, I2C2 peripherals.
| instance | - I2C instance number 0..2 |
Definition at line 1595 of file pin_init.c.
| void deinit_i2s_pins | ( | uint32_t | instance | ) |
I2S method sets registers according routing settings. Call this method code to disable routing of desired pins for I2S0 periphery.
| instance | - I2S instance number (0 is expected) |
| void deinit_jtag_pins | ( | uint32_t | instance | ) |
JTAG method sets registers according routing settings. Call this method code to disable routing of desired pins for JTAG periphery.
| instance | - JTAG instance number (0 is expected) |
Definition at line 1630 of file pin_init.c.
| void deinit_llwu_pins | ( | uint32_t | instance | ) |
LLWU method sets registers according routing settings. Call this method code to disable routing of desired pins for LLWU periphery.
| instance | - LLWU instance number (0 is expected) |
Definition at line 1658 of file pin_init.c.
| void deinit_lptmr_pins | ( | uint32_t | instance | ) |
LPTMR method sets registers according routing settings. Call this method code to disable routing of desired pins for LPTMR0 periphery.
| instance | - LPTMR instance number (0 is expected) |
| void deinit_osc_pins | ( | uint32_t | instance | ) |
OSC method sets registers according routing settings. Call this method code to disable routing of desired pins for OSC periphery.
| instance | - OSC instance number (0 is expected) |
Definition at line 1680 of file pin_init.c.
| void deinit_pdb_pins | ( | uint32_t | instance | ) |
PDB method sets registers according routing settings. Call this method code to disable routing of desired pins for PDB0 periphery.
| instance | - PDB instance number (0 is expected) |
| void deinit_rcm_pins | ( | uint32_t | instance | ) |
RCM method sets registers according routing settings. Call this method code to disable routing of desired pins for RCM periphery.
| instance | - RCM instance number (0 is expected) |
| void deinit_rtc_pins | ( | uint32_t | instance | ) |
RTC method sets registers according routing settings. Call this method code to disable routing of desired pins for RTC periphery.
| instance | - RTC instance number (0 is expected) |
| void deinit_scb_pins | ( | uint32_t | instance | ) |
SCB method sets registers according routing settings. Call this method code to disable routing of desired pins for SystemControl periphery.
| instance | - SCB instance number (0 is expected) |
| void deinit_sdhc_pins | ( | uint32_t | instance | ) |
SDHC method sets registers according routing settings. Call this method code to disable routing of desired pins for SDHC periphery.
| instance | - SDHC instance number (0 is expected) |
| void deinit_sim_pins | ( | uint32_t | instance | ) |
SIM method sets registers according routing settings. Call this method code to disable routing of desired pins for SIM periphery.
| instance | - SIM instance number (0 is expected) |
| void deinit_spi_pins | ( | uint32_t | instance | ) |
SPI method sets registers according routing settings. Call this method code to disable routing of desired pins for: SPI0, SPI1, SPI2 peripherals.
| instance | - SPI instance number 0..2 |
Definition at line 1711 of file pin_init.c.
| void deinit_supply_pins | ( | uint32_t | instance | ) |
SUPPLY method sets registers according routing settings. Call this method code to disable routing of desired pins for SUPPLY periphery.
| instance | - SUPPLY instance number (0 is expected) |
| void deinit_tpiu_pins | ( | uint32_t | instance | ) |
TPIU method sets registers according routing settings. Call this method code to disable routing of desired pins for TPIU periphery.
| instance | - TPIU instance number (0 is expected) |
Definition at line 1741 of file pin_init.c.
| void deinit_uart_pins | ( | uint32_t | instance | ) |
UART method sets registers according routing settings. Call this method code to disable routing of desired pins for: UART0, UART1, UART2, UART3, UART4, UART5 peripherals.
| instance | - UART instance number 0..5 |
Definition at line 1776 of file pin_init.c.
| void deinit_usb_pins | ( | uint32_t | instance | ) |
USB method sets registers according routing settings. Call this method code to disable routing of desired pins for USB0 periphery.
| instance | - USB instance number (0 is expected) |
| void deinit_usbdcd_pins | ( | uint32_t | instance | ) |
USBDCD method sets registers according routing settings. Call this method code to disable routing of desired pins for USBDCD periphery.
| instance | - USBDCD instance number (0 is expected) |
| void deinit_vref_pins | ( | uint32_t | instance | ) |
VREF method sets registers according routing settings. Call this method code to disable routing of desired pins for VREF periphery.
| instance | - VREF instance number (0 is expected) |
| void hardware_init | ( | void | ) |
Definition at line 1397 of file hardware_init.c.
References init_adc_pins(), init_cmp_pins(), init_enet_pins(), init_gpio_pins(), init_i2c_pins(), init_jtag_pins(), init_llwu_pins(), init_osc_pins(), init_spi_pins(), init_tpiu_pins(), and init_uart_pins().

| void init_adc_pins | ( | uint32_t | instance | ) |
ADC method sets registers according routing settings. Call this method code to route desired pins into: ADC0, ADC1 peripherals.
| instance | - ADC instance number 0..1 |
Definition at line 1406 of file pin_init.c.
Referenced by hardware_init().

| void init_can_pins | ( | uint32_t | instance | ) |
CAN method sets registers according routing settings. Call this method code to route desired pins into CAN0 periphery.
| instance | - CAN instance number (0 is expected) |
| void init_cmp_pins | ( | uint32_t | instance | ) |
CMP method sets registers according routing settings. Call this method code to route desired pins into: CMP0, CMP1, CMP2 peripherals.
| instance | - CMP instance number 0..2 |
Definition at line 1439 of file pin_init.c.
Referenced by hardware_init().

| void init_cmt_pins | ( | uint32_t | instance | ) |
CMT method sets registers according routing settings. Call this method code to route desired pins into CMT periphery.
| instance | - CMT instance number (0 is expected) |
| void init_dac_pins | ( | uint32_t | instance | ) |
DAC method sets registers according routing settings. Call this method code to route desired pins into DAC0 periphery.
| instance | - DAC instance number (0 is expected) |
| void init_dma_pins | ( | uint32_t | instance | ) |
DMA method sets registers according routing settings. Call this method code to route desired pins into DMA periphery.
| instance | - DMA instance number (0 is expected) |
| void init_enet_pins | ( | uint32_t | instance | ) |
ENET method sets registers according routing settings. Call this method code to route desired pins into ENET periphery.
| instance | - ENET instance number (0 is expected) |
Definition at line 1473 of file pin_init.c.
Referenced by hardware_init().

| void init_ewm_pins | ( | uint32_t | instance | ) |
EWM method sets registers according routing settings. Call this method code to route desired pins into EWM periphery.
| instance | - EWM instance number (0 is expected) |
| void init_fb_pins | ( | uint32_t | instance | ) |
FB method sets registers according routing settings. Call this method code to route desired pins into FB periphery.
| instance | - FB instance number (0 is expected) |
| void init_ftm_pins | ( | uint32_t | instance | ) |
FTM method sets registers according routing settings. Call this method code to route desired pins into: FTM0, FTM1, FTM2, FTM3 peripherals.
| instance | - FTM instance number 0..3 |
| void init_gpio_pins | ( | uint32_t | instance | ) |
GPIO method sets registers according routing settings. Call this method code to route desired pins into: PTA, PTB, PTC, PTD, PTE peripherals.
| instance | - GPIO instance number 0..4 |
Definition at line 1494 of file pin_init.c.
Referenced by hardware_init().

| void init_i2c_pins | ( | uint32_t | instance | ) |
I2C method sets registers according routing settings. Call this method code to route desired pins into: I2C0, I2C1, I2C2 peripherals.
| instance | - I2C instance number 0..2 |
Definition at line 1574 of file pin_init.c.
Referenced by hardware_init().

| void init_i2s_pins | ( | uint32_t | instance | ) |
I2S method sets registers according routing settings. Call this method code to route desired pins into I2S0 periphery.
| instance | - I2S instance number (0 is expected) |
| void init_jtag_pins | ( | uint32_t | instance | ) |
JTAG method sets registers according routing settings. Call this method code to route desired pins into JTAG periphery.
| instance | - JTAG instance number (0 is expected) |
Definition at line 1613 of file pin_init.c.
Referenced by hardware_init().

| void init_llwu_pins | ( | uint32_t | instance | ) |
LLWU method sets registers according routing settings. Call this method code to route desired pins into LLWU periphery.
| instance | - LLWU instance number (0 is expected) |
Definition at line 1644 of file pin_init.c.
Referenced by hardware_init().

| void init_lptmr_pins | ( | uint32_t | instance | ) |
LPTMR method sets registers according routing settings. Call this method code to route desired pins into LPTMR0 periphery.
| instance | - LPTMR instance number (0 is expected) |
| void init_osc_pins | ( | uint32_t | instance | ) |
OSC method sets registers according routing settings. Call this method code to route desired pins into OSC periphery.
| instance | - OSC instance number (0 is expected) |
Definition at line 1669 of file pin_init.c.
Referenced by hardware_init().

| void init_pdb_pins | ( | uint32_t | instance | ) |
PDB method sets registers according routing settings. Call this method code to route desired pins into PDB0 periphery.
| instance | - PDB instance number (0 is expected) |
| void init_rcm_pins | ( | uint32_t | instance | ) |
RCM method sets registers according routing settings. Call this method code to route desired pins into RCM periphery.
| instance | - RCM instance number (0 is expected) |
| void init_rtc_pins | ( | uint32_t | instance | ) |
RTC method sets registers according routing settings. Call this method code to route desired pins into RTC periphery.
| instance | - RTC instance number (0 is expected) |
| void init_scb_pins | ( | uint32_t | instance | ) |
SCB method sets registers according routing settings. Call this method code to route desired pins into SystemControl periphery.
| instance | - SCB instance number (0 is expected) |
| void init_sdhc_pins | ( | uint32_t | instance | ) |
SDHC method sets registers according routing settings. Call this method code to route desired pins into SDHC periphery.
| instance | - SDHC instance number (0 is expected) |
| void init_sim_pins | ( | uint32_t | instance | ) |
SIM method sets registers according routing settings. Call this method code to route desired pins into SIM periphery.
| instance | - SIM instance number (0 is expected) |
| void init_spi_pins | ( | uint32_t | instance | ) |
SPI method sets registers according routing settings. Call this method code to route desired pins into: SPI0, SPI1, SPI2 peripherals.
| instance | - SPI instance number 0..2 |
Definition at line 1690 of file pin_init.c.
Referenced by hardware_init().

| void init_supply_pins | ( | uint32_t | instance | ) |
SUPPLY method sets registers according routing settings. Call this method code to route desired pins into SUPPLY periphery.
| instance | - SUPPLY instance number (0 is expected) |
| void init_tpiu_pins | ( | uint32_t | instance | ) |
TPIU method sets registers according routing settings. Call this method code to route desired pins into TPIU periphery.
| instance | - TPIU instance number (0 is expected) |
Definition at line 1730 of file pin_init.c.
Referenced by hardware_init().

| void init_uart_pins | ( | uint32_t | instance | ) |
UART method sets registers according routing settings. Call this method code to route desired pins into: UART0, UART1, UART2, UART3, UART4, UART5 peripherals.
| instance | - UART instance number 0..5 |
Definition at line 1751 of file pin_init.c.
Referenced by hardware_init().

| void init_usb_pins | ( | uint32_t | instance | ) |
USB method sets registers according routing settings. Call this method code to route desired pins into USB0 periphery.
| instance | - USB instance number (0 is expected) |
| void init_usbdcd_pins | ( | uint32_t | instance | ) |
USBDCD method sets registers according routing settings. Call this method code to route desired pins into USBDCD periphery.
| instance | - USBDCD instance number (0 is expected) |
| void init_vref_pins | ( | uint32_t | instance | ) |
VREF method sets registers according routing settings. Call this method code to route desired pins into VREF periphery.
| instance | - VREF instance number (0 is expected) |