![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Main ISF header file. Contains code common to all ISF components. More...

Go to the source code of this file.
Data Structures | |
| struct | version_info_t |
| This structure holds the version information of device/lib/component /user application etc. More... | |
| struct | build_info_t |
| This structure holds the build information of device/lib/component /user application etc. More... | |
| struct | isf_info_t |
| struct | device_info_t |
| This structure holds the ROM device information such as device id and number of EmbApps present. This information is returned by the _fw_device_info_get() API. More... | |
Macros | |
| #define | MAX_ISF_APPLICATIONS (32) |
| Maximum number of applications. More... | |
| #define | APP_ID_NULL (0) |
| Null application ID. More... | |
| #define | MAX_ISF_COMMIT_ID_SIZE (8) |
| The maximum size of the ISF commit_id. More... | |
| #define | ISF_EMB_APPS_PRESENT 5 |
| The number of separate addressable apps in the build. More... | |
| #define | USER_APP_ID_START (ISF_APP_ID_LAST) |
| #define | ISF_TASK_INDEX_START (50) |
| ISF starting task index. More... | |
Typedefs | |
| typedef int32 | isf_status_t |
| ISF return status type. More... | |
| typedef uint32 | isf_duration_t |
| ISF time duration in microseconds. More... | |
Enumerations | |
| enum | isf_status_enum { ISF_SUCCESS = 0, ISF_ERR_LIB_INIT = 1 } |
| ISF library return status type. More... | |
| enum | isf_app_type_enum { ISF_INVALID_APP = 0, ISF_MAILBOX_APP = 1, ISF_RLI_APP = 2, ISF_BASIC_APP = 3, ISF_EMB_APP = 4, ISF_APP_TYPE_DATALOGGER = 5, ISF_APP_TYPE_SENSOR_FUSION = 6, ISF_APP_TYPE_USER1 = 7, ISF_APP_TYPE_MAX = 128 } |
| ISF Embedded Application types. More... | |
| enum | isf_app_id_enum { ISF_APP_ID_DEV_INFO = 0, ISF_APP_ID_MBOX = 1, ISF_APP_ID_LAST } |
| ISF application number. More... | |
Functions | |
| isf_info_t | isf_get_info (void) |
| API to get ISF information. More... | |
| isf_status_t | isf_lib_init (void *pNull) |
| API to get ISF information. More... | |
| void | _fw_device_info_get (device_info_t *info_ptr) |
| uint32 | isf_time_util_get_usec (void) |
| This API returns the time in microseconds. More... | |
Main ISF header file. Contains code common to all ISF components.
Definition in file isf.h.
| #define APP_ID_NULL (0) |
Null application ID.
Value for null application ID.
Definition at line 103 of file isf.h.
Referenced by ci_qr_update(), and ci_update_first_data_mb().
| #define ISF_EMB_APPS_PRESENT 5 |
The number of separate addressable apps in the build.
The number of addressable apps includes, when applicable, the Mailbox App, instances of BasicApp, EmbApp, and RLI Apps. This number is reported in the DeviceInfo Command response. Apps are numbered from 1. I.e., if three apps are present they will be numbered 1, 2, and 3. App 1 is almost always the mailbox app.
Definition at line 122 of file isf.h.
Referenced by _fw_device_info_get().
| #define ISF_TASK_INDEX_START (50) |
| #define MAX_ISF_APPLICATIONS (32) |
Maximum number of applications.
The maximum number of applications that can exists. Note
that the application id can be anywhere between APP_ID_NULL and
NO_APP_FBID_INDX, but the maximum number of those applications
is limited to the value set here.
Definition at line 95 of file isf.h.
Referenced by ci_mbox_init().
| #define MAX_ISF_COMMIT_ID_SIZE (8) |
The maximum size of the ISF commit_id.
The maximum size of the ISF commit_id from which build is made.
Definition at line 111 of file isf.h.
Referenced by isf_get_info().
| #define USER_APP_ID_START (ISF_APP_ID_LAST) |
| enum isf_app_id_enum |
| enum isf_app_type_enum |
ISF Embedded Application types.
| enum isf_status_enum |
| void _fw_device_info_get | ( | device_info_t * | info_ptr | ) |
Definition at line 77 of file isf.c.
References device_info_t::emb_apps_present, ISF_EMB_APPS_PRESENT, isf_get_info(), device_info_t::isf_info, and device_info_t::system_device_id.
Referenced by ci_mbox_init(), and isf_app_callback_dev_info().


| isf_info_t isf_get_info | ( | void | ) |
API to get ISF information.
The isf_get_info() function is called by an application that needs
retrieve ISF version and part number that the library is targeted for.
Definition at line 29 of file isf.c.
References isf_info_t::build_info, build_info_t::buildDay, build_info_t::buildHours, build_info_t::buildId, build_info_t::buildMinutes, build_info_t::buildMonth, build_info_t::buildSeconds, build_info_t::buildYear, ISF_BUILD_DAY, ISF_BUILD_HOURS, ISF_BUILD_MINUTES, ISF_BUILD_MONTH, ISF_BUILD_SECONDS, ISF_BUILD_YEAR, isf_commit_id, ISF_LIB_VERSION_MAJOR, ISF_LIB_VERSION_MINOR, version_info_t::majorVersion, MAX_ISF_COMMIT_ID_SIZE, version_info_t::minorVersion, and isf_info_t::version_info.
Referenced by _fw_device_info_get().

| isf_status_t isf_lib_init | ( | void * | pOptions | ) |
API to get ISF information.
The isf_get_info() function is called by an application that needs
retrieve library version and part number that the library is targeted for.
API to get ISF information.
Definition at line 18 of file isf_init.c.
Referenced by App1_task(), and BasicApp1_MainTask().

| uint32 isf_time_util_get_usec | ( | void | ) |
This API returns the time in microseconds.
This API call uses the RTOS services to calculate and return the elapsed time since the system started running. Note that if the elapsed time has exceeded a 32bit value, that is 2^32-1 or 4294.96 seconds, then the time elapsed will rollover and start at zero.
Definition at line 55 of file isf_util.c.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_PeriodicCallback(), and isr_bm_callback_tmr().