![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
API definitions, types, and macros for the Intelligent Sensing Framework (ISF) Command Interpreter (CI). More...
#include "isf_types.h"

Go to the source code of this file.
Data Structures | |
| struct | ci_host_cmd_packet_t |
| This structure contains host command information. More... | |
| struct | ci_app_resp_packet_t |
| This structure enables an application to read from or write to the host. More... | |
Macros | |
| #define | CI_CMD_LAST CI_CMD_MAX |
| The maximum enumeration value implemented as a valid CI command. More... | |
| #define | CI_MAX_FLASH_BYTES 24 |
Typedefs | |
| typedef ci_status_enum | ci_status_t |
| Type definition for the CI status values. More... | |
| typedef ci_response_enum | ci_response_t |
| Type definition for the CI response values. More... | |
| typedef ci_response_t(* | ci_funcp_t) (ci_host_cmd_packet_t *, ci_app_resp_packet_t *) |
| This is a CI callback function pointer. More... | |
Enumerations | |
| enum | ci_status_enum { ISF_CI_FAILURE = 1, ISF_CI_FAILURE_INVALID_PARAMETERS = 2 } |
| ISF CI return status type. More... | |
| enum | ci_rw_enum { CI_RW_NULL = 0, CI_RW_READ, CI_RW_WRITE } |
| CI read or write operation. More... | |
| enum | ci_commands_enum { CI_CMD_READ_VERSION = 0, CI_CMD_READ_CONFIG, CI_CMD_WRITE_CONFIG, CI_CMD_READ_APP_DATA, CI_CMD_UPDATE_QUICKREAD, CI_CMD_READ_APP_STATUS, CI_CMD_RESET_APP, CI_CMD_DEVICE_WRITE, CI_CMD_DEVICE_READ, CI_CMD_GET_APP_SUBSCRIPTION, CI_CMD_WRITE_SREC_FLASH, CI_CMD_MAX = 128 } |
| CI host command instructions. More... | |
| enum | ci_response_enum { CI_ERROR_NONE = 0, CI_ERROR_PARAM = 0x04, CI_INVALID_COUNT = 0x19, CI_ERROR_COMMAND = 0x1c, CI_ERROR_INVALID_LENGTH = 0x21, CI_ERROR_FIFO_BUSY = 0x22, CI_ERROR_FIFO_ALLOCATED = 0x23, CI_ERROR_FIFO_OVERSIZE = 0x24, CI_ERROR_CB_NOT_REGISTERED = 0x25, CI_RESP_QUICKREAD = 0x40, CI_ERROR_MAX = 0x80 } |
| These are the CI errors provided to the host. More... | |
Functions | |
| ci_response_t | isf_app_callback_mbox (ci_host_cmd_packet_t *apHostPacket, ci_app_resp_packet_t *apAppPacket) |
| This function is the mailbox application callback. More... | |
| ci_response_t | isf_app_callback_dev_info (ci_host_cmd_packet_t *apHostPacket, ci_app_resp_packet_t *apAppPacket) |
| Callback function for the device info command, ISF_APP_ID_DEV_INFO. More... | |
| uint32 | isf_ci_app_write (uint8 aAppId, uint32 anumBytes, uint8 *apSrc) |
| This API writes data to the host via the mailboxes. More... | |
| uint32 | isf_ci_app_read (uint8 aAppId, uint32 anumBytes, uint8 *apDst) |
| This API reads data from the host via the mailboxes. More... | |
| ci_status_t | isf_ci_qr_update (uint8 aAppId, int8 anumBytes, uint8 *apSrc) |
| This API updates the Quick-Read mailboxes. More... | |
| isf_status_t | ci_init (void) |
| This API initializes the Command Interpreter. More... | |
API definitions, types, and macros for the Intelligent Sensing Framework (ISF) Command Interpreter (CI).
Copyright (c) 2015, Freescale Semiconductor, Inc.
Definition in file isf_ci.h.
| #define CI_CMD_LAST CI_CMD_MAX |
The maximum enumeration value implemented as a valid CI command.
Definition at line 179 of file isf_ci.h.
Referenced by ci_protocol_CB_mbox().
| #define CI_MAX_FLASH_BYTES 24 |
Definition at line 180 of file isf_ci.h.
Referenced by App1_ci_app_callback(), and BasicApp1_CI_Callback().
| typedef ci_response_t(* ci_funcp_t) (ci_host_cmd_packet_t *, ci_app_resp_packet_t *) |
| typedef ci_response_enum ci_response_t |
| typedef ci_status_enum ci_status_t |
| enum ci_commands_enum |
CI host command instructions.
The host indicates which command the Command Interpreter runs. ci_commands_enum is used to identify this command. The maximum number of possible commands is 128 represented by 7 bits.
| enum ci_response_enum |
These are the CI errors provided to the host.
Any errors identified by the Command Interpreter are returned to the host. Any of these errors may be passed back to the host from the application. There are 7 bits allocated to contain error status resulting in 128 possible different status values.
| enum ci_rw_enum |
| enum ci_status_enum |
| isf_status_t ci_init | ( | void | ) |
This API initializes the Command Interpreter.
The Command Interpreter requires a one time initialization at system startup performed by this API call. It creates and initializes internal variables. In addition, it installs an interrupt service routine for the slave-port interrupt.
| ISF_SUCCESS | The initialization completed successfully. |
| ISF_ERR_LIB_INIT | The interrupt service routine for the uart channel used by the Command Interpereter could not installed. |
| ci_response_t isf_app_callback_dev_info | ( | ci_host_cmd_packet_t * | apHostPacket, |
| ci_app_resp_packet_t * | apAppPacket | ||
| ) |
Callback function for the device info command, ISF_APP_ID_DEV_INFO.
| apHostPacket | - host command packet |
| apAppPacket | - application response packet. |
| packet_ptr | - host command packet |
| mb_data_ptr | - pointer to first mailbox address containing data. |
Definition at line 768 of file ci_protocol_mbox.c.
References _fw_device_info_get(), ci_host_cmd_packet_t::appId, ci_app_resp_packet_t::bytes_left, ci_app_resp_packet_t::bytes_xfer, CI_ERROR_NONE, CI_RW_WRITE, isf_ci_app_write(), and ci_app_resp_packet_t::rw.

| ci_response_t isf_app_callback_mbox | ( | ci_host_cmd_packet_t * | apHostPacket, |
| ci_app_resp_packet_t * | apAppPacket | ||
| ) |
This function is the mailbox application callback.
This mailbox function is referred to as the mailbox application. This callback function is invoked when the host sends commands to the mailbox application via the mailboxes. This is the mechanism whereby the host reads or writes to the mailbox configuration data to configure the mailboxes for Quick-Read or the interrupt output (INT_O) behavior.
| [in] | apHostPacket | Host command packet pointer that points to a data structure of type ci_host_cmd_packet_t. The data structure contains the host command and parameters for the mailbox application to process. |
| [in,out] | apAppPacket | An application response packet pointer that points to a data structure of type ci_app_resp_packet_t. The mailbox application fills this data structure with data as a result of handling the host command. |
| CI_ERROR_NONE | The host command completed successfully. |
| CI_ERROR_COMMAND | The host command in apHostPacket->cmd is not recognized. |
| CI_INVALID_COUNT | The byte count in apHostPacket->byte_cnt is invalid because it is zero or it exceeds the mailbox configuration data size. |
| CI_ERROR_INVALID_LENGTH | The byte count apHostPacket->byte combined with apHostPacket->offset exceeds the mailbox configuration data size. |
This function is the mailbox application callback.
| packet_ptr | - host command packet |
| mb_data_ptr | - pointer to first mailbox address containing data. |
Definition at line 620 of file ci_protocol_mbox.c.
References ci_host_cmd_packet_t::appId, ci_host_cmd_packet_t::byte_cnt, ci_app_resp_packet_t::bytes_left, ci_app_resp_packet_t::bytes_xfer, CI_CMD_READ_APP_DATA, CI_CMD_READ_CONFIG, CI_CMD_READ_VERSION, CI_CMD_RESET_APP, CI_CMD_UPDATE_QUICKREAD, CI_CMD_WRITE_CONFIG, CI_ERROR_COMMAND, CI_ERROR_INVALID_LENGTH, CI_ERROR_NONE, CI_INVALID_COUNT, ci_qr_update(), CI_RW_NULL, CI_RW_READ, CI_RW_WRITE, ci_update_first_data_mb(), ci_regs_t::ciCtrlReg, ci_host_cmd_packet_t::cmd, isf_ci_app_read(), isf_ci_app_write(), ci_host_cmd_packet_t::offset, ci_regs_t::qr_config, qr_config_clear, ci_ctrl_reg_t::reg, and ci_app_resp_packet_t::rw.

This API reads data from the host via the mailboxes.
This API function is called by an application that reads data from the host in response to a host command.
| [in] | aAppId | ID of the application reading data from the host. |
| [in] | anumBytes | The number of bytes to read from the mailboxes. The range is 1 to 28. |
| [in] | apDst | Pointer to the destination where the data is to be stored. |
Definition at line 226 of file ci_protocol_mbox.c.
References ISF_SUCCESS.
Referenced by App1_ci_app_callback(), BasicApp1_CI_Callback(), isf_app_callback_mbox(), and rli_ci_app_callback().

This API writes data to the host via the mailboxes.
This API function is called by an application that sends data to the host in response to a host command. Data is sent to the host via the mailboxes.
| [in] | aAppId | ID of application writing data to the host. |
| [in] | anumBytes | The number of bytes to write to the mailboxes. The range is 1 to 28. |
| [in] | apSrc | Pointer to the source of the data to write to the host. |
Definition at line 277 of file ci_protocol_mbox.c.
References ISF_SUCCESS, and MAX_NUM_OUT_BUFFER.
Referenced by App1_ci_app_callback(), BasicApp1_CI_Callback(), ci_mbox_init(), isf_app_callback_dev_info(), isf_app_callback_mbox(), and rli_ci_app_callback().

| ci_status_t isf_ci_qr_update | ( | uint8 | aAppId, |
| int8 | anumBytes, | ||
| uint8 * | apSrc | ||
| ) |
This API updates the Quick-Read mailboxes.
This API function is called by an application to write data to the host via the mailboxes designated as Quick-Read for that application. The host must configure the mailboxes for Quick-Read by configuring the mailbox application. The host reads these Quick-Read mailboxes directly without sending a command to the CI.
| [in] | aAppId | ID of the application writing data to the mailboxes for the host. |
| [in] | anumBytes | The number of bytes to write to the mailboxes. The range is 1 to 28. |
| [in] | apSrc | Pointer to the source of the data to write to the mailboxes designated as Quick-Read for the application specified in appId. |
| ISF_SUCCESS | The Quick-Read update completed successfully. |
| ISF_CI_FAILURE | A timeout error occurred while waiting for the mailboxes to be free for updates. |
Definition at line 100 of file ci_protocol_mbox.c.
References qr_config_t::appId, ci_ctrl_reg_t::Bits, ci_ctrl_reg_t::blockTransferMode, qr_config_t::byte_id, ccitt_crc16_cal(), ci_insert_crc, CI_PROTOCOL_DATA_OFFSET, CI_PROTOCOL_ID_SIZE, CI_RESP_QUICKREAD, ci_send_packet(), CI_STREAMING_MODE, ci_regs_t::ciCtrlReg, FIRST_QR_MAILBOX_NUM, ISF_CI_FAILURE, ISF_SUCCESS, MAX_NUM_MAILBOXES, MB_APP_RESP_SIZE, MB_RESP_INDEX_APP_ID, MB_RESP_INDEX_BYTES_XFER, MB_RESP_INDEX_COUNT, MB_RESP_INDEX_STATUS_CC, MBOX_CRC_BYTE_SIZE, NUM_QR_MAILBOXES, and ci_regs_t::qr_config.
Referenced by App1_ci_app_callback(), and App1_MainTask().