![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|

Go to the source code of this file.
Functions | |
| void | isf_EventHandler_Init (void) |
| int32 | isf_EventHandler_RegisterEvent (eventCallback_t *pCallback, void *pUserData) |
| int32 | isf_EventHandler_UnregisterEvent (uint32 token) |
| int32 | isf_EventHandler_GetSignal (uint32 token) |
| void | EventHandler_task (void) |
Variables | |
| event_t * | pEventHandler_Events |
| semaphore_t | sema_ev_access |
Definition in file isf_eventhandler.c.