![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "fsl_os_abstraction.h"

Go to the source code of this file.
Data Structures | |
| struct | isf_eh_event_t |
Macros | |
| #define | MAX_EVENTS 32 |
| #define | ALL_EVENTS 0x00FFFFFF |
Typedefs | |
| typedef void( | eventCallback_t) (void *) |
Functions | |
| void | isf_EventHandler_Init (void) |
| int32 | isf_EventHandler_RegisterEvent (eventCallback_t *pCallback, void *pUserData) |
| int32 | isf_EventHandler_UnregisterEvent (uint32 token) |
| int32 | isf_EventHandler_GetSignal (uint32 token) |
| void | EventHandler_task (void) |
Definition in file isf_eventhandler.h.