![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The isf_init.c file contains implementation of the ISF library initialization functions. More...

Go to the source code of this file.
Functions | |
| isf_status_t | isf_lib_init (void *pOptions) |
| Please see isf_init.h for complete documentation. More... | |
| void | isf_system_sync (void) |
| This function synchronizes the user tasks and the system initialization. More... | |
Variables | |
| event_t | isfSysEventHandler |
| volatile uint8 | synchCreate = 0 |
The isf_init.c file contains implementation of the ISF library initialization functions.
Definition in file isf_init.c.
| isf_status_t isf_lib_init | ( | void * | pOptions | ) |
Please see isf_init.h for complete documentation.
This function initializes the ISF library.
API to get ISF information.
Definition at line 18 of file isf_init.c.
References bm_init(), ci_init(), ISF_ERR_LIB_INIT, ISF_SUCCESS, ISF_SYSTEM_READY_EVENT, and isfSysEventHandler.
Referenced by App1_task(), and BasicApp1_MainTask().


| void isf_system_sync | ( | void | ) |
This function synchronizes the user tasks and the system initialization.
Definition at line 50 of file isf_init.c.
References FALSE, ISF_SYSTEM_READY_EVENT, isfSysEventHandler, and synchCreate.
Referenced by App1_task(), BasicApp1_MainTask(), BM_task(), CI_task(), and RLI1_MainTask().

| event_t isfSysEventHandler |
Definition at line 13 of file isf_init.c.
Referenced by isf_lib_init(), and isf_system_sync().
| volatile uint8 synchCreate = 0 |
Definition at line 16 of file isf_init.c.
Referenced by isf_system_sync().