![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The isf_sensor_base_types.h file contains declarations for the general base types used in the isf sensor type-specific header files. More...
#include <isf_types.h>

Go to the source code of this file.
Typedefs | |
| typedef uint32 | isf_timestamp_t |
| Standard timestamp. More... | |
The isf_sensor_base_types.h file contains declarations for the general base types used in the isf sensor type-specific header files.
Definition in file isf_sensor_base_types.h.
| typedef uint32 isf_timestamp_t |
Standard timestamp.
Definition at line 15 of file isf_sensor_base_types.h.