![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The isf_sensor_configuration_extern.h contains external declarations referenced by the Sensor Manager for the Digital Sensor Abstration (DSA) implementation. More...
#include "isf_dsa_adapter.h"

Go to the source code of this file.
Variables | |
| isf_SensorConfig_t | gSensorList [] |
| This is the external declaration of the DSA sensor list array containing the sensor adapters and sensor hardware mapping information. More... | |
| isf_SensorHandle_t * | gSensorHandleList [] |
| This is the external declaration of the DSA sensor handle list array containing the sensor adapters and device specific information. More... | |
| uint8 | gNumSupportedSensors |
| This is the external declaration of the current number of supported sensors. This is used by the Sensor Manager component. More... | |
The isf_sensor_configuration_extern.h contains external declarations referenced by the Sensor Manager for the Digital Sensor Abstration (DSA) implementation.
Definition in file isf_sensor_configuration_extern.h.
| uint8 gNumSupportedSensors |
This is the external declaration of the current number of supported sensors. This is used by the Sensor Manager component.
Note: This declaration must not be changed by the user.
This is the external declaration of the current number of supported sensors. This is used by the Sensor Manager component.
This is the external declaration of the current number of available sensors.
Definition at line 64 of file isf_sensor_configuration.c.
| isf_SensorHandle_t* gSensorHandleList[] |
This is the external declaration of the DSA sensor handle list array containing the sensor adapters and device specific information.
This is the external declaration of the DSA sensor handle list array containing the sensor adapters and device specific information.
Definition at line 69 of file isf_sensor_configuration.c.
Referenced by App1_MainTask().
| isf_SensorConfig_t gSensorList[] |
This is the external declaration of the DSA sensor list array containing the sensor adapters and sensor hardware mapping information.
Note: This declaration must not be changed by the user.
This is the external declaration of the DSA sensor list array containing the sensor adapters and sensor hardware mapping information.
Definition at line 37 of file isf_sensor_configuration.c.