![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
isf_spi_master_types.h defines the spi protocol adapter structure and types. More...
#include "isf_types.h"#include "isf.h"#include "fsl_dspi_hal.h"#include "fsl_dspi_master_driver.h"

Go to the source code of this file.
Data Structures | |
| struct | spi_master_BusConfig_struct |
| struct | spi_mater_BusHandle_struct |
| This structure defines the data bus handle. More... | |
| struct | spi_mater_SlaveCmd |
| This structure defines the spi slave command format. More... | |
| struct | spi_mater_slaveInfo |
| This structure defines the slave specific spi information. More... | |
| struct | spi_master_CommSpecificInfo_t |
Typedefs | |
| typedef struct spi_master_BusConfig_struct | spi_master_busConfig_t |
| typedef struct spi_mater_BusHandle_struct | spi_master_busHandle_t |
| This structure defines the data bus handle. More... | |
| typedef struct spi_mater_SlaveCmd | spi_mater_slaveCmd_t |
| This structure defines the spi slave command format. More... | |
| typedef isf_status_t(* | fnslaveinit_t) (void) |
| typedef isf_status_t(* | fnwritepreProcessing_t) (void *cmdOut, uint32 offset, uint32 size, void *writebuffer) |
| typedef isf_status_t(* | fnwritepostProcossing_t) (void *cmd) |
| typedef isf_status_t(* | fnreadpreProcessing_t) (void *cmdout, uint32 offset, uint32 size) |
| typedef isf_status_t(* | fnreadpostProcossing_t) (void *cmd, void *dataOut) |
| typedef struct spi_mater_slaveInfo | spi_master_slaveInfo_t |
| This structure defines the slave specific spi information. More... | |
isf_spi_master_types.h defines the spi protocol adapter structure and types.
File: isf_spi_master_types.h
Copyright (c) 2015, Freescale Semiconductor, Inc.
Definition in file isf_spi_master_types.h.
| typedef isf_status_t(* fnreadpostProcossing_t) (void *cmd, void *dataOut) |
Definition at line 48 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnreadpreProcessing_t) (void *cmdout, uint32 offset, uint32 size) |
Definition at line 47 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnslaveinit_t) (void) |
Definition at line 44 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnwritepostProcossing_t) (void *cmd) |
Definition at line 46 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnwritepreProcessing_t) (void *cmdOut, uint32 offset, uint32 size, void *writebuffer) |
Definition at line 45 of file isf_spi_master_types.h.
| typedef struct spi_master_BusConfig_struct spi_master_busConfig_t |
| typedef struct spi_mater_BusHandle_struct spi_master_busHandle_t |
This structure defines the data bus handle.
| typedef struct spi_mater_slaveInfo spi_master_slaveInfo_t |
This structure defines the slave specific spi information.
| typedef struct spi_mater_SlaveCmd spi_mater_slaveCmd_t |
This structure defines the spi slave command format.