![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
System Communications channel configuration. More...
#include <isf_sysconf_types.h>#include <isf_sysconf_comms.h>#include "isf.h"#include "Events.h"#include "isf_i2c_master_types.h"#include "isf_uart_types.h"#include "isf_spi_master_types.h"
Go to the source code of this file.
Enumerations | |
| enum | { I2C_BUS_0 = 0, I2C_NUM_BUS } |
| enum | { UART_BUS_0 = 0, UART_NUM_BUS } |
| enum | { SPI_BUS_0 = 0, SPI_NUM_BUS } |
Functions | |
| uint32 | get_ci_comm (void) |
Variables | |
| const i2c_Master_BusConfig_t | gSys_I2cBusConfig [] |
| const uint8 | gSys_NumI2cBuses = I2C_INSTANCE_COUNT |
| i2c_Master_busHandle_t | i2c_master_busHandle [I2C_INSTANCE_COUNT] |
| mutex_t | i2c_Master_mutexHandler [I2C_INSTANCE_COUNT] |
| const uint8 | gSys_NumUartBuses = UART_INSTANCE_COUNT |
| uart_busHandle_t | uart_busHandle [UART_INSTANCE_COUNT] |
| mutex_t | uart_lock [UART_INSTANCE_COUNT] |
| mutex_t | uart_rdlock [UART_INSTANCE_COUNT] |
| const uint8 | gSys_NumSpiBuses = SPI_INSTANCE_COUNT |
| spi_master_busHandle_t | spi_busHandle [SPI_INSTANCE_COUNT] |
| mutex_t | spi_lock [SPI_INSTANCE_COUNT] |
| mutex_t | spi_rdlock [SPI_INSTANCE_COUNT] |
| const sys_channelDescriptor_t | gSys_ConfiguredChannelList [] |
| This data structure/variable holds the complete state of the rli magnetometer sensor embedded application. More... | |
| const uint8 | gSys_NumChannels = sizeof(gSys_ConfiguredChannelList)/sizeof(sys_channelDescriptor_t) |
System Communications channel configuration.
Copyright (c) 2015, Freescale, Inc.
Definition in file isf_sysconf_comms.c.
| anonymous enum |
| Enumerator | |
|---|---|
| I2C_BUS_0 | |
| I2C_NUM_BUS | |
Definition at line 18 of file isf_sysconf_comms.c.
| anonymous enum |
| Enumerator | |
|---|---|
| UART_BUS_0 | |
| UART_NUM_BUS | |
Definition at line 39 of file isf_sysconf_comms.c.
| anonymous enum |
| Enumerator | |
|---|---|
| SPI_BUS_0 | |
| SPI_NUM_BUS | |
Definition at line 57 of file isf_sysconf_comms.c.
| uint32 get_ci_comm | ( | void | ) |
Definition at line 93 of file isf_sysconf_comms.c.
References COMM_CHANNEL_UART2.
Referenced by ci_init().

| const sys_channelDescriptor_t gSys_ConfiguredChannelList[] |
This data structure/variable holds the complete state of the rli magnetometer sensor embedded application.
Definition at line 71 of file isf_sysconf_comms.c.
| const i2c_Master_BusConfig_t gSys_I2cBusConfig[] |
Definition at line 22 of file isf_sysconf_comms.c.
| const uint8 gSys_NumChannels = sizeof(gSys_ConfiguredChannelList)/sizeof(sys_channelDescriptor_t) |
Definition at line 98 of file isf_sysconf_comms.c.
Referenced by dm_channel_init().
| const uint8 gSys_NumI2cBuses = I2C_INSTANCE_COUNT |
Definition at line 28 of file isf_sysconf_comms.c.
Referenced by i2c_master_adapter_init().
| const uint8 gSys_NumSpiBuses = SPI_INSTANCE_COUNT |
Definition at line 63 of file isf_sysconf_comms.c.
Referenced by spi_master_adapter_init().
| const uint8 gSys_NumUartBuses = UART_INSTANCE_COUNT |
Definition at line 45 of file isf_sysconf_comms.c.
Referenced by uart_adapter_init().
| i2c_Master_busHandle_t i2c_master_busHandle[I2C_INSTANCE_COUNT] |
Definition at line 29 of file isf_sysconf_comms.c.
| mutex_t i2c_Master_mutexHandler[I2C_INSTANCE_COUNT] |
Definition at line 30 of file isf_sysconf_comms.c.
Referenced by i2c_master_adapter_init().
| spi_master_busHandle_t spi_busHandle[SPI_INSTANCE_COUNT] |
Definition at line 64 of file isf_sysconf_comms.c.
| mutex_t spi_lock[SPI_INSTANCE_COUNT] |
Definition at line 65 of file isf_sysconf_comms.c.
Referenced by spi_master_adapter_init().
| mutex_t spi_rdlock[SPI_INSTANCE_COUNT] |
Definition at line 66 of file isf_sysconf_comms.c.
Referenced by spi_master_adapter_init().
| uart_busHandle_t uart_busHandle[UART_INSTANCE_COUNT] |
Definition at line 46 of file isf_sysconf_comms.c.
| mutex_t uart_lock[UART_INSTANCE_COUNT] |
Definition at line 47 of file isf_sysconf_comms.c.
Referenced by uart_adapter_init().
| mutex_t uart_rdlock[UART_INSTANCE_COUNT] |
Definition at line 48 of file isf_sysconf_comms.c.
Referenced by uart_adapter_init().