![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "fsl_device_registers.h"#include "fsl_port_hal.h"#include "fsl_sim_hal.h"#include "pin_init.h"
Go to the source code of this file.
Functions | |
| void | init_adc_pins (uint32_t instance) |
| ADC method sets registers according routing settings. Call this method code to route desired pins into: ADC0, ADC1 peripherals. More... | |
| void | deinit_adc_pins (uint32_t instance) |
| ADC method sets registers according routing settings. Call this method code to disable routing of desired pins for: ADC0, ADC1 peripherals. More... | |
| void | init_cmp_pins (uint32_t instance) |
| CMP method sets registers according routing settings. Call this method code to route desired pins into: CMP0, CMP1, CMP2 peripherals. More... | |
| void | deinit_cmp_pins (uint32_t instance) |
| CMP method sets registers according routing settings. Call this method code to disable routing of desired pins for: CMP0, CMP1, CMP2 peripherals. More... | |
| void | init_enet_pins (uint32_t instance) |
| ENET method sets registers according routing settings. Call this method code to route desired pins into ENET periphery. More... | |
| void | deinit_enet_pins (uint32_t instance) |
| ENET method sets registers according routing settings. Call this method code to disable routing of desired pins for ENET periphery. More... | |
| void | init_gpio_pins (uint32_t instance) |
| GPIO method sets registers according routing settings. Call this method code to route desired pins into: PTA, PTB, PTC, PTD, PTE peripherals. More... | |
| void | deinit_gpio_pins (uint32_t instance) |
| GPIO method sets registers according routing settings. Call this method code to disable routing of desired pins for: PTA, PTB, PTC, PTD, PTE peripherals. More... | |
| void | init_i2c_pins (uint32_t instance) |
| I2C method sets registers according routing settings. Call this method code to route desired pins into: I2C0, I2C1, I2C2 peripherals. More... | |
| void | deinit_i2c_pins (uint32_t instance) |
| I2C method sets registers according routing settings. Call this method code to disable routing of desired pins for: I2C0, I2C1, I2C2 peripherals. More... | |
| void | init_jtag_pins (uint32_t instance) |
| JTAG method sets registers according routing settings. Call this method code to route desired pins into JTAG periphery. More... | |
| void | deinit_jtag_pins (uint32_t instance) |
| JTAG method sets registers according routing settings. Call this method code to disable routing of desired pins for JTAG periphery. More... | |
| void | init_llwu_pins (uint32_t instance) |
| LLWU method sets registers according routing settings. Call this method code to route desired pins into LLWU periphery. More... | |
| void | deinit_llwu_pins (uint32_t instance) |
| LLWU method sets registers according routing settings. Call this method code to disable routing of desired pins for LLWU periphery. More... | |
| void | init_osc_pins (uint32_t instance) |
| OSC method sets registers according routing settings. Call this method code to route desired pins into OSC periphery. More... | |
| void | deinit_osc_pins (uint32_t instance) |
| OSC method sets registers according routing settings. Call this method code to disable routing of desired pins for OSC periphery. More... | |
| void | init_spi_pins (uint32_t instance) |
| SPI method sets registers according routing settings. Call this method code to route desired pins into: SPI0, SPI1, SPI2 peripherals. More... | |
| void | deinit_spi_pins (uint32_t instance) |
| SPI method sets registers according routing settings. Call this method code to disable routing of desired pins for: SPI0, SPI1, SPI2 peripherals. More... | |
| void | init_tpiu_pins (uint32_t instance) |
| TPIU method sets registers according routing settings. Call this method code to route desired pins into TPIU periphery. More... | |
| void | deinit_tpiu_pins (uint32_t instance) |
| TPIU method sets registers according routing settings. Call this method code to disable routing of desired pins for TPIU periphery. More... | |
| void | init_uart_pins (uint32_t instance) |
| UART method sets registers according routing settings. Call this method code to route desired pins into: UART0, UART1, UART2, UART3, UART4, UART5 peripherals. More... | |
| void | deinit_uart_pins (uint32_t instance) |
| UART method sets registers according routing settings. Call this method code to disable routing of desired pins for: UART0, UART1, UART2, UART3, UART4, UART5 peripherals. More... | |
Definition in file pin_init.c.