![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|

Go to the source code of this file.
Functions | |
| void | init_adc_pins (uint32_t instance) |
| ADC method sets registers according routing settings. Call this method code to route desired pins into: ADC0, ADC1 peripherals. More... | |
| void | deinit_adc_pins (uint32_t instance) |
| ADC method sets registers according routing settings. Call this method code to disable routing of desired pins for: ADC0, ADC1 peripherals. More... | |
| void | init_can_pins (uint32_t instance) |
| CAN method sets registers according routing settings. Call this method code to route desired pins into CAN0 periphery. More... | |
| void | deinit_can_pins (uint32_t instance) |
| CAN method sets registers according routing settings. Call this method code to disable routing of desired pins for CAN0 periphery. More... | |
| void | init_cmp_pins (uint32_t instance) |
| CMP method sets registers according routing settings. Call this method code to route desired pins into: CMP0, CMP1, CMP2 peripherals. More... | |
| void | deinit_cmp_pins (uint32_t instance) |
| CMP method sets registers according routing settings. Call this method code to disable routing of desired pins for: CMP0, CMP1, CMP2 peripherals. More... | |
| void | init_cmt_pins (uint32_t instance) |
| CMT method sets registers according routing settings. Call this method code to route desired pins into CMT periphery. More... | |
| void | deinit_cmt_pins (uint32_t instance) |
| CMT method sets registers according routing settings. Call this method code to disable routing of desired pins for CMT periphery. More... | |
| void | init_dac_pins (uint32_t instance) |
| DAC method sets registers according routing settings. Call this method code to route desired pins into DAC0 periphery. More... | |
| void | deinit_dac_pins (uint32_t instance) |
| DAC method sets registers according routing settings. Call this method code to disable routing of desired pins for DAC0 periphery. More... | |
| void | init_dma_pins (uint32_t instance) |
| DMA method sets registers according routing settings. Call this method code to route desired pins into DMA periphery. More... | |
| void | deinit_dma_pins (uint32_t instance) |
| DMA method sets registers according routing settings. Call this method code to disable routing of desired pins for DMA periphery. More... | |
| void | init_enet_pins (uint32_t instance) |
| ENET method sets registers according routing settings. Call this method code to route desired pins into ENET periphery. More... | |
| void | deinit_enet_pins (uint32_t instance) |
| ENET method sets registers according routing settings. Call this method code to disable routing of desired pins for ENET periphery. More... | |
| void | init_ewm_pins (uint32_t instance) |
| EWM method sets registers according routing settings. Call this method code to route desired pins into EWM periphery. More... | |
| void | deinit_ewm_pins (uint32_t instance) |
| EWM method sets registers according routing settings. Call this method code to disable routing of desired pins for EWM periphery. More... | |
| void | init_fb_pins (uint32_t instance) |
| FB method sets registers according routing settings. Call this method code to route desired pins into FB periphery. More... | |
| void | deinit_fb_pins (uint32_t instance) |
| FB method sets registers according routing settings. Call this method code to disable routing of desired pins for FB periphery. More... | |
| void | init_ftm_pins (uint32_t instance) |
| FTM method sets registers according routing settings. Call this method code to route desired pins into: FTM0, FTM1, FTM2, FTM3 peripherals. More... | |
| void | deinit_ftm_pins (uint32_t instance) |
| FTM method sets registers according routing settings. Call this method code to disable routing of desired pins for: FTM0, FTM1, FTM2, FTM3 peripherals. More... | |
| void | init_gpio_pins (uint32_t instance) |
| GPIO method sets registers according routing settings. Call this method code to route desired pins into: PTA, PTB, PTC, PTD, PTE peripherals. More... | |
| void | deinit_gpio_pins (uint32_t instance) |
| GPIO method sets registers according routing settings. Call this method code to disable routing of desired pins for: PTA, PTB, PTC, PTD, PTE peripherals. More... | |
| void | init_i2c_pins (uint32_t instance) |
| I2C method sets registers according routing settings. Call this method code to route desired pins into: I2C0, I2C1, I2C2 peripherals. More... | |
| void | deinit_i2c_pins (uint32_t instance) |
| I2C method sets registers according routing settings. Call this method code to disable routing of desired pins for: I2C0, I2C1, I2C2 peripherals. More... | |
| void | init_i2s_pins (uint32_t instance) |
| I2S method sets registers according routing settings. Call this method code to route desired pins into I2S0 periphery. More... | |
| void | deinit_i2s_pins (uint32_t instance) |
| I2S method sets registers according routing settings. Call this method code to disable routing of desired pins for I2S0 periphery. More... | |
| void | init_jtag_pins (uint32_t instance) |
| JTAG method sets registers according routing settings. Call this method code to route desired pins into JTAG periphery. More... | |
| void | deinit_jtag_pins (uint32_t instance) |
| JTAG method sets registers according routing settings. Call this method code to disable routing of desired pins for JTAG periphery. More... | |
| void | init_llwu_pins (uint32_t instance) |
| LLWU method sets registers according routing settings. Call this method code to route desired pins into LLWU periphery. More... | |
| void | deinit_llwu_pins (uint32_t instance) |
| LLWU method sets registers according routing settings. Call this method code to disable routing of desired pins for LLWU periphery. More... | |
| void | init_lptmr_pins (uint32_t instance) |
| LPTMR method sets registers according routing settings. Call this method code to route desired pins into LPTMR0 periphery. More... | |
| void | deinit_lptmr_pins (uint32_t instance) |
| LPTMR method sets registers according routing settings. Call this method code to disable routing of desired pins for LPTMR0 periphery. More... | |
| void | init_osc_pins (uint32_t instance) |
| OSC method sets registers according routing settings. Call this method code to route desired pins into OSC periphery. More... | |
| void | deinit_osc_pins (uint32_t instance) |
| OSC method sets registers according routing settings. Call this method code to disable routing of desired pins for OSC periphery. More... | |
| void | init_pdb_pins (uint32_t instance) |
| PDB method sets registers according routing settings. Call this method code to route desired pins into PDB0 periphery. More... | |
| void | deinit_pdb_pins (uint32_t instance) |
| PDB method sets registers according routing settings. Call this method code to disable routing of desired pins for PDB0 periphery. More... | |
| void | init_rcm_pins (uint32_t instance) |
| RCM method sets registers according routing settings. Call this method code to route desired pins into RCM periphery. More... | |
| void | deinit_rcm_pins (uint32_t instance) |
| RCM method sets registers according routing settings. Call this method code to disable routing of desired pins for RCM periphery. More... | |
| void | init_rtc_pins (uint32_t instance) |
| RTC method sets registers according routing settings. Call this method code to route desired pins into RTC periphery. More... | |
| void | deinit_rtc_pins (uint32_t instance) |
| RTC method sets registers according routing settings. Call this method code to disable routing of desired pins for RTC periphery. More... | |
| void | init_scb_pins (uint32_t instance) |
| SCB method sets registers according routing settings. Call this method code to route desired pins into SystemControl periphery. More... | |
| void | deinit_scb_pins (uint32_t instance) |
| SCB method sets registers according routing settings. Call this method code to disable routing of desired pins for SystemControl periphery. More... | |
| void | init_sdhc_pins (uint32_t instance) |
| SDHC method sets registers according routing settings. Call this method code to route desired pins into SDHC periphery. More... | |
| void | deinit_sdhc_pins (uint32_t instance) |
| SDHC method sets registers according routing settings. Call this method code to disable routing of desired pins for SDHC periphery. More... | |
| void | init_sim_pins (uint32_t instance) |
| SIM method sets registers according routing settings. Call this method code to route desired pins into SIM periphery. More... | |
| void | deinit_sim_pins (uint32_t instance) |
| SIM method sets registers according routing settings. Call this method code to disable routing of desired pins for SIM periphery. More... | |
| void | init_spi_pins (uint32_t instance) |
| SPI method sets registers according routing settings. Call this method code to route desired pins into: SPI0, SPI1, SPI2 peripherals. More... | |
| void | deinit_spi_pins (uint32_t instance) |
| SPI method sets registers according routing settings. Call this method code to disable routing of desired pins for: SPI0, SPI1, SPI2 peripherals. More... | |
| void | init_supply_pins (uint32_t instance) |
| SUPPLY method sets registers according routing settings. Call this method code to route desired pins into SUPPLY periphery. More... | |
| void | deinit_supply_pins (uint32_t instance) |
| SUPPLY method sets registers according routing settings. Call this method code to disable routing of desired pins for SUPPLY periphery. More... | |
| void | init_tpiu_pins (uint32_t instance) |
| TPIU method sets registers according routing settings. Call this method code to route desired pins into TPIU periphery. More... | |
| void | deinit_tpiu_pins (uint32_t instance) |
| TPIU method sets registers according routing settings. Call this method code to disable routing of desired pins for TPIU periphery. More... | |
| void | init_uart_pins (uint32_t instance) |
| UART method sets registers according routing settings. Call this method code to route desired pins into: UART0, UART1, UART2, UART3, UART4, UART5 peripherals. More... | |
| void | deinit_uart_pins (uint32_t instance) |
| UART method sets registers according routing settings. Call this method code to disable routing of desired pins for: UART0, UART1, UART2, UART3, UART4, UART5 peripherals. More... | |
| void | init_usb_pins (uint32_t instance) |
| USB method sets registers according routing settings. Call this method code to route desired pins into USB0 periphery. More... | |
| void | deinit_usb_pins (uint32_t instance) |
| USB method sets registers according routing settings. Call this method code to disable routing of desired pins for USB0 periphery. More... | |
| void | init_usbdcd_pins (uint32_t instance) |
| USBDCD method sets registers according routing settings. Call this method code to route desired pins into USBDCD periphery. More... | |
| void | deinit_usbdcd_pins (uint32_t instance) |
| USBDCD method sets registers according routing settings. Call this method code to disable routing of desired pins for USBDCD periphery. More... | |
| void | init_vref_pins (uint32_t instance) |
| VREF method sets registers according routing settings. Call this method code to route desired pins into VREF periphery. More... | |
| void | deinit_vref_pins (uint32_t instance) |
| VREF method sets registers according routing settings. Call this method code to disable routing of desired pins for VREF periphery. More... | |
Definition in file pin_init.h.