![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_Sensor_Analog_1_Functions.h>

Data Fields | |
| uint32 | timeStamp |
| uint16 | data [MAX_ADC_CHANNELS] |
| uint8 | addr |
This structure defines the dummy DSA data buffer format.
Definition at line 128 of file fsl_Sensor_Analog_1_Functions.h.
| uint8 addr |
Definition at line 132 of file fsl_Sensor_Analog_1_Functions.h.
| uint16 data[MAX_ADC_CHANNELS] |
The Sensor data
Definition at line 131 of file fsl_Sensor_Analog_1_Functions.h.
Referenced by Analog_1_fixed_converter(), Analog_1_float_converter(), Analog_1_fsl_Sensor_Generic_Analog_Initialize(), and Analog_1_fsl_Sensor_Generic_AnalogCallback().
| uint32 timeStamp |
The time stamp for the data packet.
Definition at line 130 of file fsl_Sensor_Analog_1_Functions.h.
Referenced by Analog_1_fixed_converter(), Analog_1_float_converter(), Analog_1_fsl_Sensor_Generic_Analog_Initialize(), and Analog_1_fsl_Sensor_Generic_AnalogCallback().