![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure stores sample Information necessary to communicate with non I2C slave device. More...
#include <fsl_Sensor_Analog_1_Functions.h>

Data Fields | |
| uint16_t | dummy |
| uint16_t | address |
This structure stores sample Information necessary to communicate with non I2C slave device.
Definition at line 114 of file fsl_Sensor_Analog_1_Functions.h.
| uint16_t address |
Definition at line 117 of file fsl_Sensor_Analog_1_Functions.h.
| uint16_t dummy |
Definition at line 116 of file fsl_Sensor_Analog_1_Functions.h.