![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <BasicApp1_types.h>

Definition at line 372 of file BasicApp1_types.h.
| uint8 processedData[34] |
Definition at line 394 of file BasicApp1_types.h.
| DATA_TYPE_SUB0 rawAccelerometerData_Sub0[DATA_FIFO_LEN_SUB0] |
Definition at line 374 of file BasicApp1_types.h.
| DATA_TYPE_SUB1 rawAccelerometerData_Sub1[DATA_FIFO_LEN_SUB1] |
Definition at line 375 of file BasicApp1_types.h.
| DATA_TYPE_SUB2 rawAccelerometerData_Sub2[DATA_FIFO_LEN_SUB2] |
Definition at line 376 of file BasicApp1_types.h.
| DATA_TYPE_SUB3 rawAccelerometerData_Sub3[DATA_FIFO_LEN_SUB3] |
Definition at line 377 of file BasicApp1_types.h.
| DATA_TYPE_SUB4 rawAccelerometerData_Sub4[DATA_FIFO_LEN_SUB4] |
Definition at line 378 of file BasicApp1_types.h.
| DATA_TYPE_SUB5 rawAccelerometerData_Sub5[DATA_FIFO_LEN_SUB5] |
Definition at line 379 of file BasicApp1_types.h.
| DATA_TYPE_SUB6 rawAccelerometerData_Sub6[DATA_FIFO_LEN_SUB6] |
Definition at line 380 of file BasicApp1_types.h.
| DATA_TYPE_SUB7 rawAccelerometerData_Sub7[DATA_FIFO_LEN_SUB7] |
Definition at line 381 of file BasicApp1_types.h.
| DATA_TYPE_SUB15 rawAltitudeData_Sub15[DATA_FIFO_LEN_SUB15] |
Definition at line 389 of file BasicApp1_types.h.
| DATA_TYPE_SUB19 rawAnalogData_Sub19[DATA_FIFO_LEN_SUB19] |
Definition at line 393 of file BasicApp1_types.h.
| DATA_TYPE_SUB18 rawCustomData_Sub18[DATA_FIFO_LEN_SUB18] |
Definition at line 392 of file BasicApp1_types.h.
| DATA_TYPE_SUB10 rawGyrometerData_Sub10[DATA_FIFO_LEN_SUB10] |
Definition at line 384 of file BasicApp1_types.h.
| DATA_TYPE_SUB11 rawGyrometerData_Sub11[DATA_FIFO_LEN_SUB11] |
Definition at line 385 of file BasicApp1_types.h.
| DATA_TYPE_SUB8 rawMagnetometerData_Sub8[DATA_FIFO_LEN_SUB8] |
Definition at line 382 of file BasicApp1_types.h.
| DATA_TYPE_SUB9 rawMagnetometerData_Sub9[DATA_FIFO_LEN_SUB9] |
Definition at line 383 of file BasicApp1_types.h.
| DATA_TYPE_SUB14 rawOrientationData_Sub14[DATA_FIFO_LEN_SUB14] |
Definition at line 388 of file BasicApp1_types.h.
| DATA_TYPE_SUB16 rawPedometerData_Sub16[DATA_FIFO_LEN_SUB16] |
Definition at line 390 of file BasicApp1_types.h.
| DATA_TYPE_SUB17 rawPedometerData_Sub17[DATA_FIFO_LEN_SUB17] |
Definition at line 391 of file BasicApp1_types.h.
| DATA_TYPE_SUB12 rawPressureData_Sub12[DATA_FIFO_LEN_SUB12] |
Definition at line 386 of file BasicApp1_types.h.
| DATA_TYPE_SUB13 rawTemperatureData_Sub13[DATA_FIFO_LEN_SUB13] |
Definition at line 387 of file BasicApp1_types.h.