![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_Sensor_Custom_1_Functions.h>

Data Fields | |
| uint32 | timeStamp |
| int16 | data [3] |
| uint8 | addr |
This structure defines the dummy DSA data buffer format.
Definition at line 119 of file fsl_Sensor_Custom_1_Functions.h.
| uint8 addr |
Definition at line 123 of file fsl_Sensor_Custom_1_Functions.h.
Referenced by Custom_1_fsl_Sensor_Custom_Initialize().
| int16 data[3] |
The Sensor data
Definition at line 122 of file fsl_Sensor_Custom_1_Functions.h.
Referenced by Custom_1_fixed_Custom_converter(), Custom_1_float_Custom_converter(), Custom_1_fsl_Sensor_Custom_Initialize(), and Custom_1_fsl_Sensor_Custom_PeriodicCallback().
| uint32 timeStamp |
The time stamp for the data packet.
Definition at line 121 of file fsl_Sensor_Custom_1_Functions.h.
Referenced by Custom_1_fixed_Custom_converter(), Custom_1_float_Custom_converter(), Custom_1_fsl_Sensor_Custom_Initialize(), and Custom_1_fsl_Sensor_Custom_PeriodicCallback().