![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines important settings. More...
#include <fsl_Sensor_Custom_1_Functions.h>

Data Fields | |
| uint8 | sampleRateIndex |
| Holds the ODR index into the rate array fsl_mma865x_period */. More... | |
This structure defines important settings.
Definition at line 159 of file fsl_Sensor_Custom_1_Functions.h.
| uint8 sampleRateIndex |
Holds the ODR index into the rate array fsl_mma865x_period */.
Definition at line 161 of file fsl_Sensor_Custom_1_Functions.h.