![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This defines the DSA sensor configuration structure defining each individual sensor adapter in the DSA Sensor List. More...
#include <isf_dsa_adapter.h>

Data Fields | |
| const isf_dsa_Adapter_t * | pAdapter |
| void * | pSensorSpecificSettings |
| sys_channelId_t | channelId |
| const void * | commInfo |
This defines the DSA sensor configuration structure defining each individual sensor adapter in the DSA Sensor List.
Definition at line 154 of file isf_dsa_adapter.h.
| sys_channelId_t channelId |
Sensor device physical channel identification value.
Definition at line 158 of file isf_dsa_adapter.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Initialize(), fsl_fxlc95000_Initialize(), fsl_fxls8471_i2cspi_3D_accel_Initialize(), fsl_fxls8952_i2c_3D_accel_Initialize(), fsl_fxos8700_i2cspi_6D_AccMag_Initialize(), fsl_mag3110_i2c_3D_mag_Initialize(), fsl_mma8491q_i2c_3D_accel_Initialize(), fsl_mma865x_i2c_3D_accel_Initialize(), fsl_mma955x_Initialize(), and fsl_mpl3115_i2c_1D_press_Initialize().
| const void* commInfo |
Sensor device specific communications info.
Definition at line 159 of file isf_dsa_adapter.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Initialize(), fsl_fxlc95000_Initialize(), fsl_fxls8471_i2cspi_3D_accel_Initialize(), fsl_fxls8952_i2c_3D_accel_Initialize(), fsl_fxos8700_i2cspi_6D_AccMag_Initialize(), fsl_mag3110_i2c_3D_mag_Initialize(), fsl_mma8491q_i2c_3D_accel_Initialize(), fsl_mma865x_i2c_3D_accel_Initialize(), fsl_mma955x_Initialize(), and fsl_mpl3115_i2c_1D_press_Initialize().
| const isf_dsa_Adapter_t* pAdapter |
Pointer to the statically initialized adapter structure.
Definition at line 156 of file isf_dsa_adapter.h.
Referenced by BasicApp1_FlashSensor(), configure_sensor(), convert_sensor_data(), init_sensor(), shutdown_sensor(), start_sensor(), and stop_sensor().
| void* pSensorSpecificSettings |
Pointer to the adapter sensor specific settings.
Definition at line 157 of file isf_dsa_adapter.h.
Referenced by fsl_fusion_task(), fsl_fusion_virt_3D_orient_Configure(), fsl_fusion_virt_3D_orient_Convert(), fsl_fusion_virt_3D_orient_EndData(), fsl_fusion_virt_3D_orient_Initialize(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fusion_virt_3D_orient_Shutdown(), fsl_fusion_virt_3D_orient_StartData(), fsl_fusion_virt_3D_orient_ValidateSettings(), fsl_fxas21002_i2cspi_3D_gyro_Configure(), fsl_fxas21002_i2cspi_3D_gyro_Convert(), fsl_fxlc95000_Configure(), fsl_fxlc95000_Convert(), fsl_fxlc95000_EndData(), fsl_fxlc95000_Flash(), fsl_fxlc95000_Shutdown(), fsl_fxlc95000_StartData(), fsl_fxls8471_i2cspi_3D_accel_Convert(), fsl_fxls8952_i2c_3D_accel_Configure(), fsl_fxls8952_i2c_3D_accel_Convert(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_Shutdown(), fsl_fxls8952_i2c_3D_accel_StartData(), fsl_fxls8952_i2c_3D_accel_ValidateSettings(), fsl_fxos8700_i2cspi_6D_AccMag_Configure(), fsl_fxos8700_i2cspi_6D_AccMag_Convert(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_StartData(), fsl_fxos8700_i2cspi_6D_AccMag_ValidateSettings(), fsl_mag3110_i2c_3D_mag_Convert(), fsl_mma8491q_i2c_3D_accel_Convert(), fsl_mma865x_i2c_3D_accel_Convert(), fsl_mma955x_Configure(), fsl_mma955x_Convert(), fsl_mma955x_EndData(), fsl_mma955x_Initialize(), fsl_mma955x_Shutdown(), fsl_mma955x_StartData(), fsl_mpl3115_i2c_1D_press_Convert(), fxlc95000_GetConfig(), fxlc95000_GetData(), fxlc95000_ValidateConfig(), fxlc95000_WriteConfig(), fxls8471_SetConfig(), mag3110_SetConfig(), mag3110_ValidateConfig(), mma865x_SetConfig(), mma955x_GetConfig(), mma955x_GetData(), mma955x_GetPedometerData(), mma955x_ValidateConfig(), mma955x_WriteConfig(), and mpl3115_SetConfig().