![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure holds the build information of device/lib/component /user application etc. More...
#include <isf.h>

Data Fields | |
| uint8 | buildYear |
| The Year of the build (valid values: 2000 + buildYear, max value = 2255) More... | |
| uint8 | buildMonth |
| The Month of the build (valid values: 1(JAN) to 12(DEC)) More... | |
| uint8 | buildDay |
| The Day of the build (valid values: 1 to 31) More... | |
| uint8 | buildHours |
| The time of build in hours (in 24-hour notation) (valid values: 0 to 23) More... | |
| uint8 | buildMinutes |
| The time of build in minutes (valid values: 0 to 59) More... | |
| uint8 | buildSeconds |
| The time of build in seconds (valid values: 0 to 59) More... | |
| uint8 | buildId [MAX_ISF_COMMIT_ID_SIZE] |
| The last commit_id from which the build is made. More... | |
This structure holds the build information of device/lib/component /user application etc.
| uint8 buildDay |
The Day of the build (valid values: 1 to 31)
Definition at line 152 of file isf.h.
Referenced by isf_get_info().
| uint8 buildHours |
The time of build in hours (in 24-hour notation) (valid values: 0 to 23)
Definition at line 154 of file isf.h.
Referenced by isf_get_info().
| uint8 buildId[MAX_ISF_COMMIT_ID_SIZE] |
The last commit_id from which the build is made.
Definition at line 160 of file isf.h.
Referenced by isf_get_info().
| uint8 buildMinutes |
The time of build in minutes (valid values: 0 to 59)
Definition at line 156 of file isf.h.
Referenced by isf_get_info().
| uint8 buildMonth |
The Month of the build (valid values: 1(JAN) to 12(DEC))
Definition at line 150 of file isf.h.
Referenced by isf_get_info().
| uint8 buildSeconds |
The time of build in seconds (valid values: 0 to 59)
Definition at line 158 of file isf.h.
Referenced by isf_get_info().
| uint8 buildYear |
The Year of the build (valid values: 2000 + buildYear, max value = 2255)
Definition at line 148 of file isf.h.
Referenced by isf_get_info().