![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Stream instance structure is used internally to encapsulate the information of a stream and the current trigger state of the dataset(s) belonging to that stream. It also contains a pointer to the next stream to create a single linked list of streams. More...
#include <ci_protocol_stream.h>

Stream instance structure is used internally to encapsulate the information of a stream and the current trigger state of the dataset(s) belonging to that stream. It also contains a pointer to the next stream to create a single linked list of streams.