![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_fxas21002_i2cspi_3D_gyro.h>

Data Fields | |
| uint32 | timeStamp |
| int16 | gyro [3] |
| uint8 | temperature |
This structure defines the dummy DSA data buffer format.
Definition at line 25 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| int16 gyro[3] |
The gyronetometer data
Definition at line 27 of file fsl_fxas21002_i2cspi_3D_gyro.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Initialize(), and fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback().
| uint8 temperature |
The device temperature measured in celsius scale
Definition at line 28 of file fsl_fxas21002_i2cspi_3D_gyro.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback().
| uint32 timeStamp |
The time stamp for the data packet.
Definition at line 26 of file fsl_fxas21002_i2cspi_3D_gyro.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Initialize(), and fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback().