![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_fxlc95000_i2cspi_pedo.h>

Data Fields | |
| uint32 | timeStamp |
| int16 | accel [3] |
| int16 | temp |
This structure defines the dummy DSA data buffer format.
Definition at line 28 of file fsl_fxlc95000_i2cspi_pedo.h.
| int16 accel[3] |
The accelerometer data
Definition at line 30 of file fsl_fxlc95000_i2cspi_pedo.h.
| int16 temp |
The temperature data
Definition at line 31 of file fsl_fxlc95000_i2cspi_pedo.h.
| uint32 timeStamp |
The time stamp for the data packet.
Definition at line 29 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_PeriodicCallback().