![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <fsl_fxlc95000_i2cspi_pedo.h>

Definition at line 35 of file fsl_fxlc95000_i2cspi_pedo.h.
| dm_ChannelDescriptor_t cDescriptor |
Device Messaging channel descriptor
Definition at line 36 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_Initialize().
| dm_DeviceDescriptor_t deviceHandle |
Device messaging device handle.
Definition at line 37 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_Configure(), fsl_fxlc95000_EndData(), fsl_fxlc95000_Initialize(), fsl_fxlc95000_Shutdown(), fsl_fxlc95000_StartData(), fxlc95000_GetConfig(), fxlc95000_GetData(), fxlc95000_ValidateConfig(), and fxlc95000_WriteConfig().
| semaphore_t deviceSemaphore |
Task synchronization mechanism for this data structure.
Definition at line 38 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_Configure(), fsl_fxlc95000_EndData(), fsl_fxlc95000_Initialize(), fsl_fxlc95000_PeriodicCallback(), and fsl_fxlc95000_StartData().
| fxlc95000_appConfigRegister_t localCfgBuffer |
Hold a local copy of the FXLC95000 App config registers
Definition at line 41 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_Configure().
| uint8 localCfgBufSize |
Number of bytes on the localCfgBuffer array
Definition at line 42 of file fsl_fxlc95000_i2cspi_pedo.h.
| fxlc95000_DataBuffer_t* pCurrentSample |
Holds the most recently read sample
Definition at line 40 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_Initialize(), and fsl_fxlc95000_PeriodicCallback().
| uint8 tempReadBuffer[32] |
scratch buffer for result of miscellaneous reads
Definition at line 43 of file fsl_fxlc95000_i2cspi_pedo.h.
| bm_callback_token_t token |
Bus Manager handle
Definition at line 39 of file fsl_fxlc95000_i2cspi_pedo.h.
Referenced by fsl_fxlc95000_Configure(), fsl_fxlc95000_EndData(), fsl_fxlc95000_Shutdown(), and fsl_fxlc95000_StartData().