![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <fxlc95000.h>

Data Fields | |
| const int32 | sampleDataOffset |
| const int32 | sampleDataSize |
| const int32 | configRegisterReadOffset |
| const int32 | configRegisterReadSize |
| const float | engFloatConversionFactor |
| const uint8 | engFixedTotalWidth |
| const uint8 | engFixedIntegerWidth |
| const uint8 | engFixedSignBit |
| const uint8 | resolution |
| const uint8 | range |
| const uint8 | mode |
| const fxlc95000_CommandList_t | writeConfigRegisterPreamble |
| const fxlc95000_CommandList_t | readConfigCommands |
| const fxlc95000_CommandList_t | validateSettingsCommands |
| const fxlc95000_CommandList_t | initializeCommands |
| const fxlc95000_CommandList_t | configureCommands |
| const fxlc95000_CommandList_t | startDataCommands |
| const fxlc95000_CommandList_t | endDataCommands |
| const fxlc95000_CommandList_t | calibrateCommands |
| const fxlc95000_CommandList_t | shutdownCommands |
| const fxlc95000_CommandList_t | getDataCommands |
| const fxlc95000_CommandList_t | flashPreprocessCommands |
| const fxlc95000_CommandList_t | flashPostprocessCommands |
Definition at line 63 of file fxlc95000.h.
| const fxlc95000_CommandList_t calibrateCommands |
Definition at line 83 of file fxlc95000.h.
| const int32 configRegisterReadOffset |
Definition at line 67 of file fxlc95000.h.
Referenced by fxlc95000_GetConfig().
| const int32 configRegisterReadSize |
Definition at line 68 of file fxlc95000.h.
Referenced by fxlc95000_GetConfig(), and fxlc95000_WriteConfig().
| const fxlc95000_CommandList_t configureCommands |
Definition at line 80 of file fxlc95000.h.
| const fxlc95000_CommandList_t endDataCommands |
Definition at line 82 of file fxlc95000.h.
| const uint8 engFixedIntegerWidth |
Definition at line 71 of file fxlc95000.h.
| const uint8 engFixedSignBit |
Definition at line 72 of file fxlc95000.h.
| const uint8 engFixedTotalWidth |
Definition at line 70 of file fxlc95000.h.
| const float engFloatConversionFactor |
Definition at line 69 of file fxlc95000.h.
| const fxlc95000_CommandList_t flashPostprocessCommands |
Definition at line 87 of file fxlc95000.h.
Referenced by fsl_fxlc95000_Flash().
| const fxlc95000_CommandList_t flashPreprocessCommands |
Definition at line 86 of file fxlc95000.h.
Referenced by fsl_fxlc95000_Flash().
| const fxlc95000_CommandList_t getDataCommands |
Definition at line 85 of file fxlc95000.h.
| const fxlc95000_CommandList_t initializeCommands |
Definition at line 79 of file fxlc95000.h.
| const uint8 mode |
Definition at line 75 of file fxlc95000.h.
| const uint8 range |
Definition at line 74 of file fxlc95000.h.
| const fxlc95000_CommandList_t readConfigCommands |
Definition at line 77 of file fxlc95000.h.
Referenced by fxlc95000_GetConfig().
| const uint8 resolution |
Definition at line 73 of file fxlc95000.h.
| const int32 sampleDataOffset |
Definition at line 65 of file fxlc95000.h.
Referenced by fxlc95000_GetData().
| const int32 sampleDataSize |
Definition at line 66 of file fxlc95000.h.
Referenced by fxlc95000_GetData().
| const fxlc95000_CommandList_t shutdownCommands |
Definition at line 84 of file fxlc95000.h.
| const fxlc95000_CommandList_t startDataCommands |
Definition at line 81 of file fxlc95000.h.
Referenced by fsl_fxlc95000_StartData().
| const fxlc95000_CommandList_t validateSettingsCommands |
Definition at line 78 of file fxlc95000.h.
Referenced by fxlc95000_ValidateConfig().
| const fxlc95000_CommandList_t writeConfigRegisterPreamble |
Definition at line 76 of file fxlc95000.h.
Referenced by fxlc95000_WriteConfig().