![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
the structure defines the configuration table. More...
#include <fsl_fxos8700_i2cspi_6D_AccMag.h>

Data Fields | |
| void * | memberVariable |
| uint8 | startAddress |
| uint8 | size |
the structure defines the configuration table.
Definition at line 97 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| void* memberVariable |
reference to the member variable.
Definition at line 98 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| uint8 size |
size of the memeber to be configured.
Definition at line 100 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| uint8 startAddress |
start address to the member variable.
Definition at line 99 of file fsl_fxos8700_i2cspi_6D_AccMag.h.