![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This defines the DSA adapter functional interface. More...
#include <isf_dsa_adapter.h>

Data Fields | |
| event_t * | pEventGroup |
| uint32 | nEventFieldIndex |
| isf_dsa_SensorSettings_t | sensorSettings |
This defines the DSA adapter functional interface.
Definition at line 90 of file isf_dsa_adapter.h.
| uint32 nEventFieldIndex |
The event flag of the event group to signal after depositing sensor sample in pSampleBuffer.
Definition at line 93 of file isf_dsa_adapter.h.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxlc95000_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_PeriodicCallback(), and init_sensor().
| event_t* pEventGroup |
The event group to signal after depositing sensor sample in pDataBuff.
Definition at line 92 of file isf_dsa_adapter.h.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxlc95000_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_PeriodicCallback(), and init_sensor().
| isf_dsa_SensorSettings_t sensorSettings |
The configuration parameters from the user including the fifo to use
Definition at line 94 of file isf_dsa_adapter.h.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), configure_sensor(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxlc95000_Configure(), fsl_fxlc95000_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_Configure(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_Configure(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_Configure(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_i2c_3D_accel_Configure(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_Configure(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_Configure(), fsl_mma955x_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_Configure(), fsl_mpl3115_i2c_1D_press_PeriodicCallback(), and mpl3115_ValidateConfig().