![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This defines the DSA adapter control interface abstract function list. More...
#include <isf_dsa_adapter.h>

Data Fields | |
| isf_dsa_status_t(* | Initialize )(isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t(* | ValidateSettings )(isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| isf_dsa_status_t(* | Configure )(isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| isf_dsa_status_t(* | StartData )(isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t(* | EndData )(isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t(* | Calibrate )(isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| isf_dsa_status_t(* | Shutdown )(isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t(* | Flash )(isf_SensorHandle_t *pSensorHandle, void *pFlashData, uint8 numBytes) |
| isf_dsa_data_converter_t * | Convert |
This defines the DSA adapter control interface abstract function list.
Definition at line 126 of file isf_dsa_adapter.h.
| isf_dsa_status_t(* Calibrate) (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
Pointer to the adapter Calibrate() function.
Definition at line 133 of file isf_dsa_adapter.h.
| isf_dsa_status_t(* Configure) (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
Pointer to the adapter Configure() function.
Definition at line 130 of file isf_dsa_adapter.h.
Referenced by configure_sensor().
| isf_dsa_data_converter_t* Convert |
Pointer to the adapter Convert() function.
Definition at line 136 of file isf_dsa_adapter.h.
Referenced by convert_sensor_data(), and isf_dsa_get_data_converter().
| isf_dsa_status_t(* EndData) (isf_SensorHandle_t *pSensorHandle) |
Pointer to the adapter EndData() function.
Definition at line 132 of file isf_dsa_adapter.h.
Referenced by stop_sensor().
| isf_dsa_status_t(* Flash) (isf_SensorHandle_t *pSensorHandle, void *pFlashData, uint8 numBytes) |
Pointer to the adapter Flash() function.
Definition at line 135 of file isf_dsa_adapter.h.
Referenced by BasicApp1_FlashSensor().
| isf_dsa_status_t(* Initialize) (isf_SensorHandle_t *pSensorHandle) |
Pointer to the adapter Initialize() function.
Definition at line 128 of file isf_dsa_adapter.h.
Referenced by init_sensor().
| isf_dsa_status_t(* Shutdown) (isf_SensorHandle_t *pSensorHandle) |
Pointer to the adapter Shutdown() function.
Definition at line 134 of file isf_dsa_adapter.h.
Referenced by shutdown_sensor().
| isf_dsa_status_t(* StartData) (isf_SensorHandle_t *pSensorHandle) |
Pointer to the adapter StartData() function.
Definition at line 131 of file isf_dsa_adapter.h.
Referenced by start_sensor().
| isf_dsa_status_t(* ValidateSettings) (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
Pointer to the adapter ValidateSettings() function.
Definition at line 129 of file isf_dsa_adapter.h.
Referenced by configure_sensor().